Other Parts Discussed in Thread: SYSBIOS
Thank you for your reply! I found that I did not add flags correctly, so it crashed after not knowing what to do with them.
Anyways, I now have a problem where my code uses VFP register arguments, whereas the compiler does not. I added the earlier mentioned flags for that reason, but it does not seem to work.. I'm getting the following log output:
**** Build of configuration am335x_debug for project ethercat ****
"C:\\ti\\ccsv6\\utils\\bin\\gmake" -k all
'Building file: ../am335xx_app.cfg'
'Invoking: XDCtools'
"C:/ti/xdctools_3_31_02_38_core/xs" --xdcpath="C:/ti/bios_6_45_01_29/packages;C:/ti/pdk_am335x_1_0_4/packages;" xdc.tools.configuro -o configPkg -t gnu.targets.arm.A8F -p ti.platforms.evmAM3359 -r debug -c "C:/Program Files (x86)/GNU Tools ARM Embedded/5.4 2016q3" "../am335xx_app.cfg"
'Finished building: ../am335xx_app.cfg'
' '
'Building file: ../tiescappl.c'
'Invoking: GNU Compiler'
"C:/Program Files (x86)/GNU Tools ARM Embedded/5.4 2016q3/bin/arm-none-eabi-gcc.exe" -c -mcpu=cortex-a8 -mtune=cortex-a8 -march=armv7-a -marm -mfloat-abi=hard -DAM335X_FAMILY_BUILD -DECAT_LIMITED_DEMO -Dam3359 -I"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/starterware/include/" -I"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/starterware/include/utils" -I"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/starterware/include/hw" -I"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/starterware/include/am335x/" -I"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/protocols/ethercat_slave/include" -I"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/board/include" -I"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/os_drivers/include" -I"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/os_drivers/lld/pruss" -I"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/protocols/ethercat_slave/firmware/v1.0" -I"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/starterware/library/qspilib/include" -I"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/starterware/device/" -I"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/control/foc" -I"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/examples/ethercat_slave" -g -gstrict-dwarf -Wall -mfloat-abi=hard -mfpu=vfp -MMD -MP -MF"tiescappl.d" -MT"tiescappl.o" -o"tiescappl.o" @"configPkg/compiler.opt" "../tiescappl.c"
In file included from C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/protocols/ethercat_slave/include/tiescutils.h:36:0,
from ../tiescappl.c:41:
C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/protocols/ethercat_slave/include/tiescbsp.h:217:21: warning: inline function 'bsp_pdi_access_perm_array' declared but never defined
PROTO inline Uint8 bsp_pdi_access_perm_array(Uint16 address, Uint8 access,
^
C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/protocols/ethercat_slave/include/tiescbsp.h:216:21: warning: inline function 'bsp_pdi_access_perm_dword' declared but never defined
PROTO inline Uint8 bsp_pdi_access_perm_dword(Uint16 address, Uint8 access);
^
C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/protocols/ethercat_slave/include/tiescbsp.h:215:21: warning: inline function 'bsp_pdi_access_perm_word' declared but never defined
PROTO inline Uint8 bsp_pdi_access_perm_word(Uint16 address, Uint8 access);
^
C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/protocols/ethercat_slave/include/tiescbsp.h:214:21: warning: inline function 'bsp_get_pdi_access_perm' declared but never defined
PROTO inline Uint8 bsp_get_pdi_access_perm(Uint16 address, Uint8 access);
^
'Finished building: ../tiescappl.c'
' '
'Building file: ../tiescutils.c'
'Invoking: GNU Compiler'
"C:/Program Files (x86)/GNU Tools ARM Embedded/5.4 2016q3/bin/arm-none-eabi-gcc.exe" -c -mcpu=cortex-a8 -mtune=cortex-a8 -march=armv7-a -marm -mfloat-abi=hard -DAM335X_FAMILY_BUILD -DECAT_LIMITED_DEMO -Dam3359 -I"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/starterware/include/" -I"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/starterware/include/utils" -I"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/starterware/include/hw" -I"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/starterware/include/am335x/" -I"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/protocols/ethercat_slave/include" -I"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/board/include" -I"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/os_drivers/include" -I"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/os_drivers/lld/pruss" -I"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/protocols/ethercat_slave/firmware/v1.0" -I"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/starterware/library/qspilib/include" -I"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/starterware/device/" -I"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/control/foc" -I"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/examples/ethercat_slave" -g -gstrict-dwarf -Wall -mfloat-abi=hard -mfpu=vfp -MMD -MP -MF"tiescutils.d" -MT"tiescutils.o" -o"tiescutils.o" @"configPkg/compiler.opt" "../tiescutils.c"
In file included from ../tiescutils.c:50:0:
C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/starterware/include/soc.h:111:20: warning: inline function 'SOCGetCoreId' declared but never defined
inline socCoreId_t SOCGetCoreId(void);
^
C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/starterware/include/soc.h:104:22: warning: inline function 'SOCGetSocFamilyId' declared but never defined
inline socFamilyId_t SOCGetSocFamilyId(void);
^
In file included from C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/protocols/ethercat_slave/include/tiescutils.h:36:0,
from ../tiescutils.c:45:
C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/protocols/ethercat_slave/include/tiescbsp.h:217:21: warning: inline function 'bsp_pdi_access_perm_array' declared but never defined
PROTO inline Uint8 bsp_pdi_access_perm_array(Uint16 address, Uint8 access,
^
C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/protocols/ethercat_slave/include/tiescbsp.h:216:21: warning: inline function 'bsp_pdi_access_perm_dword' declared but never defined
PROTO inline Uint8 bsp_pdi_access_perm_dword(Uint16 address, Uint8 access);
^
C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/protocols/ethercat_slave/include/tiescbsp.h:215:21: warning: inline function 'bsp_pdi_access_perm_word' declared but never defined
PROTO inline Uint8 bsp_pdi_access_perm_word(Uint16 address, Uint8 access);
^
C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/protocols/ethercat_slave/include/tiescbsp.h:214:21: warning: inline function 'bsp_get_pdi_access_perm' declared but never defined
PROTO inline Uint8 bsp_get_pdi_access_perm(Uint16 address, Uint8 access);
^
'Finished building: ../tiescutils.c'
' '
'Building target: ethercat.out'
'Invoking: GNU Linker'
"C:/Program Files (x86)/GNU Tools ARM Embedded/5.4 2016q3/bin/arm-none-eabi-gcc.exe" -march=armv7-a -marm -mfloat-abi=hard -DAM335X_FAMILY_BUILD -DECAT_LIMITED_DEMO -Dam3359 -g -gstrict-dwarf -Wall -mfloat-abi=hard -mfpu=vfp -Wl,-Map,"ethercat.map" -nostartfiles -static -Wl,--gc-sections -L"C:/ti/bios_6_45_01_29/packages/gnu/targets/arm/libs/install-native/arm-none-eabi/lib/fpu" -L"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/os_drivers/lib/am335x" -L"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/board/lib/am335x" -L"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/protocols/ethercat_slave/stack_lib/am335x" -L"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/starterware/binary/dal/lib/am335x-evm/a8/release/gcc" -L"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/starterware/binary/device/lib/am335x-evm/a8/release/gcc" -L"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/starterware/binary/board/lib/am335x-evm/a8/release/gcc" -L"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/starterware/binary/soc/lib/am335x-evm/a8/release/gcc" -L"C:/ti/sysbios_ind_sdk_02.01.02.02/sdk/starterware/binary/utils/lib/am335x-evm/a8/release/gcc" -Wl,--defsym,STACKSIZE=0x18000 -Wl,--defsym,HEAPSIZE=0x400 -Wl,--defsym,STACKSIZE=0x1C000 -o"ethercat.out" "./tiescappl.o" "./tiescutils.o" -Wl,-T"../AM335x.lds" -Wl,-T"configPkg/linker.cmd" -Wl,--start-group -lc -lgcc -lutils -lrdimon -lsoc -lm -lnosys -ldal -lsys_bios_driver -lboard -ldevice -lecat_slave_stack_gcc -lboard_support -Wl,--end-group
makefile:155: recipe for target 'ethercat.out' failed
c:/program files (x86)/gnu tools arm embedded/5.4 2016q3/bin/../lib/gcc/arm-none-eabi/5.4.1/../../../../arm-none-eabi/bin/ld.exe: error: ethercat.out uses VFP register arguments, c:/program files (x86)/gnu tools arm embedded/5.4 2016q3/bin/../lib/gcc/arm-none-eabi/5.4.1\libgcc.a(_udivmoddi4.o) does not
c:/program files (x86)/gnu tools arm embedded/5.4 2016q3/bin/../lib/gcc/arm-none-eabi/5.4.1/../../../../arm-none-eabi/bin/ld.exe: failed to merge target specific data of file c:/program files (x86)/gnu tools arm embedded/5.4 2016q3/bin/../lib/gcc/arm-none-eabi/5.4.1\libgcc.a(_udivmoddi4.o)
c:/program files (x86)/gnu tools arm embedded/5.4 2016q3/bin/../lib/gcc/arm-none-eabi/5.4.1/../../../../arm-none-eabi/bin/ld.exe: error: ethercat.out uses VFP register arguments, c:/program files (x86)/gnu tools arm embedded/5.4 2016q3/bin/../lib/gcc/arm-none-eabi/5.4.1\libgcc.a(_fixunsdfdi.o) does not
c:/program files (x86)/gnu tools arm embedded/5.4 2016q3/bin/../lib/gcc/arm-none-eabi/5.4.1/../../../../arm-none-eabi/bin/ld.exe: failed to merge target specific data of file c:/program files (x86)/gnu tools arm embedded/5.4 2016q3/bin/../lib/gcc/arm-none-eabi/5.4.1\libgcc.a(_fixunsdfdi.o)
c:/program files (x86)/gnu tools arm embedded/5.4 2016q3/bin/../lib/gcc/arm-none-eabi/5.4.1/../../../../arm-none-eabi/bin/ld.exe: error: ethercat.out uses VFP register arguments, c:/program files (x86)/gnu tools arm embedded/5.4 2016q3/bin/../lib/gcc/arm-none-eabi/5.4.1\libgcc.a(_fixunssfdi.o) does not
c:/program files (x86)/gnu tools arm embedded/5.4 2016q3/bin/../lib/gcc/arm-none-eabi/5.4.1/../../../../arm-none-eabi/bin/ld.exe: failed to merge target specific data of file c:/program files (x86)/gnu tools arm embedded/5.4 2016q3/bin/../lib/gcc/arm-none-eabi/5.4.1\libgcc.a(_fixunssfdi.o)
collect2.exe: error: ld returned 1 exit status
gmake: *** [ethercat.out] Error 1
gmake: Target 'all' not remade because of errors.
**** Build Finished ****