Hi,
I am trying to read the signal (generated by a waveform generator) using PRU capture input (capture6 rise and fall) / LATCH0.
The GREEN colored waveform indicates the input waveform to LATCH0 and the PURPLE colored waveform is the EDIO7_OUT indicating the waveform read using capture6 rise and fall.
I am unable to read the input waveform correctly at all times.
Waveform snapshot no.1 indicates the correctly read input signal and 2 and 3 indicates the input signal being misread.
In my program i am enabling capture6 rise and fall one-shot mode so that I can use the corresponding status flags and clear them by reading its corresponding capture registers.
Thank you!
Kind Regards,
Sagar Kunder
Waveform no.1
Waveform no.2
Waveform no.3