This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TMS320DM355: DM355 - Setting the ARM INTMUX Control Register

Part Number: TMS320DM355

Tool/software: Linux

Are there any examples of modifying the: 

ARM_INTMUX - ARM Interrupt Mux Control Register

I would specifically like to set BIt 2 - INT17 to SPI1 INT0 

There is no reference to that resister in arch/arm/mach-davinci/dm355.c - which is where i would have expected it....

Any help would be much appreciated!