Tool/software: Linux
I am using tda2xx board. sometimes I need to connect external camera, so can I connect USB camera with tda2xx board and how to connect ,get the data?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Linux
I am using tda2xx board. sometimes I need to connect external camera, so can I connect USB camera with tda2xx board and how to connect ,get the data?
Hi,
I need to use external camera via Ethernet, so I choose one camera and also attach that camera link so can u tell this camera is suitable or not for tda2xx board
HI,
1) suppose I use multides surround view kit ,can I connect other camera ( 60fps) with this view kit ?
thanks,
Hi Kalaiventhan,
If you use UB913/UB914 SERDES kit you cannot get 60 fps with 1MP capture. You can use the same camera but the fps will be low.
The max pixel clock is 100 MHz
Calculation is 100000000/height/width/2.
Or you can scale down the capture in VIP and then get 60 fps.
Regards,
Rishabh