This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

some confusion on NFS

Other Parts Discussed in Thread: TVP5150

Hi:

I'm using the DM6446 platform, and I followed the User's Guide to create the NFS.In my opinion,I have succeeded, because I can access the folder successfully.

what I confused is that the information print on the hyperterminal when mouting the NFS.see below informatin and pay attention to the characters in bold.

TI UBL Version: 1.12, Flash type: NAND
Booting PSP Boot Loader
PSPBootMode = NAND
Starting NAND Copy...
Initializing NAND flash...
Valid MagicNum found.
NAND Boot success.
   DONE

U-Boot 1.2.0 (Feb 11 2009 - 07:43:48)

dram_init info:
 start:0x80000000, size:0x8000000
DRAM:  128 MB
NAND:  64 MB
*** Warning - bad CRC or NAND, using default environment

In:    serial
Out:   serial
Err:   serial
ARM Clock : 297MHz
DDR Clock : 135MHz
ETH PHY : BroadCom PHY Chip
Hit any key to stop autoboot:  0
SEED_DVS6446_v1.2 # setenv bootargs mem=60M console=ttyS0,115200n8 root=/dev/nfs
 noinitrd rw ip=dhcp nfsroot=192.168.1.114:/opt/nfs video=dm64xxfb: output=pal
SEED_DVS6446_v1.2 # boot

Loading from NAND 64MiB 1,8V 8-bit, offset 0x168000
   Image Name:   Linux-2.6.10_mvl401-davinci_evm
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    1551676 Bytes =  1.5 MB
   Load Address: 80008000
   Entry Point:  80008000
Automatic boot of image at addr 0x80800000 ...
## Booting image at 80800000 ...
   Image Name:   Linux-2.6.10_mvl401-davinci_evm
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    1551676 Bytes =  1.5 MB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
OK

Starting kernel ...

Uncompressing Linux.............................................................
Linux version 2.6.10_mvl401-davinci_evm (root@phoenix) (gcc version 3.4.3 (Monta
Vista 3.4.3-25.0.30.0501131 2005-07-23)) #46 Fri Jul 11 01:17:42 CST 2008
CPU: ARM926EJ-Sid(wb) [41069265] revision 5 (ARMv5TEJ)
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
Machine: DaVinci EVM
Memory policy: ECC disabled, Data cache writeback
Built 1 zonelists
Kernel command line: mem=60M console=ttyS0,115200n8 root=/dev/nfs noinitrd rw ip
=dhcp nfsroot=192.168.1.114:/opt/nfs video=dm64xxfb: output=pal
PID hash table entries: 256 (order: 8, 4096 bytes)
Console: colour dummy device 80x30
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory: 60MB = 60MB total
Memory: 57508KB available (2524K code, 613K data, 144K init)
Mount-cache hash table entries: 512 (order: 0, 4096 bytes)
CPU: Testing write buffer coherency: ok
spawn_desched_task(00000000)
desched cpu_callback 3/00000000
ksoftirqd started up.
desched cpu_callback 2/00000000
desched thread 0 started up.
NET: Registered protocol family 16
Registering platform device 'nor_davinci.0'. Parent at platform
Registering platform device 'nand_davinci.0'. Parent at platform
Registering platform device 'musb_hdrc'. Parent at platform
DaVinci I2C DEBUG: 12:14:45 May 16 2008
Registering platform device 'i2c'. Parent at platform
SCSI subsystem initialized
usbcore: registered new driver usbfs
usbcore: registered new driver hub
devfs: 2004-01-31 Richard Gooch (rgooch@atnf.csiro.au)
devfs: boot_options: 0x1
NTFS driver 2.1.22 [Flags: R/W].
JFFS2 version 2.2. (NAND) (C) 2001-2003 Red Hat, Inc.
yaffs May 16 2008 12:14:06 Installing.
Registering platform device 'davincifb.0'. Parent at platform
Console: switching to colour frame buffer device 90x30
Registering platform device 'davinci_resizer.2'. Parent at platform
Registering platform device 'davinci_previewer.2'. Parent at platform
Registering platform device 'davinci_pwm0.0'. Parent at platform
Registering platform device 'davinci_pwm1.1'. Parent at platform
Registering platform device 'davinci_pwm2.2'. Parent at platform
Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled
Registering platform device 'serial8250'. Parent at platform
ttyS0 at MMIO 0x1c20000 (irq = 40) is a 16550A
ttyS1 at MMIO 0x1c20400 (irq = 41) is a 16550A
io scheduler noop registered
io scheduler anticipatory registered
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize
Registering platform device 'ti_davinci_emac'. Parent at platform
TI DaVinci EMAC Linux version updated 4.0
TI DaVinci EMAC: Installed 1 instances.
netconsole: not configured, aborting
i2c /dev entries driver
Linux video capture interface: v1.00
Registering platform device 'vpfe.1'. Parent at platform
TVP5150 support for SEED_DVS6446 by Stephen Zhang
DaVinci v4l2 capture driver V1.0 loaded
elevator: using anticipatory as default io scheduler
DaVinci NAND Controller rev. 2.1
NAND device: Manufacturer ID: 0x20, Chip ID: 0x36 (ST Micro NAND 64MiB 1,8V 8-bi
t)
Scanning device for bad blocks
Creating 1 MTD partitions on "NAND 64MiB 1,8V 8-bit":
0x00460000-0x04000000 : "Flash Partition 0"
Initializing USB Mass Storage driver...
usbcore: registered new driver usb-storage
USB Mass Storage support registered.
usbcore: registered new driver usbhid
drivers/usb/input/hid-core.c: v2.0:USB HID core driver
mice: PS/2 mouse device common for all mice
musb_hdrc: version 2.2a/db-0.4.8 [pio] [host] [debug=0]
musb_hdrc: USB Host mode controller at c4066000 using PIO, IRQ 12
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
Registering platform device 'mmc0.1'. Parent at platform
 : Supporting 4-bit mode
Registering platform device 'davinci-audio.0'. Parent at platform
DAVINCI AIC23 audio support initialized
NET: Registered protocol family 2
IP: routing cache hash table of 512 buckets, 4Kbytes
TCP: Hash tables configured (established 4096 bind 8192)
NET: Registered protocol family 1
NET: Registered protocol family 17
Sending DHCP requests ., OK
IP-Config: Got DHCP answer from 0.0.0.0, my address is 192.168.1.107
IP-Config: Complete:
      device=eth0, addr=192.168.1.107, mask=255.255.255.0, gw=192.168.1.1,
     host=192.168.1.107, domain=, nis-domain=(none),
     bootserver=0.0.0.0, rootserver=192.168.1.114, rootpath=
Looking up port of RPC 100003/2 on 192.168.1.114
Looking up port of RPC 100005/1 on 192.168.1.114
VFS: Mounted root (nfs filesystem).
Mounted devfs on /dev
Freeing init memory: 144K
INIT: version 2.85 booting
Mounting a tmpfs over /dev...done.
Creating initial device nodes...done.
Activating swap...done.
Remounting root filesystem...done.
Calculating module dependencies
WARNING: Couldn't open directory /lib/modules/2.6.10_mvl401-davinci_evm: No such
 file or directory
FATAL: Could not open /lib/modules/2.6.10_mvl401-davinci_evm/modules.dep.temp fo
r writing: No such file or directory
Loading modules:
Starting checking all file systems: fsck
fsck 1.35 (28-Feb-2004)
Starting mounting local filesystems: mount nothing was mounted
Cleaning: /etc/network/ifstate.
Setting up IP spoofing protection: rp_filter.
Disable TCP/IP Explicit Congestion Notification: done.
Starting network interfaces: done.
Starting hotplug subsystem:
   pci
   pci      [success]
   usb
   usb      [success]
   isapnp
   isapnp   [success]
   ide
   ide      [success]
   input
   input    [success]
   scsi
   scsi     [success]
done.
Starting portmap daemon: portmap.
Cleaning: /tmp /var/lock /var/run done.
Setting pseudo-terminal access permissions...done.
Updating /etc/motd...done.
INIT: Entering runlevel: 3
Starting system log daemon: syslogd klogd.
Starting NFS common utilities: statd lockd.
Starting internet superserver: inetd.
Starting MontaVista target tools daemon: mvltdmvltd version 2.1 MontaVista Softw
are,Inc.
.
MontaVista(R) Linux(R) Professional Edition 4.0 (0501140)

192.168.1.107 login: root
Last login: Tue Jun  6 11:53:32 1905 on console
Linux 192.168.1.107 2.6.10_mvl401-davinci_evm #46 Fri Jul 11 01:17:42 CST 2008 a
rmv5tejl GNU/Linux

Welcome to MontaVista(R) Linux(R) Professional Edition 4.0 (0501140).

root@192.168.1.107:~#

why it occur the WARNING and FATAL? And how to correct it?