This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: eMMC compatibility

Part Number: AM5728

Hi ,

We are designing our custom board on AM5728 Processor

We are thinking to go with 16GB eMMC NAND Flash Memory .

We have selected the memory chip, but it  comes with 5.1 JEDEC Standard and it supports HS400 mode.

The eMMC JEDEC Standard in AM5728 is limited to 4.5 and HS200 mode

So my question is by using a 5.1 JEDEC and HS400 mode eMMC NAND Flash chip, will there be any backward compatibility when i interface it to the processor.??

In AM57X IDK , a 16 GB eMMC NAND Flash is used with its JEDEC standard being 5.0 . So can i consider 5.1 is also backward compatible ?

Thanks,

Chandan