This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/DRA726: Weston screen rotation

Part Number: DRA726
Other Parts Discussed in Thread: AM5728

Tool/software: Linux

Our new 7 inch LCD is 800x1280 so the display is sideways which is unacceptable for our customer.

I am able to rotate the display when on the command line but when I load weston the display is then sideways.

What would be the equivalent of xrandr for weston? or some other command that would get the screen to rotate?

I used the automotive SDK 3.02 as a base. For the splash screen in u-boot I just rotated the picture and reflashed the QSPI.

For the demo to the customer I am going to use my Funtoo Linux but for the real project I will use embedded wizard with weston as I use with the 12 inch display.

Michel