A customer I'm supporting has been looking at the datasheet for the AM5728, and is curious about the dual GMACs. The datasheet shows only 1 MAC and a 3 port switch, and he is wondering if this means that there two MAC addresses? I've looked in the TRM and section 24.11.4.8.5.2 mentions a Dual MAC Mode, and table 18-271 mentions a bit field that "contains the last three octets (NIC specific) of the MAC address of the GMAC_SW port 0" and table 18-275 referencing the MAC address of the GMAC_SW port 1.
Would someone be able to verify that there are two MAC addresses, or the number of interfaces the driver gives us?
Thanks,
Barend