This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/66AK2E05: Yocto build fail

Part Number: 66AK2E05

Tool/software: Linux

Hi,

I try to build Yocto by referring "http://processors.wiki.ti.com/index.php?title=Processor_SDK_Building_The_SDK&oldid=218732" 

Parsing recipes: 100% |################################################################################################################| Time: 0:07:06
Parsing of 2507 .bb files complete (0 cached, 2507 parsed). 3254 targets, 499 skipped, 0 masked, 0 errors.
WARNING: No recipes available for:
/home/alibivmuser/tisdk/rootfs/tisdk/sources/meta-openamp/recipes-bsp/device-tree/device-tree-generation_%.bbappend
NOTE: Resolving any missing task queue dependencies
NOTE: preferred version 4.9% of nativesdk-linux-libc-headers not available (for item nativesdk-linux-libc-headers)
NOTE: versions of nativesdk-linux-libc-headers available: 4.4 4.8
NOTE: preferred version 4.9% of nativesdk-linux-libc-headers not available (for item nativesdk-linux-libc-headers-dev)
NOTE: versions of nativesdk-linux-libc-headers available: 4.4 4.8
NOTE: preferred version 4.9% of linux-libc-headers not available (for item linux-libc-headers)
NOTE: versions of linux-libc-headers available: 4.4 4.8
NOTE: preferred version 4.9% of linux-libc-headers not available (for item linux-libc-headers-dev)
NOTE: versions of linux-libc-headers available: 4.4 4.8

Build Configuration:
BB_VERSION = "1.32.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Ubuntu-14.04"
TARGET_SYS = "arm-linux-gnueabi"
MACHINE = "k2e-evm"
DISTRO = "arago"
DISTRO_VERSION = "2017.06"
TUNE_FEATURES = "arm armv7a vfp thumb neon callconvention-hard"
TARGET_FPU = "hard"
meta-processor-sdk = "HEAD:2b7f7b00654eb3faaea7c66271ebe508b9ffc019"
meta-arago-distro
meta-arago-extras = "HEAD:8f49ed67d0627a04ac72fd388fda7756273ba2d7"
meta-browser = "HEAD:08576b03af624b65ad949c410d84c11c7d1f2e39"
meta-openamp = "HEAD:8a214032bfb7e8124bc1485c70c69f7d60abb819"
meta-qt5 = "HEAD:2c9f0e4eb0e9097f6f872ec1e1d81768a8ab5f1b"
meta-networking
meta-ruby
meta-python
meta-oe
meta-gnome = "HEAD:fe5c83312de11e80b85680ef237f8acb04b4b26e"
meta-ti = "HEAD:a18d57af8384ced25996739bb66d197c69efb77b"
meta-linaro-toolchain
meta-optee = "HEAD:49b0f32d7e955f250b0022d1b2f403f45a2c2d9c"
meta = "HEAD:e3911133ee9aad7cc3ae89faea80a097f6614fab"

Initialising tasks: 100% |#############################################################################################################| Time: 0:00:09
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
No currently running tasks (139 of 3695) 3% |### |
/usr/bin/env: relocation error: /home/linuxbrew/.linuxbrew/lib/libpthread.so.0: symbol __libc_vfork, version GLIBC_PRIVATE not defined in file libc.soERROR: Failed to spawn fakeroot worker to run /home/alibivmuser/tisdk/rootfs/tisdk/sources/oe-core/meta/recipes-kernel/linux-libc-headers/linux-libc-headers_4.8.bb:do_install: [Errno 32] Broken pipe
WARNING: /home/alibivmuser/tisdk/rootfs/tisdk/sources/bitbake/lib/bb/runqueue.py:1797: ResourceWarning: unclosed file <_io.BufferedWriter name=30>
return True

WARNING: /home/alibivmuser/tisdk/rootfs/tisdk/sources/bitbake/lib/bb/runqueue.py:1797: ResourceWarning: unclosed file <_io.BufferedReader name=31>
return True

NOTE: Tasks Summary: Attempted 139 tasks of which 0 didn't need to be rerun and 1 failed.

Summary: There were 3 WARNING messages shown.
Summary: There was 1 ERROR message shown, returning a non-zero exit code.
alibivmuser@ALIBIVM05:~/tisdk/rootfs$

Regards,

Arun 

  • Hi Arun,

    /usr/bin/env: relocation error: /home/linuxbrew/.linuxbrew/lib/libpthread.so.0: symbol __libc_vfork, version GLIBC_PRIVATE not defined in file libc.soERROR: Failed to spawn fakeroot worker to run /home/alibivmuser/tisdk/rootfs/tisdk/sources/oe-core/meta/recipes-kernel/linux-libc-headers/linux-libc-headers_4.8.bb:do_install: [Errno 32] Broken pipe

    Are you trying to build the unmodified filesystem, or did you add some resource to the .bb recipes?

    Best Regards,
    Yordan
  • Hi Yordan, 

    I am using unmodified source.

    Regards,

    Arun 

  • Hi Arun,

    Can you check the permissions of the tisdk folder & subfolders? Make sure you don't need root access.

    Best Regards,
    Yordan
  • Hi Yordan,

    From the above shared log it seems i am not accessing as root .

    Log :-

    alibivmuser@ALIBIVM05:~/tisdk/rootfs$

     

    Regards,

    Arun 

  • Sorry for the delay. Yes, I see that you're not accessing as root. But some folders may require root access, so you should change this using chown -R ~/tisdk/ <your user different from root>:<group different from root>

    Best Regards,
    Yordan
  • Hi Yordan, 

    Please give me some straightforward answer some time you are saying don't be root  now you are saying give privilege of root . 

    Are you not aware which folder needed root access ? 

    Arun 

  • You DON'T need to be root! Perhaps you don't understand what I am saying (or maybe I didn't express myself clear enough).
    You need to ensure that NEITHER of the folders in tisdk/ requires root access. This is done by executing chown!!
  • Hi Yordan,

    I try to download http://software-dl.ti.com/processor-sdk-mirror/sources/git2_git.ti.com.ti-linux-kernel.ti-linux-kernel.git.tar.gz

    On web link http://software-dl.ti.com/processor-sdk-mirror/sources/ 

    the size of "git2_git.ti.com.ti-linux-kernel.ti-linux-kernel.git.tar.gz" is listed 4.4G but when i am downloading it seems the size of file is 2.1G. 

    When i am unpacking the tar getting error log like 

    gzip: stdin: unexpected end of file
    tar: Unexpected EOF in archive
    tar: Unexpected EOF in archive
    tar: Error is not recoverable: exiting now

    Full logs:- 

    alibivmuser@arun:~/npci/vnl/git-down-linux$ axel -va software-dl.ti.com/.../git2_git.ti.com.ti-linux-kernel.ti-linux-kernel.git.tar.gz
    Initializing download: software-dl.ti.com/.../git2_git.ti.com.ti-linux-kernel.ti-linux-kernel.git.tar.gz
    Opening output file git2_git.ti.com.ti-linux-kernel.ti-linux-kernel.git.tar.gz
    Server unsupported, starting from scratch with one connection.
    Starting download

    Connection 0 finished ]

    Downloaded 2048,0 megabytes in 2:16:20 seconds. (256,35 KB/s)
    alibivmuser@arun:~/npci/vnl/git-down-linux$
    alibivmuser@arun:~/npci/vnl/git-down-linux$ ls
    git2_git.ti.com.ti-linux-kernel.ti-linux-kernel.git.tar.gz
    alibivmuser@arun:~/npci/vnl/git-down-linux$
    alibivmuser@arun:~/npci/vnl/git-down-linux$ du -sh git2_git.ti.com.ti-linux-kernel.ti-linux-kernel.git.tar.gz
    2,1G git2_git.ti.com.ti-linux-kernel.ti-linux-kernel.git.tar.gz
    alibivmuser@arun:~/npci/vnl/git-down-linux$
    alibivmuser@arun:~/npci/vnl/git-down-linux$ tar -xvf git2_git.ti.com.ti-linux-kernel.ti-linux-kernel.git.tar.gz
    ./
    ./branches/
    ./FETCH_HEAD
    ./packed-refs
    ./description
    ./HEAD
    ./hooks/
    ./hooks/commit-msg.sample
    ./hooks/pre-applypatch.sample
    ./hooks/pre-commit.sample
    ./hooks/pre-rebase.sample
    ./hooks/pre-push.sample
    ./hooks/post-update.sample
    ./hooks/prepare-commit-msg.sample
    ./hooks/applypatch-msg.sample
    ./hooks/update.sample
    ./gc.log.lock
    ./config
    ./objects/
    ./objects/54/
    ./objects/54/247ac8cb5b756aca18144d1766ed116341edc9
    ./objects/43/
    ./objects/43/1c86e8542ba99e7f9ce1dcaf154057bcb53222
    ./objects/43/d4a1e6052b191f4aeabe0cc2e21bab9cf3498b
    ./objects/43/2de01939722dae42ba25563c12591bf8a8011d
    ./objects/be/
    ./objects/be/c5414daee0af2056317e6a2a26ab6af7b1fb30
    ./objects/c4/
    ./objects/c4/565ab320089abd45054c1471a441cef81aa449
    ./objects/4e/
    ./objects/4e/66d58fd10c5a880bf0b4baa728b14bca997d82
    ./objects/4e/2fdcb0ffeb998e6c4f703d11c49b3b83539f18
    ./objects/17/
    ./objects/17/c41da3b55f1c7d94460f98647f0fdb084a9dbe
    ./objects/17/72777f6f903538d373460c75a4dc2b8416fac3
    ./objects/17/8c3dfe853a18391b029e6b62e1eed22be1871e
    ./objects/3f/
    ./objects/3f/18cc669a61c783f1bdaa749fdbac39f50e8a50
    ./objects/3f/c7f12c8ee7aef6e671956e61180347846375d6
    ./objects/0e/
    ./objects/0e/cdcd3a520b99287d0573df4feb43bdceb44b87
    ./objects/0e/e61171617cbdbc66e880b0dacf074792eab46c
    ./objects/0e/a3b074a433209e185d96b0a8720a0d4a0f7dce
    ./objects/ce/
    ./objects/ce/d6f3f6b901293039cc562cc90db12fdeab395d
    ./objects/ce/e1241ee874a552a56b83e20d522cdbf4d0b910
    ./objects/ce/9ec37bddb633404a0c23e1acb181a264e7f7f2
    ./objects/c9/
    ./objects/c9/d0654b910dac448e83af5204d7d812ed5f905e
    ./objects/c9/3f837c7541bd021b72a492b2ddd701ef796b3d
    ./objects/31/
    ./objects/31/1e51e726552f11d001919562c8580ef924bfe6
    ./objects/31/6a1c94a8b42bef40f78a36a34bdef54cba6b8a
    ./objects/31/a3faf3229697d646eab0fc942b24d73b0bcfa1
    ./objects/70/
    ./objects/70/550e98a918c167dc3359ef3b66c6097dda813a
    ./objects/70/ee63620db648ff9c69151a211f8ddc6c84a811
    ./objects/70/809c4c54dbbd5eba6030a2a690cc8a1fdfe066
    ./objects/9a/
    ./objects/9a/91c11a7fbba2b5cfa30be39bd8dab947dd95a4
    ./objects/f4/
    ./objects/f4/bd578bed551451d15852e36e254d2e585cba11
    ./objects/f4/5e6e045d5e1cb6d963d72d7e3dc3bf91529e5b
    ./objects/86/
    ./objects/86/79916119a8b92aed9ab07eeb95dddd9b199be8
    ./objects/86/698af3d7fc45f8a43fa60de409ca339cd52d6c
    ./objects/42/
    ./objects/42/8d0adb474d5c33a687a2fcdd1c544a6bc0cf6e
    ./objects/42/0eb6d7efc4591ef1968106cdaa980ea06fe00e
    ./objects/42/90bec51d91c0313b921d2de1e8028d214a6969
    ./objects/d8/
    ./objects/d8/e3904b80c4e5b65531e06ebb4bc86323b76ea1
    ./objects/b2/
    ./objects/b2/3e2459768fb350be2a6d2352adb25eb9a6bbdb
    ./objects/5d/
    ./objects/5d/0c18afa827ceb1b7ee0961d440affa4fb9fea5
    ./objects/5d/b9bf742a6cff8c3fcd540d49a5020f1d2c241b
    ./objects/0f/
    ./objects/0f/69dd59926dc9b4c1b89f1f8cace6617af921a4
    ./objects/68/
    ./objects/68/586da9b8eefb15f0cac32d4b059c0b9165c187
    ./objects/68/b9c1e66dca85760e555e5a8631d85589eea52c
    ./objects/09/
    ./objects/09/a5f9672be5d66ef5cdd043e411b979baa94f18
    ./objects/09/668bb0e36ce76575c5d52e1eca399b7235d64c
    ./objects/aa/
    ./objects/aa/ddfcb4931810ea4bec490a36ec0a325ca10645
    ./objects/aa/29b2022fe1942d6f7f64dfa8e2d0407e17d101
    ./objects/63/
    ./objects/63/debf7dd3472e34afaa5e059b547b9ea2010c52
    ./objects/b1/
    ./objects/b1/7185821e106a3352fe32293445014456a8d518
    ./objects/b1/f0cd6c764ab018b4bcecd2e039af95155aa803
    ./objects/6c/
    ./objects/6c/056c1f25f3a46a1282e15e9af8772cb2b8038f
    ./objects/f0/
    ./objects/f0/f52afb60f57f31c099dc849c6757fea5664e89
    ./objects/19/
    ./objects/19/45a8ea20998490b48aa70dfe56c4fbaad744ea
    ./objects/a1/
    ./objects/a1/e294dff01f66d0fce67ecb39067baf9b7f02ef
    ./objects/a1/2921fe0797c122f9dfccafc1c0c89198a88733
    ./objects/ee/
    ./objects/ee/8ab55262fe65172f9865f76db6632bf945040f
    ./objects/d1/
    ./objects/d1/d84c9626bb3a519863b3ffc40d347166f9fb83
    ./objects/67/
    ./objects/67/9ddbea158e0cba6b0fff74ee05d080978d7bc1
    ./objects/9e/
    ./objects/9e/9beb633e76e7d0ef8f30cd56f0862836ac6526
    ./objects/9e/927ae7fceda8cdb6a6a77697c55da285d85746
    ./objects/c3/
    ./objects/c3/5ecc887c9c9332d6ae0d4c34494751cf63c7f7
    ./objects/c3/de641d81f8e5a61187cd181a5e42fbade9e380
    ./objects/ef/
    ./objects/ef/507c830ec2c0ad803519e2f100cb04ec6ba6a0
    ./objects/ef/bdc63b514a7648626e5556f2e9b4b7533e5233
    ./objects/88/
    ./objects/88/cc85d1928d5671df1cb2778068577bf6bc3e99
    ./objects/88/e711eb3c6168c59f421d1d5748469e4e1545bc
    ./objects/f7/
    ./objects/f7/9c71b0fccb6efa34c3fb43322c2a32210c4ea1
    ./objects/f7/9a951824d621a969eb1814c8b21c3192444847
    ./objects/6e/
    ./objects/6e/2028aaa1373081e553d4442736ce0d1dd279e8
    ./objects/5a/
    ./objects/5a/bee1e293a4f318ff701825282cad66f68a1a7b
    ./objects/eb/
    ./objects/eb/3cbc29413714216fe3d3b2e70993c4d6a02ec5
    ./objects/eb/43a7ff076d4ef1a4617c3cfc235db1c84c68a2
    ./objects/1e/
    ./objects/1e/bcb9e73d3a95beb8174000fab9f5cf534fdf52
    ./objects/1e/a52a1ffa87662c728a2d311aa5879d475c6e1f
    ./objects/1e/7c6b308107cdbf70fa1c4241fe1256d5773e3f
    ./objects/f5/
    ./objects/f5/43b318cca7497b0c33d5a8342bc8d35bad1741
    ./objects/f5/caecb092f6e8c642101f8c56c3fbb136de7052
    ./objects/7b/
    ./objects/7b/0e45eca8a55e922aca906843366873c4c73389
    ./objects/7b/30782b7586af7e5434e4bf5746a3bff86f6d15
    ./objects/58/
    ./objects/58/59dceae8256b2dbd83a8c43cef8158de5be369
    ./objects/8b/
    ./objects/8b/be33b1d74a44b937d6ddbf1d0b9c12bc0632ad
    ./objects/1c/
    ./objects/1c/b108f8e10d3c5e7e00a3468b25adb9d3e558c4
    ./objects/1c/e8051cf06081d839f888c299fed1d1acf5d46f
    ./objects/1c/08c22c874ac88799cab1f78c40f46110274915
    ./objects/ba/
    ./objects/ba/ef3c06812314ae2aa167300d46c3803c4ef1e4
    ./objects/bd/
    ./objects/bd/717c56efa61298fead24e219e799728592599a
    ./objects/4f/
    ./objects/4f/c409048d5afb1ad853f294b4262ecf2c980a49
    ./objects/4f/cb8f06977a9355efcd75821206da69cf947e92
    ./objects/7e/
    ./objects/7e/e1c64e2c0d7b9dfd620838f8f683e2ab399f4b
    ./objects/7e/a5d509a39d41dc7a2b10bc5404293e047241a7
    ./objects/fa/
    ./objects/fa/6a573120a516fb02e6a407177ed1669233ddfe
    ./objects/fa/fb6cd4b6a8e3d3ab02644f6434735a9eed6d51
    ./objects/fa/e146d95014fd95d3bb7116137c34383c1d16f4
    ./objects/9c/
    ./objects/9c/0ea7ce3464a6533e59b88136bee46fa5d637e1
    ./objects/ae/
    ./objects/ae/c3aec3f152267b60d0f2784bf5d34bb0e790f6
    ./objects/ae/93e3f09544fe613d17cfefcd4e2ef1f187ce7d
    ./objects/ae/c154a6966d9e1e840c69c1fbb0330b719e2c5b
    ./objects/a2/
    ./objects/a2/0af2c733995fcd05fc65f7465bdd2e409d335c
    ./objects/pack/
    ./objects/pack/pack-b148e1c2d4f00b0bc7fd9dca8e7f2b82a4637630.pack
    ./objects/pack/pack-64f5d424f0dbf1447ec84f2f61b694e9e5048843.idx
    ./objects/pack/pack-612565d2a489b4f39cc0394ec6544faff50e1e5a.pack
    ./objects/pack/pack-8b2d98f7beb2ea766ff58eab03f63d2f61468a41.pack
    ./objects/pack/pack-0cfe6324989bf560ac686ab36f30e7090e7839c5.idx
    ./objects/pack/pack-8675a09801de2e5fa873f4a9402653c8a253facc.idx
    ./objects/pack/pack-e9a4357b93e712c0e6892649d3101b1815e3e347.pack
    ./objects/pack/pack-b2d2f99be24d4405e5619d695b6b82143582254c.idx
    ./objects/pack/pack-548eb8d6b3c4137b9ea807c199ffb9c54e66dd78.idx
    ./objects/pack/pack-1714ef57106c3e46974bf0f14a07e39db4444304.idx
    ./objects/pack/pack-ff810ef00654a68e9231cd1ad329fed7db0a5970.pack
    ./objects/pack/pack-1d00a3ae0c41a69b9c5478d0990cdd6a742e3c8a.idx
    ./objects/pack/pack-2afb9eb9392abee95ba4297cc6e37b62954143c5.pack
    ./objects/pack/pack-3b189690a344d9a51ac7d7fed67bf7378cc1c6ee.idx
    ./objects/pack/pack-c9191d273a06ac7dd243a3357bee4a65a2f3a86b.pack
    ./objects/pack/pack-c16e7564811cb8839b319fd6d14cf1f0bc3d6b55.idx
    ./objects/pack/pack-a41d3dea3c08e8fb3f5132f2ffd5bbc7c68c00cf.idx
    ./objects/pack/pack-6d05d4cdf4510afea453493dd2a8ae1a354bd7f5.idx
    ./objects/pack/pack-4fb467b89c35202b03acc0cdf5a7437e14734154.pack
    ./objects/pack/pack-f78304edb741683c083e4bcdef98c395cb5b9fb7.pack
    ./objects/pack/pack-8383036d3b8c90d5bfd140782c2c00f5e207f316.idx
    ./objects/pack/pack-2895b99fdf482b813fc80a95fc2de80ad763aacb.idx
    ./objects/pack/pack-3e0be112b08ba493a159588cb7f1c25d0cb26202.idx
    ./objects/pack/pack-e0f702c759e257519c84cd4a0edc0242635773f7.pack
    ./objects/pack/pack-4dec30f4b84b444923d2fcfbef4a565e30dc112a.pack
    ./objects/pack/pack-b2d2f99be24d4405e5619d695b6b82143582254c.pack
    ./objects/pack/pack-b04c5b86bd0996c418f0888aa90f26b83386d8f7.idx
    ./objects/pack/pack-100e38d80af3ed34a568d2197ce8c46de56fd2ed.idx
    ./objects/pack/pack-6751361202ec08789d8439bc984f70cbac8c65c6.pack
    ./objects/pack/pack-cb9c60cc9f54fd5deee8e5c0ac3d2c1a0afd8aef.idx
    ./objects/pack/pack-c9191d273a06ac7dd243a3357bee4a65a2f3a86b.idx
    ./objects/pack/pack-43ee3ed038b4a82aeed3961ac46c13749afe0de3.pack
    ./objects/pack/pack-5b040b28302cc7fbafd6b91b80f3b0fce172b8fa.pack
    ./objects/pack/pack-8bc54892f715367dfe97bf0d1e36152d23cb54ff.idx
    ./objects/pack/pack-859a81c285442fd142d34cc101e60c98d8e0edc7.idx
    ./objects/pack/pack-98fdcc9bf892b699064454127f09e00d79804914.idx
    ./objects/pack/pack-c5e537b153727b0ab1fcc70f346b357d55124375.idx
    ./objects/pack/pack-f914f628e2b996a29173913aedd93b38d1a1db78.pack
    ./objects/pack/pack-9fc480ebaec9be0703a0c82717c4637e5a9a7ce9.pack
    ./objects/pack/pack-3f82c7afbd3f8ad713ae656b50c4408bcd3c94aa.pack
    ./objects/pack/pack-c16e7564811cb8839b319fd6d14cf1f0bc3d6b55.pack
    ./objects/pack/pack-1bf545faa5ff02785ec468af97131980e1f4f3c5.pack
    ./objects/pack/pack-927428854cbd7fb134b030fdc9045a31c21a9545.pack
    ./objects/pack/pack-68433e23d776c66406d4c0fe8a7b9d00df5c4d9c.idx
    ./objects/pack/pack-0fbafcc876ae0b2b149997256e245d2ca963f0c2.idx
    ./objects/pack/pack-b80888eb1df75c9b286e8837529798e90449b74c.pack
    ./objects/pack/pack-be293d70e8c9d438497c37f6667cddbdc34a88ca.idx
    ./objects/pack/pack-5092fbcbfbaeab30d111e5ac99fa5d1c94fe7a75.pack
    ./objects/pack/pack-dc069a5d336cb0fef4ea166367306d6e6200ba34.pack
    ./objects/pack/pack-e1bd2674643ec5fcf098b1a07948f19be543cf70.idx
    ./objects/pack/pack-7f9032cd14e38a96995fc9da860f893be3dc21ae.idx
    ./objects/pack/pack-c73924002b11aad49a745a5e9066ef7fbf7759ee.idx
    ./objects/pack/pack-4cc7fd69a854858e6ee78c9a2432746e24a06903.idx
    ./objects/pack/pack-7a4356fcb0213af3799cf65da539323eedc24f1e.pack
    ./objects/pack/pack-c4c5c3f26f67d8161bc2e278a0eb09418eaed801.pack
    ./objects/pack/pack-68f8c56b3a43f85f73a6957e978b95a244f3e0ae.idx
    ./objects/pack/pack-ac2cc30c6904b6ca716bc3bdc352bf6e7ca254d5.idx
    ./objects/pack/pack-6c253a12241044e7a52465cbe56c348a30144756.pack
    ./objects/pack/pack-6d05d4cdf4510afea453493dd2a8ae1a354bd7f5.pack
    ./objects/pack/pack-73d1384dee52222b0be40f66b752cf8428a9c6da.pack
    ./objects/pack/pack-531c26b4ed8142d99b95a00205570a64fd2605ef.pack
    ./objects/pack/pack-b0b9082606a1694a4c9f773fbd93c40d3d895a69.idx
    ./objects/pack/pack-700b8be366dd9924d4e128e7d81494753c141ffd.idx
    ./objects/pack/pack-3f4092fad30dabe3c2329ae0bb6601f09609f78c.pack
    ./objects/pack/pack-feb619460ba811cd07965af6d80ab72b06f8a7ae.pack
    ./objects/pack/pack-6cfcc3b4e8564ad2b9a581a2701823a9f1105510.idx
    ./objects/pack/pack-737cf3d669be50862ffa0bc9e8133a96933843c3.pack
    ./objects/pack/pack-c4c5c3f26f67d8161bc2e278a0eb09418eaed801.idx
    ./objects/pack/pack-8d479b1ac66bfbd2bd1656830ffc1c6ace921ea0.idx
    ./objects/pack/pack-46270cc039ffca2eaf36e3a5dd1bc2919975d49c.pack
    ./objects/pack/pack-741c26c27b033396a069622225bb6f1f9fbb40a2.pack
    ./objects/pack/pack-d620d880fe614ace2e06ea9c96071d5cc54288ff.idx
    ./objects/pack/pack-459ffed4b79e48b95e63792efda94c0ef52d03f7.pack
    ./objects/pack/pack-e3f225deb53fd1d379c274c611b0815535214169.pack
    ./objects/pack/pack-d13aa70b8ff2ece90c79ed37229a3ec5fb5f3741.idx
    ./objects/pack/pack-76f561f839051df13459b5a869a83176934e388a.pack
    ./objects/pack/pack-fa9d5e84bfa7b63601827062bc37ac917c3d8f3c.pack
    ./objects/pack/pack-68f8c56b3a43f85f73a6957e978b95a244f3e0ae.pack
    ./objects/pack/pack-69ffcfe2c7066b62fc7bc3008c4dd802fcf99c77.pack
    ./objects/pack/pack-d192e2a6de88299d744e05044cfdb50fbd49ddb9.idx
    ./objects/pack/pack-43b39922770761c0f92d8e4d4c3b5b692ffca6df.idx
    ./objects/pack/pack-1fedfa1cf5724200125b085d55a48c1c3fa63f3a.idx
    ./objects/pack/pack-f90cde831ef2e65eb0f3e9f06f45ff766508da92.idx
    ./objects/pack/pack-edad9ca0adfb922e0f6efc7f42fc7711ade29a56.idx
    ./objects/pack/pack-64448e9bf62caf05956c25d28b89cdd078633942.idx
    ./objects/pack/pack-e448aa66b2b50b78fcd811f8f78af4b0817a82d3.pack
    ./objects/pack/pack-dc395f3803275178bdf176ef3a5b5f6c06b30b25.pack
    ./objects/pack/pack-6bb3deb0e4aac320755096238a1b479553f7a2c5.idx
    ./objects/pack/pack-2895b99fdf482b813fc80a95fc2de80ad763aacb.pack
    ./objects/pack/pack-1786c46a645ff55609678026241b19b789d5a839.pack
    ./objects/pack/pack-b0b9082606a1694a4c9f773fbd93c40d3d895a69.pack
    ./objects/pack/pack-5326a86e5c26873e774e834449ffeacb17c02d65.pack
    ./objects/pack/pack-c04de846e6722707c869eb692f8994bf7ab6d657.pack
    ./objects/pack/pack-1e964fba78ef86e439e4d5a7b0a753cd1302666f.pack
    ./objects/pack/pack-221cebf0d80b84124f6b8edbd9eed17baae6245f.pack
    ./objects/pack/pack-4b53d6e5f9ff79534ccdcd9ebb2789e5c3a4683e.idx
    ./objects/pack/pack-1373667c7d1bf9de30d73e1f09a0bb9f23cbd9f9.idx
    ./objects/pack/pack-e7c3922a1425cbc19fed9ea92c85150beb252369.idx
    ./objects/pack/pack-062c5034c9acfe50c816849870c2e1ab531565bd.idx
    ./objects/pack/pack-9fc480ebaec9be0703a0c82717c4637e5a9a7ce9.idx
    ./objects/pack/pack-7f9032cd14e38a96995fc9da860f893be3dc21ae.pack
    ./objects/pack/pack-1ee5fab38c619e40afe8c597f13d2f6f300e8896.pack
    ./objects/pack/pack-bf35c52df3235196d180e4942418722ebce63a6e.idx
    ./objects/pack/pack-c9008c3be44f8aee531f5e9b21ca893bd7001064.idx
    ./objects/pack/pack-6aa1c680f6c1be9a576e691aaf2bcda90cdf4a59.idx
    ./objects/pack/pack-b1bcc8af31303fe1ffcdbea295921c89bdd5614e.pack
    ./objects/pack/pack-46270cc039ffca2eaf36e3a5dd1bc2919975d49c.idx
    ./objects/pack/pack-1e4415cfa550f8ef2b885b17db71dedae809b611.idx
    ./objects/pack/pack-c73924002b11aad49a745a5e9066ef7fbf7759ee.pack
    ./objects/pack/pack-8c7cf3ceb4eb6f387c638821729f458812e0f65e.idx
    ./objects/pack/pack-5b040b28302cc7fbafd6b91b80f3b0fce172b8fa.idx
    ./objects/pack/pack-6220af885123c3acdf5025c32a7cb6719ffc3bc2.idx
    ./objects/pack/pack-198b890d094f7fbbec3eaac7994d0521edef7869.pack
    ./objects/pack/pack-662b4a84f245da410a97543653b7f7759d80ac64.idx
    ./objects/pack/pack-baa3ed94579f2c9cf54c21b2bc74af926180b68f.pack
    ./objects/pack/pack-136d6b90b049cf734b65f4c6a0dd9e08f0f94158.pack
    ./objects/pack/pack-763963709c41b36fc09f89157264c8ba580bd970.idx
    ./objects/pack/pack-a622b31e73d238555a6249aa6eb6b19358effbbb.idx
    ./objects/pack/pack-efa991151347e785c33c5412690a322a424c1b39.idx
    ./objects/pack/pack-612565d2a489b4f39cc0394ec6544faff50e1e5a.idx
    ./objects/pack/pack-7596494ad82512f63acd7d5e6e5ab29154be8251.idx
    ./objects/pack/pack-d13aa70b8ff2ece90c79ed37229a3ec5fb5f3741.pack
    ./objects/pack/pack-ae89cdfa068a806bb17e759838b41274aee5679a.idx
    ./objects/pack/pack-391aec370b57735d4d752573290bc197ad58be33.idx
    ./objects/pack/pack-bdf0b0801cd4086194354c00b73752cc0f7c5323.pack
    ./objects/pack/pack-467e07f7ed8afaca6fc13eb3caf12a3a7db61a51.idx
    ./objects/pack/pack-21661c1fae0c6b942f6074c72381136b3329edfd.pack
    ./objects/pack/pack-ba7387535f871f68054de48547a3a72d88c296f1.idx
    ./objects/pack/pack-4f3ab42cbb6b4ee614956346ca0e2ab313f98c27.pack
    ./objects/pack/pack-33cac432df15cda7f2a022fe84b55e9e37d86f72.pack
    ./objects/pack/pack-2c1b2ec6308c6be11618e3dde12594f24119dc85.idx
    ./objects/pack/pack-adc5ecfd79179d291d75cfed503a831f60a1f8d8.idx
    ./objects/pack/pack-464b3c8e24a3077a64c2ac2ff29d4ed33c341475.idx
    ./objects/pack/pack-f90cde831ef2e65eb0f3e9f06f45ff766508da92.pack
    ./objects/pack/pack-1ee5fab38c619e40afe8c597f13d2f6f300e8896.idx
    ./objects/pack/pack-3f82c7afbd3f8ad713ae656b50c4408bcd3c94aa.idx
    ./objects/pack/pack-1d00a3ae0c41a69b9c5478d0990cdd6a742e3c8a.pack
    ./objects/pack/pack-e77ebb37fedf0cc667af02a47bbc750f84dc5172.pack
    ./objects/pack/pack-e54c340bf35d055ccec288f018cdf601c8c0d768.pack
    ./objects/pack/pack-149ed4744c4bdd397d5eb61c5b01dcc80bba9299.pack
    ./objects/pack/pack-490426ca56e63589ad69bcc28031d579439f0e34.pack
    ./objects/pack/pack-7a4356fcb0213af3799cf65da539323eedc24f1e.idx
    ./objects/pack/pack-bd77a2a949373126dd29d9cb90673ef0245fc22e.idx
    ./objects/pack/pack-6bb3deb0e4aac320755096238a1b479553f7a2c5.pack
    ./objects/pack/pack-8b2d98f7beb2ea766ff58eab03f63d2f61468a41.idx
    ./objects/pack/pack-ac2cc30c6904b6ca716bc3bdc352bf6e7ca254d5.pack
    ./objects/pack/pack-e448aa66b2b50b78fcd811f8f78af4b0817a82d3.idx
    ./objects/pack/pack-901919f5bfe29105348e681518986be932805876.pack
    ./objects/pack/pack-88be3f8fd17fa222ccd6ac1339305ac55a66b0df.pack
    ./objects/pack/pack-7d45de254874d12fea29f8227ff33211fec7611b.pack
    ./objects/pack/pack-a83824419e35824b0c04c772e7074de0f1d15240.pack
    ./objects/pack/pack-459ffed4b79e48b95e63792efda94c0ef52d03f7.idx
    ./objects/pack/pack-d0df188eb0ed4618ffe86960271eb1272bb3695f.pack
    ./objects/pack/pack-43ee3ed038b4a82aeed3961ac46c13749afe0de3.idx
    ./objects/pack/pack-0c0089c6c97bdac21302fd583668057e20b3b82b.pack
    ./objects/pack/pack-27b080cceb11f36b510530f76c34fa916a400479.idx
    ./objects/pack/pack-0324331b7664df56a0ffddd761db3f8620d56683.pack
    ./objects/pack/pack-8fa233cddcf81d49c108a641b6b57cd9cc430cc6.idx
    ./objects/pack/pack-700b8be366dd9924d4e128e7d81494753c141ffd.pack
    ./objects/pack/pack-16a87266a2a26cc12006b6b7ec4bcc2ac86c998e.idx
    ./objects/pack/pack-737cf3d669be50862ffa0bc9e8133a96933843c3.idx
    ./objects/pack/pack-0324331b7664df56a0ffddd761db3f8620d56683.idx
    ./objects/pack/pack-3e0be112b08ba493a159588cb7f1c25d0cb26202.pack
    ./objects/pack/pack-a050bda29401c174b597686559ce1ce0c7f0c100.idx
    ./objects/pack/pack-64448e9bf62caf05956c25d28b89cdd078633942.pack
    ./objects/pack/pack-5914edb2e6b381b0587b4b5fb9c4f6430356f717.pack
    ./objects/pack/pack-2b9bf59186b8a2ab28c1f7624c68d04e88847d08.pack
    ./objects/pack/pack-d192e2a6de88299d744e05044cfdb50fbd49ddb9.pack
    ./objects/pack/pack-b1bcc8af31303fe1ffcdbea295921c89bdd5614e.idx
    ./objects/pack/pack-69441f3f9aa6593f4abe9d26ae49b05e72ae92e4.idx
    ./objects/pack/pack-43b39922770761c0f92d8e4d4c3b5b692ffca6df.pack
    ./objects/pack/pack-7e047f5b721997b810aa8bdadbeee46a87df0939.idx
    ./objects/pack/pack-e670a012d4f75eda7dffd34b3646cd8ea1ff3be9.idx
    ./objects/pack/pack-8eb5dda426b66a436327e1bee1824db0c7cf36be.idx
    ./objects/pack/pack-162004663b39b804fec935640195d69d3a88dd86.pack
    ./objects/pack/pack-8c61e16d34a28319ac1716718cdbce0b27ae6a61.pack
    ./objects/pack/pack-cd7d72892a2d131fec2c01f372747482d48eb362.pack

    gzip: stdin: unexpected end of file
    tar: Unexpected EOF in archive
    tar: Unexpected EOF in archive
    tar: Error is not recoverable: exiting now
    alibivmuser@arun:~/npci/vnl/git-down-linux$ ls
    branches config description FETCH_HEAD gc.log.lock git2_git.ti.com.ti-linux-kernel.ti-linux-kernel.git.tar.gz HEAD hooks objects packed-refs
    alibivmuser@arun:~/npci/vnl/git-down-linux$
    alibivmuser@arun:~/npci/vnl/git-down-linux$ axel -va software-dl.ti.com/.../git2_git.ti.com.ti-linux-kernel.ti-linux-kernel.git.tar.gz

  • Hi,

    Can you try the following:
    1. download and install the SDK from this link:
    software-dl.ti.com/.../index_FDS.html
    use ti-processor-sdk-linux-k2e-evm-04.01.00.06-Linux-x86-Install.bin.
    2. Once you setup the sdk execute the following steps:
    cd ~/ti-processor-sdk-linux-k2e-evm-04.01.00.06
    git clone git://arago-project.org/git/projects/oe-layersetup.git tisdk
    cd tisdk
    ./oe-layertool-setup.sh -f configs/processor-sdk/processor-sdk-04.01.00.06-config.txt
    cd build
    . conf/setenv
    export PATH=~/ti-processor-sdk-linux-k2e-evm-04.01.00.06/linux-devkit/sysroots/x86_64-arago-linux/usr/bin:$PATH
    MACHINE=k2e-evm bitbake tisdk-rootfs-image

    Best Regards,
    Yordan
  • Hi Yordan, 

    I did the suggested step but its give me error like 

    gzip: stdin: unexpected end of file
    tar: Unexpected EOF in archive
    tar: Unexpected EOF in archive
    tar: Error is not recoverable: exiting now

                 then 

    i try to open the tar (tar -xvf git2_git.ti.com.ti-linux-kernel.ti-linux-kernel.git.tar.gz ) file manually 

                then again i got the same error like  

    gzip: stdin: unexpected end of file
    tar: Unexpected EOF in archive
    tar: Unexpected EOF in archive
    tar: Error is not recoverable: exiting now

                then

    I try to verify the size of file listed on web and the downloaded one and its the size is different 

    Regards,

    Arun 

  • Arun,

    At which point do you get this errors? Running the above steps does not require the downloading of any archive...

    Best Regards,
    Yordan