This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TDA2EXEVM: Try to Load .elf file on Cortex A15 of TDA2EX

Part Number: TDA2EXEVM

Tool/software: Code Composer Studio

Hi,

On TDA2EX board First we work on IPU2 processor, For that in Linker file we use the address

MEMORY
{
   IPU_RAM: org = 0x00000000 len = 0x3000 
   DDR3_IPU2: org = 0x83f00000 len = 0x9FD000

}

Its working Fine. .elf get loaded properly and executed properly

For A15 i changed DDR3_IPU2 address to 0x402f0000 

Now i want to load same code for A15, Connect the Target A15 then run the script to enable the PRCM module same did for IPU2, but when i try to load same elf i get the following error

CortexA15_0: File Loader: Verification failed: Values at address 0x00000000 do not match Please verify target memory and memory map.
CortexA15_0: GEL: File: D:\TDA2EX_FICOSA_WS\001_Os_UNIPHASE_ARM\04_Testing\01_Em\Test_App_TDA2EX\App_Os_AlarmandCounters\obj\App_Os_AlarmandCounters.elf: a data verification error occurred, file load failed.
CortexA15_0: Unable to terminate memory download: NULL buffer pointer at 0x3aa4

Please suggest If their is any changes in Linker File or Compiler Flag or Linker Flag  to load the elf on A15

Following Compiler Flag used

CCFLAGS= --silicon_version=7M4 --abi=eabi

Thanks,

Harshalkumar Shinde