This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA3XEVM: Why IR1443 ES2.0 EVM can not be connected to TDA3x EVM

Part Number: TDA3XEVM

Hi champion,
   I am running the processor SDK radar 3.2.0.0 applicaiton on TDA3x EVM with DIB, VAB and radar EVM. I find a that the application can run with AR1443 ES1.0 EVM, but can not run with IR1443 ES2.0 EVM.  When the IR1443 ES2.0 EVM connected, the radar initializaiton can not pass. Below is the log.

IPU1-0]  Enter Choice:
[IPU1-0]
[IPU1-0]   1406.545720 s:
[IPU1-0]   1406.545812 s:  CHAINS: Init AR12xx ...
[IPU1-0]   1406.546117 s:  UTILS_MCSPI: McSPI is configured in interrupt mode!!

  I don't know potential difference between ES1.0 and 2.0 for 1443 which can cause this issue. Could you help to check?

Thanks,
Adam