This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[TDA2x EVM] Can't connect to USB UART

Hi,

I have a TDA2x EVM board like so: 

I have flashed the boot and filesystem partitions onto the SD card as per instructions in Vision SDK Linux User Guide.

After that I inserted the micro SD card into the board, set SYSBOOT pin configuration as: 11100000 10000001

Now when I power on and press the Power reset button, I expect some log messages on UART terminal.

However, I don't see any /dev/ttyUSB* entry in /dev

Am I missing some other settings or mistaken in some step? Please help me out here.

Thanks,

Bhargav