Part Number: TMS320C6748
Other Parts Discussed in Thread: OMAP-L138, AM1808, SYSBIOS, OMAPL138
Got below/attached question:
am trying to use the TI example for MMCSD on the C6748 LCDK. With a kingston mmc chip
The example fails in the attached function underlined in yellow, (inside ff.c file)
Attached is the whole project
Need your help
BYTE check_fs ( /* 0:The FAT BR, 1:Valid BR but not an FAT, 2:Not a BR, 3:Disk error */
FATFS *fs, /* File system object */
DWORD sect /* Sector# (lba) to check if it is an FAT boot record or not */
)
{
if (disk_read(fs->drv, fs->win, sect, 1) != RES_OK) /* Load boot record */
return 3;
if (LD_WORD(&fs->win[BS_55AA]) != 0xAA55) /* Check record signature (always placed at offset 510 even if the sector size is >512) */
return 2;
if ((LD_DWORD(&fs->win[BS_FilSysType]) & 0xFFFFFF) == 0x544146) /* Check "FAT" string */
return 0;
if ((LD_DWORD(&fs->win[BS_FilSysType32]) & 0xFFFFFF) == 0x544146)
return 0;
return 1;