Part Number: TMS320C6746
Hello,
- We are planning to use the C6746 DSP on a new board and I was wondering if there are any caveats to using different power rails for the different power groups. Specifically, I would like to use 2.75V for Power Group A (because of a UART requirement) but use 3.3V for the rest of the device. Is this a problem? Is there a power sequencing requirement if we use different rails for the different power groups?
- Looking at the power on sequencing (§5.3.1) of the datasheet, it seems that the only valid voltages for the IO supply groups are 1.8V and 3.3V. Can you confirm this is the case?
- Is there any work around that can enable use of a 2.75V rail?
Best,
Nadeem