Moreover, whenever I try to connect the clock (MCASP1_ACLKR (Bit Clock) - P9_42) with my oscilloscope, I don't see any pulses. Looks like there is no proper clock signal on this pin. What can I do to debug, and fix this?
Any ideas?
Parag
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Linux
I am trying to interface an I2S microphone (https://www.adafruit.com/product/3421) with BeagleBone Black. I followed the article (http://www.ti.com/lit/an/sprac97/sprac97.pdf), and able to update the device tree, and the Linux kernel as suggested in the article.
The I2S component (for microphone) of the device tree is included as a dtsi in the main device tree source. The content of the dtsi is as below
&am33xx_pinmux {
mcasp1_pins: mcasp1_pins {
pinctrl-single,pins = <
/* sink must enable receivers */
0x1a0 0x23
/* P9_42 mcasp1_aclkx - bit clock */
0x1a4 0x23
/* P9_27 mcasp1_fsx - frame sync */
0x1a8 0x23
/* P9_41 mcasp1_axr0 - i2s input */
>;
};
};
&mcasp1 {
#sound-dai-cells = <0>;
pinctrl-names = "default";
pinctrl-0 = <&mcasp1_pins>;
status = "okay";
op-mode = <0>;
tdm-slots = <2>;
num-serializer = <4>;
serial-dir = < /* 1 TX 2 RX 0 unused */
2 0 0 0
>;
rx-num-evt = <1>;
tx-num-evt = <1>;
};
/ {
pcm5102a: pcm5102a {
#sound-dai-cells = <0>;
compatible = "ti,pcm5102a";
status = "okay";
};
sound1: sound@1 {
compatible = "simple-audio-card";
simple-audio-card,name = "PCM5102a";
simple-audio-card,format = "i2s";
simple-audio-card,bitclock-master = <&sound1_master>;
simple-audio-card,frame-master = <&sound1_master>;
simple-audio-card,bitclock-inversion;
simple-audio-card,cpu {
sound-dai = <&mcasp1>;
};
sound1_master: simple-audio-card,codec {
#sound-dai-cells = <0>;
sound-dai = <&pcm5102a>;
clocks = <&mcasp1_fck>;
clock-names = "mclk";
};
};
};
I have also compiled the kernel with a new driver pcm5102 as suggested in the document. Finally, I see the driver listed in the output of the arecord command.
root@arm:/sys/class/gpio# arecord -l **** List of CAPTURE Hardware Devices **** card 0: PCM5102a [PCM5102a], device 0: davinci-mcasp.0-pcm5102a-hifi pcm5102a-hifi-0 [] Subdevices: 1/1 Subdevice #0: subdevice #0
However whenever I try to record audio, I am not getting any audio data. The audio file is formed, but the file size is always 44 bytes irrespective of how long I try to record audio for. Clearly no data is there in the file.
Recording using arecord command gives error as below
arecord -d 10 -Dhw:0,0 -f dat audio.wav Recording WAVE 'audio.wav' : Signed 16 bit Little Endian, Rate 48000 Hz, Stereo arecord: pcm_read:2032: read error: Input/output error
Moreover, whenever I try to connect the clock (MCASP1_ACLKR (Bit Clock) - P9_42) with my oscilloscope, I don't see any pulses. Looks like there is no proper clock signal on this pin. What can I do to debug, and fix this?
Any ideas?
Parag
Same result. I had already removed the following from the codec component of simple-audio-card from the device tree.
- clocks = <&mcasp1_fck>;
- clock-names = "mclk";
The signals on framesync, bitclock, data as as follows.
Frame rate: 46.9 KHz
BitClock rate: 1.5 MHz
Data: 32.76 KHz (even when not recording or playing anything!!! It varies between 32.76 to 32.78 KHz when recording)
Recorded sound is continuous shrill noise as earlier.
Parag Sharma said:The signals on framesync, bitclock, data as as follows.
Frame rate: 46.9 KHz
BitClock rate: 1.5 MHz
We should have 48KHz for FS and 1.536MHz for bclk. This might be the an issue. You can check what FS/bclk values you have in Raspberry Pi and compare with these here. You can also check what FS/bclk values you have on AM335x TI board (EVM or StarterKit) and compare with these here.
Also in the link you sent we have "The I2S is a small, low cost MEMS mic with a range of about 50Hz - 15KHz, good for just about all general audio recording/detection." Does this mean that max FS supported is 15KHz, while you are providing 46.9KHz?
Parag Sharma said:Data: 32.76 KHz (even when not recording or playing anything!!! It varies between 32.76 to 32.78 KHz when recording)
Recorded sound is continuous shrill noise as earlier.
This does not looks correct. There should be no audio data on data pin when there are no FS/Bclk signals. This might be HW malfunction. Can you try with playback mode only, what do you observe on FS/bclk/data pins in playback mode?
Regards,
Pavel
Hi Pavel,
Thanks for your pointers. I finally figured out the reason why the data pin (MCASP1_AXR0) always had some signal even when not recording/playing. Beaglebone DTS (am335x-bone-common.dts) has a setting for clkout2_pins which was setting clock to the same pin (P9_41). The moment I commented this, everything started working as expected.
I was finally able to record sound using my i2s microphone and BeagleBone black.
Amazing 3 months effort, but worth it every bit. I learnt so much. Thank you so much Pavel.