Hi
I am having a problem running the DM6437 out of DDR. My problem can be recreated with the following steps:
Code Composer Studio Version: 4.1.3.00038
Updated with latest patches.
1. Create a new CCS project (i.e. - test). No reference project.
Device Variant: Generic C64x+ Device
Device Endianness: little
Code Generation tools: TI v7.0.4
Runtime Support Library: <automatic>
Use DSP/BIOS v5.xx: 5.41.02.14
2. Create a empty main.c (i.e. - void main (void) {}
Add file to project
3. Under new tab - Create a NewTargetConfiguration.ccxml
Set to: Texas Instruments XDS100v2 USB Emulator
TMS320TCI6482
Under Advanced Tab: Set init script to evmdm6437.gel
4. Under new tab - Create a DSP/BIOS Configuration TCF file
filter 6437
Select: ti.platforms.evmDM6437
5. Build and debug project
project halts at main with no issues
6. Open TCF configuration tool
Open MEM - Memory Section Management Properties
Under BIOS Data tab, BIOS Code tab, Compiler Sections tab - change all from IRAM to DDR2
Save and close tool
7. Build and debug project
Project hangs never reaching main()
I would appreciate any help I can get on this issue.
Regards,
Thomas