Tool/software: Linux
Hello, I trying to compile qtwebengine, But it failed.
| {standard input}: Assembler messag es:
| {standard input}:93127: Warning: end of file not at end of a line; newline inserted
| {standard input}: Error: open CFI at the end of file; missing .cfi_endproc directive
| arm-linux-gnueabihf-g++: internal compiler error: Killed (program cc1plus)
| Please submit a full bug report,
| with preprocessed source if appropriate.
| See <https://bugs.linaro.org> for instructions.
| ninja: build stopped: subcommand failed.
| Makefile.gyp_run:357: recipe for target 'invoke_ninja' failed
| make[3]: *** [invoke_ninja] Error 1
| make[3]: Leaving directory '/home/llr/oe/tisdk-am57xx-v3.01/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/qtwebengine/5.6.0+gitAUTOINC+643aa579fc_8252b18aa3-r0.tisdk0/git/src/core'
| Makefile:116: recipe for target 'sub-gyp_run-pro-make_first' failed
| make[2]: *** [sub-gyp_run-pro-make_first] Error 2
| make[2]: Leaving directory '/home/llr/oe/tisdk-am57xx-v3.01/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/qtwebengine/5.6.0+gitAUTOINC+643aa579fc_8252b18aa3-r0.tisdk0/git/src/core'
| Makefile:49: recipe for target 'sub-core-make_first' failed
| make[1]: *** [sub-core-make_first] Error 2
| make[1]: Leaving directory '/home/llr/oe/tisdk-am57xx-v3.01/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/qtwebengine/5.6.0+gitAUTOINC+643aa579fc_8252b18aa3-r0.tisdk0/git/src'
| Makefile:44: recipe for target 'sub-src-make_first' failed
| make: *** [sub-src-make_first] Error 2
| ERROR: oe_runmake failed
| ERROR: Function failed: do_compile (log file is located at /home/llr/oe/tisdk-am57xx-v3.01/build/arago-tmp-external-linaro-toolchain/work/armv7ahf-neon-linux-gnueabi/qtwebengine/5.6.0+gitAUTOINC+643aa579fc_8252b18aa3-r0.tisdk0/temp/log.do_compile.1339)
ERROR: Task 8 (/home/llr/oe/tisdk-am57xx-v3.01/sources/meta-qt5/recipes-qt/qt5/qtwebengine_git.bb, do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 1612 tasks of which 1606 didn't need to be rerun and 1 failed