Other Parts Discussed in Thread: TUSB8041
Tool/software: Linux
For AM5728 Sitara processor for design, where no SD card interface is given; I have 2 queries:
1)Is it possible for usb-boot of AM5728 evenif USB Hub IC:TUSB8041 is present on the path between AM5728 processor and USB connectors?? (The schematics of USB section is same as in AM5728 EVM.)
2)Once boot files are transferred to EVM board via UART to DDR3, what is the procedure to move them to eMMC so that further on power-on of board, it can boot via eMMC ; once eMMC boot pins are configured??