Part Number: AM5726
Tool/software: Linux
In the event that I have an AM5726 SR2.0 with SYSBOOT[15] set to 0, are the following 2 statements correct?
• the Software Workaround mentioned in the Errata i863 documentation is effectively implemented in u-boot-spl when the active pad_conf_entry array in board/ti/am57xx/mux_data.h contains GPMC_A19, GPMC_A20, GPMC_A21, GMPC_A22, GMPC_A24, GMPC_A25, GMPC_A26, GMPC_A27 configured with (M1 | PIN_INPUT_PULLUP)
• if the aforementioned u-boot-spl is not executed (and no other secondary boot loader is executed), then after a CPU reset the eMMC DAT terminals will be in the PU/PD contention state