Part Number: AM4379
Tool/software: TI-RTOS
Hi,
I am using IDK am4379 as ethercat slave and TwinCAT as master. I added two Objects in xml and header file and mapped to RxPDO and TxPDO respectively. When I am trying to start the network , following errors are coming.
Error 1 02-07-2018 12:10:07 429 ms | 'Box 1 (TIESC-002)' (1001): 'SAFEOP to OP' failed! Error: 'check device state for OP'. AL Status '0x0004' read and '0x0008' expected.
Error 2 02-07-2018 12:10:07 429 ms | 'Box 1 (TIESC-002)' (1001): state change aborted (requested 'OP', back to 'SAFEOP').
Error 3 02-07-2018 12:10:09 203 ms | 'Box 1 (TIESC-002)' (1001): abnormal state change (from 'SAFEOP' to 'OP'). Try to go back to 'OP'...
Can you help me to solve these issues.
Regards,
Vishnu