Part Number: TMS320C6746
Other Parts Discussed in Thread: OMAP-L138
I am wondering if I am free to write my own BIOS for the TMS320C6746 VLIW DSP as it may be going into my own DSO (digital storage oscilloscope) design for analysis of ADC data and / or communication protocol decoding via the logic analyzer port(s). Or am I restricted to using TI's proprietary bootloader blobs (TI-DSP BIOS)?
Open-source option would be nice as I may be using customized uCLinux (Microcontroller Linux) on a 600MHz Cortex M7 microcontroller to handle collection of processed ADC data to display via the on-die 2D GPU (DSP and microcontroller are interfaced via USB on the printed circuit board).
Lastly, would anyone recommend a good switchmode CPU voltage regulator for that DSP, as I may be running off Lithium Iron Phosphate battery pack.