This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/AM5728: Eth1 connection issue

Part Number: AM5728

Tool/software: TI-RTOS

Hello,

My board is evmAM5728.I use the example of NIMU_BasicExample_evmAM572x_c66xExampleProject about RTOS.

Now I want to use the  eth0 and eth1,but the example can only ping the eth0 correctly.

1. I can correctly link to eth0 and eth1

2.when I link to eth0  ,ping coorectly

but link to eth1,ping wrong

3.I want to use eth0 and eth1 at the same time,but I find only one IP (192.168.1.2)

how can I set tow ip for eth0 and eth1?

4.when I choose the obtion IP address automatically, I can get a IP (192.168.1.102) linking to eth0.ping correctly

But when I link to eth1 ,I cannot get a IP.  Why?

So I think the configuration about eth is correct.

the configuration about IP have problems.

Can you gei me some advices?