Tool/software: Linux
Software: Ti's SDK ti-processor-sdk-linux-am57xx-evm-04.00.00.04-Linux-x86-Install.bin
Hardware: customer board with a generally USB touchscreen panel
The touchscreen can works with matrixbox GUI but when start the dual-camera demo it can not works.
We can only use mouse to exit dual-camera demo.
It seems dual-camera demo is a independent test program based on QT but it has no dependance with weston. is that right?
How to let touchscreen work with dual-camera demo.