Tool/software: Linux
Customer wants to use boot from eMMC. Our Userguide has two partitions in the UDA, the FAT32 and the Linux partition, which are the boot partition and the rootfs partition respectively.
- The eMMC mode of Only UDA(FAT/linux ), whether it can be used as a mass production method? If the eMMC has bad blocks, what effect does it have on the system?
- The eMMC mode of Boot + UDA, Whether it can be used as a mass production method, can you provide more details?
- The above two methods, what are our considerations, which method do we recommend to our customers?
Looking forward to your guidance.
Appreciate and thanks.
Best Regards
Fredy