This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: Duty cycle of GPMC_CLK

Guru 15520 points

Part Number: AM5728

Hi,

I have questions about AM5728 GPMC.

Q1.
I want to know the duty cycle of GPMC_CLK.
In AM5728 Technical Reference Manual(spruhz6j) page.3561"15.4.4.9.6 GPMC_CLK",
it said as follow:
//////////////////////////////////////////////////////
The GPMC_CLK clock frequency is the GPMC_FCLK functional clock frequency divided by 1, 2, 3, or
4, depending on the GPMC_CONFIG1_i[1:0] GPMCFCLKDIVIDER bit field (where i = 0 to 7), with a
guaranteed 50-percent duty cycle. For information about the duty cycle error, see the device data
manual.
///////////////////////////////////////////////////////

It seems that 50% duty cycle are guaranteed for GPMC_CLK.
Is it guaranteed regardless of GPMC_FCLK division ratio etc?

By the way, I couldn't find the information about the duty cycle error in the data manual.
Does it mean that there are no duty cycle error?

best regards,
g.f.