This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unable to debug DSP1 with prebuilt image from processor sdk linux am57x 05_01_00_11.

Other Parts Discussed in Thread: BEAGLEBOARD-X15

Hi!

I'm using MLO, u-boot.img and arago-base-tisdk-image-am57xx-evm.tar.xz from ti-processor-sdk-linux-am57xx-evm-05.01.00.11 on board BeagleBoard-X15 REVC. I'm able to start the board, launch Target Configuration for Device AM5276 using CCS (XDS200 USB debugger) and connect to the ARM cores but when I try connecting to the DSP1 core I get the error:


Error connecting to the target:

(Error -6305) PRSC module failed to write to a router register.
(Emulation package 8.0.27.9)

Keep in mind that I try to connect to the ARM cores just to test the debugger and target configuration file.

CCS version: Version: 8.1.0.00011

Is this issue know to you?
Any ideas if I’m missing something?

Regards,
Enver