This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/DRA74: Ducati error when plan a mov file

Part Number: DRA74

Tool/software: Linux

Hi Team,

We use custom h/w and software based on DRA746 and SDK 3.02.00.03.

when we plan a mov file, there are some ducati error, as below:

23010 2018/11/20 16:17:56.000000 5952.2142 153 ECU1 CrM API 2866 log info verbose 1 T8023 GSTLogs WARN ducati gstducatividdec.c(570):codec_process:<decoder> err=-1, extendedError=80000201
23011 2018/11/20 16:17:56.000000 5952.2143 154 ECU1 CrM API 2866 log info verbose 1 T8023 GSTLogs ERROR ducati gstducati.c(61):gst_ducati_log_extended_error_info: Bit 0 (00000001): no error-free slice
23012 2018/11/20 16:17:56.000000 5952.2144 155 ECU1 CrM API 2866 log info verbose 1 T8023 GSTLogs ERROR ducati gstducati.c(61):gst_ducati_log_extended_error_info: Bit 9 (00000200): applied concealment
23013 2018/11/20 16:17:56.000000 5952.2144 156 ECU1 CrM API 2866 log info verbose 1 T8023 GSTLogs ERROR ducati gstducati.c(61):gst_ducati_log_extended_error_info: Bit 31 (80000000): gap in frame num
23018 2018/11/20 16:17:56.000000 5952.2203 157 ECU1 CrM API 2866 log info verbose 1 T8023 GSTLogs WARN ducati gstducatividdec.c(570):codec_process:<decoder> err=-1, extendedError=00000200
23019 2018/11/20 16:17:56.000000 5952.2204 158 ECU1 CrM API 2866 log info verbose 1 T8023 GSTLogs ERROR ducati gstducati.c(61):gst_ducati_log_extended_error_info: Bit 9 (00000200): applied concealment

I attach the log:7801.errorLog.txt

please download the video file from below link:

thanks a lot.

Regards,

Lingrong