This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6713B: Can the two inputs ports (Linein and Micin) work simultaneously

Part Number: TMS320C6713B

Hello everyone,

now I am working with TMS320C6713, trying to achive a scenario of ANC, but I am not sure wether the two inputs ports on the board can work simultaneously?

I have tried in Simulink to build a model to use both of the two input ports, but the Simulink allows to use only one ADC source, which you can only set for Linein or Micin.

By the way, I am using the Matlab2007b and the CCS3.3, my question is can I use the two inputs ports (Line in & Mic in) at the same time? If I can, how to achive it in Simulink?

best regards

Johnny