This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3517: EBOOT not sending BOOTME broadcasts

Part Number: AM3517

I am not having any success trying to connect the VS2008 debugger to my WEC7 device.

I am not seeing any BOOTME traffic coming from the AM3517.  Is there some EBOOT option that will enable/disable the BOOTME broadcast?  (I am not finding it)

I can successfully ping the device.

I can run the remote tools on the device (ActiveSync).

EBOOT settings:

Boot device: internal EMAC

Debug device: Internal EMAC

KITL state: enabled

The CE device is always booting the FLASH NK image.  Even though the boot settings are saying to boot from Enet.

Why can't I get the CE device to send BOOTME's?