This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA2: EVE application code does not execute on board

Part Number: TDA2

Hi,

I have created an application that should run on EVE. When I execute this application on EVE Simulator (ccs v5 Vayu simulator), it runs correctly and generates expected output. But when I try to run the same application on TDA2x board via emulator (ccs v7), it gets stuck at one point. I have some other applications, which run seamlessly through both simulator and emulator, so does not seem to be hardware issue.

What are the differences between simulator and emulator environment? Is there anything in the code that needs to be changed or configured? 

Regards,

Shruti

  • Hi Shruti,

    If it works on the simulator then generally it should work on the emulator. Where did it get stuck ? Please make sure you follow all the instructions in paragraph 3.6 of the eve_sw_getting_started.pdf of the EVE sw release, especially set EVE_SW_CONFIG macro to 1 in TDA2xx_multicore_reset.gel file.

    regards,

    Victor

  • Hi Victor,

    The code works fine with the simulator. But when I run it onto the board, it gets stuck after one block of BAM execution. Can you help me figure out the problem? I tried adding the code one by one. There is a lookup table implemented in the function, and when I comment the lookup table loop, the code runs on the board. It is a simple lookup table similar to the ones given in TIs examples. The same lookup table works with another application correctly. Can this be some illegal memory access issue? or some configurational issue?

    Regards,
    Shruti
  • Hi Shruti,

    You said it gets stuck. If you halt the CPU, where the program counter points to ? Or is the ARP32 crashed and you cannot even reconnect to it ?
    If it crashed, it could be that that the VCOP error register got set and if you don't clear the error bit, before VCOP is ran again, it will cause ARP32 to disconnect. You can monitor the state of the vcop_error register by selecting the Code Composer menu View->Register and click on VCOP_Status_Registers. if any bits of the vcop_error register is set, you need to clear it by writing the same value again. If you don't do that, next time, VCOP is executed, ARP32 will disconnect. Please refer to the EVE programmer's guide section 9.3 for meaning of the vcop_register's fields.

    regards,

    Victor