Part Number: TMS320C6416T
Hi all experts:
I have met two questions During Debugging DSP C6416, one about C6416 Power on boot failed occasionally,another about C6416 GPIO Pin
question 1:
when C6416 boot failed, using emulator save Local memory form address 0x0 to 0x400 Data, when C6416 boot success,also save Local memory from address 0x0 to 0x400 Data.
analysing failed and successful two grouops length 0x400 byte data, some datas different, What's the reason it cause to the first boot loading the Local memory data error?
question 2:
During test DSP C6416 and FPGA interconnect gpio pin, when I configure C6416 gpio pin 8 、pin 9、 pin 10 output and pin 8、pin 9、pin 10 configure the same, GPIO8、GPIO9、GPIO10
output the same Frequence square-wave, FPGA can sample GPIO8、GPIO9 signal, but can not sample GPIO pin 10 signal, I also confirm hard circurt connect no problem, What's the reason it cause to gpio 10 no output signal, which whether related to chip ?