Part Number: 66AK2H12
Hi Champs,
We need use inside of C66 core XMC Mpax address extension function on the ARM core.
because, we would like to set C66 core program to difference memory space between physical and logic address.
physical : 0x0_B800_0000
logic : 0x6000_0000
However, according to this Table 8-1, it is not allow to from ARM to the XMC register.
We need set XMC-MPAX physical/logic exchange before executing C66x core program.
Do you have any idea ?