Other Parts Discussed in Thread: DRA744, DRA746
Tool/software: Linux
Our processor is DRA74X, with 3.02.00.03 SDK version.
We have DRA744 & DRA746, i want to use different DDR configuration for different CPU at u-boot phase. Currently, i have two ideas,
1. Use GPIO, since our custom board have different GPIO value for different CPU, so if i can detect GPIO level, it'll be helpful.
2. Read the CTRL_WKUP_STD_FUSE_DIE_ID_2 register to get base_pn value, which can distinguish between DRA744 & DRA746.
Right now, i try these two ways at board_ti_get_emif_size() function of evm.c at u-boot, but fail. So, how can i know CPU type at very beginning of u-boot phase?
Regards,
Shawn