This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TDA2EVM5777: Can't get kernel image, wrong image format for bootm

Part Number: TDA2EVM5777
Other Parts Discussed in Thread: TDA2

Tool/software: Linux

Hi,

I have successfully build the vsdk on the linux without any compilation or build error. However, following the guidelines in order to run the usecase on the tda2 built from linux, I made the bootable sd card and transferred the files into it. I ended with this error, I have no clue of solving this problem. Can anyone help me figure it out. Thank you.

With best regards,

H.M. Owais

  • Hi,

    here are a few things to check:
    - SYSBOOT pins are configured correctly as described in chapter "4.2 Preparing SD card & Boot" in VisionSDK_Linux_UserGuide.pdf
    - you have "fdtfile=dra7-evm-infoadas.dtb" in uenv.txt
    - at u-boot prompt you run following commands and retry:
    env default -fa
    saveenv

    Regards,
    Yordan
  • Hi Yordan,
    Thank you for your response. I have went through the procedure you suggested me. It reset to the default environment and saved it but the the problem is still there. I can't even go to the root. Is there anything else I can do to fix it?




    With best regards,
    H.M. Owais
  • Hi,

    can you copy the complete log from the beginning and post it here as text file?
    Also can you show the output of 'printenv' command at u-boot prompt?

    Regards,
    Yordan
  • U-Boot SPL 2016.05-00013-g3331a8a-dirty (Apr 10 2019 - 11:19:50)
    DRA752-GP ES2.0
    no pinctrl for hs200_1_8v
    no pinctrl for ddr_1_8v
    ** First descriptor is NOT a primary desc on 1:1 **
    Trying to boot from MMC1
    reading dra7-ipu2-fw.lzop
    spl_load_file_fat: error reading file dra7-ipu2-fw.lzop, err - -1
    spl: error reading image dra7-ipu2-fw.lzop, err - -1
    Error loading remotecore IPU2!,Continuing with boot ...
    reading dra7-dsp1-fw.lzop
    spl_load_file_fat: error reading file dra7-dsp1-fw.lzop, err - -1
    spl: error reading image dra7-dsp1-fw.lzop, err - -1
    Error loading remotecore DSP1!,Continuing with boot ...
    reading dra7-dsp2-fw.lzop
    spl_load_file_fat: error reading file dra7-dsp2-fw.lzop, err - -1
    spl: error reading image dra7-dsp2-fw.lzop, err - -1
    Error loading remotecore DSP2!,Continuing with boot ...
    reading dra7-ipu1-fw.lzop
    spl_load_file_fat: error reading file dra7-ipu1-fw.lzop, err - -1
    spl: error reading image dra7-ipu1-fw.lzop, err - -1
    Error loading remotecore IPU1!,Continuing with boot ...
    reading u-boot.img
    reading u-boot.img
    reading u-boot.img
    reading u-boot.img
    
    
    U-Boot 2016.05-00013-g3331a8a-dirty (Apr 10 2019 - 11:19:50 +0800)
    
    CPU  : DRA752-GP ES2.0
    Model: TI DRA742
    Board: DRA74x EVM REV H.0
    DRAM:  4 GiB
    MMC:   OMAP SD/MMC: 0, OMAP SD/MMC: 1
    ** First descriptor is NOT a primary desc on 1:1 **
    GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
    part_get_info_efi: *** ERROR: Invalid GPT ***
    GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
    part_get_info_efi: *** ERROR: Invalid Backup GPT ***
    ERROR: cannot find partition: 'userdata'
    
    at arch/arm/cpu/armv7/omap-common/utils.c:199/mmc_get_part_size()
    Warning: fastboot.userdata_size: unable to calc
    SCSI:  SATA link 0 timeout.
    AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
    flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
    scanning bus for devices...
    Found 0 device(s).
    Net:
    Warning: ethernet@48484000 using MAC address from ROM
    eth0: ethernet@48484000
    Hit any key to stop autoboot:  0
    ## Error: "board_findfdt" not defined
    switch to partitions #0, OK
    mmc0 is current device
    SD/MMC found on device 0
    reading boot.scr
    ** Unable to read file boot.scr **
    reading uEnv.txt
    173 bytes read in 7 ms (23.4 KiB/s)
    Loaded env from uEnv.txt
    Importing environment from mmc0 ...
    switch to partitions #0, OK
    mmc0 is current device
    SD/MMC found on device 0
    3553296 bytes read in 390 ms (8.7 MiB/s)
    ** File not found /boot/dra7-evm-infoadas.dtb **
    Booting from mmc0 ...
    Kernel image @ 0x82000000 [ 0x000000 - 0x363810 ]
    ERROR: Did not find a cmdline Flattened Device Tree
    Could not find a valid device tree
    ** First descriptor is NOT a primary desc on 1:1 **
    switch to partitions #0, OK
    mmc1(part 0) is current device
    ** First descriptor is NOT a primary desc on 1:1 **
    mmc - MMC sub system
    
    Usage:
    mmc info - display info of the current MMC device
    mmc read addr blk# cnt
    mmc write addr blk# cnt
    mmc erase blk# cnt
    mmc rescan
    mmc part - lists available partition on current mmc device
    mmc dev [dev] [part] - show or set current mmc device [partition]
    mmc list - lists available devices
    mmc hwpartition [args...] - does hardware partitioning
      arguments (sizes in 512-byte blocks):
        [user [enh start cnt] [wrrel {on|off}]] - sets user data area attributes
        [gp1|gp2|gp3|gp4 cnt [enh] [wrrel {on|off}]] - general purpose partition
        [check|set|complete] - mode, complete set partitioning completed
      WARNING: Partitioning is a write-once setting once it is set to complete.
      Power cycling is required to initialize partitions after set to complete.
    mmc bootbus dev boot_bus_width reset_boot_bus_width boot_mode
     - Set the BOOT_BUS_WIDTH field of the specified device
    mmc bootpart-resize <dev> <boot part size MB> <RPMB part size MB>
     - Change sizes of boot and RPMB partitions of specified device
    mmc partconf dev boot_ack boot_partition partition_access
     - Change the bits of the PARTITION_CONFIG field of the specified device
    mmc rst-function dev value
     - Change the RST_n_FUNCTION field of the specified device
       WARNING: This is a write-once field and 0 / 1 / 2 are the only valid values.
    mmc setdsr <value> - set DSR register value
    
    mmc - MMC sub system
    
    Usage:
    mmc info - display info of the current MMC device
    mmc read addr blk# cnt
    mmc write addr blk# cnt
    mmc erase blk# cnt
    mmc rescan
    mmc part - lists available partition on current mmc device
    mmc dev [dev] [part] - show or set current mmc device [partition]
    mmc list - lists available devices
    mmc hwpartition [args...] - does hardware partitioning
      arguments (sizes in 512-byte blocks):
        [user [enh start cnt] [wrrel {on|off}]] - sets user data area attributes
        [gp1|gp2|gp3|gp4 cnt [enh] [wrrel {on|off}]] - general purpose partition
        [check|set|complete] - mode, complete set partitioning completed
      WARNING: Partitioning is a write-once setting once it is set to complete.
      Power cycling is required to initialize partitions after set to complete.
    mmc bootbus dev boot_bus_width reset_boot_bus_width boot_mode
     - Set the BOOT_BUS_WIDTH field of the specified device
    mmc bootpart-resize <dev> <boot part size MB> <RPMB part size MB>
     - Change sizes of boot and RPMB partitions of specified device
    mmc partconf dev boot_ack boot_partition partition_access
     - Change the bits of the PARTITION_CONFIG field of the specified device
    mmc rst-function dev value
     - Change the RST_n_FUNCTION field of the specified device
       WARNING: This is a write-once field and 0 / 1 / 2 are the only valid values.
    mmc setdsr <value> - set DSR register value
    
    Booting from eMMC ...
    Wrong Image Format for bootm command
    ERROR: can't get kernel image!
    => env default -fa
    ## Resetting to default environment
    => saveenv
    Saving Environment to MMC...
    Writing to MMC(1)... done
    =>
    =>
    =>
    => root
    Unknown command 'root' - try 'help'
    => printenv
    arch=arm
    args_fit=setenv bootargs console=${console}
    args_mmc=run finduuid;setenv bootargs console=${console} ${optargs} root=PARTUUID=${uuid} rw rootfstype=${mmcrootfstype}
    baudrate=115200
    board=dra7xx
    board_name=dra7xx
    boot_fdt=try
    boot_fit=0
    boot_os=0
    bootargs=androidboot.serialno=${serial#}
    bootcmd=if test ${dofastboot} -eq 1; then echo Boot fastboot requested, resetting dofastboot ...;setenv dofastboot 0; saveenv;echo Booting into fastboot ...; fastboot 0; fi;if test ${boot_fit} -eq 1; then run update_to_fit;fi;run findfdt; run envboot; run mmcboot;run emmc_android_boot;
    bootdelay=2
    bootdir=/boot
    bootenvfile=uEnv.txt
    bootfile=zImage
    bootm_size=0x10000000
    bootpart=0:2
    bootscript=echo Running bootscript from mmc${mmcdev} ...; source ${loadaddr}
    console=ttyO0,115200n8
    cpu=armv7
    dfu_alt_info_emmc=rawemmc raw 0 3751936;boot part 1 1;rootfs part 1 2;MLO fat 1 1;MLO.raw raw 0x100 0x100;u-boot.img.raw raw 0x300 0x1000;u-env.raw raw 0x1300 0x200;spl-os-args.raw raw 0x1500 0x200;spl-os-image.raw raw 0x1700 0x6900;spl-os-args fat 1 1;spl-os-image fat 1 1;u-boot.img fat 1 1;uEnv.txt fat 1 1
    dfu_alt_info_mmc=boot part 0 1;rootfs part 0 2;MLO fat 0 1;MLO.raw raw 0x100 0x100;u-boot.img.raw raw 0x300 0x1000;u-env.raw raw 0x1300 0x200;spl-os-args.raw raw 0x1500 0x200;spl-os-image.raw raw 0x1700 0x6900;spl-os-args fat 0 1;spl-os-image fat 0 1;u-boot.img fat 0 1;uEnv.txt fat 0 1
    dfu_alt_info_qspi=MLO raw 0x0 0x040000;u-boot.img raw 0x040000 0x0100000;u-boot-spl-os raw 0x140000 0x080000;u-boot-env raw 0x1C0000 0x010000;u-boot-env.backup raw 0x1D0000 0x010000;kernel raw 0x1E0000 0x800000
    dfu_alt_info_ram=kernel ram 0x80200000 0x4000000;fdt ram 0x80f80000 0x80000;ramdisk ram 0x81000000 0x4000000
    dfu_bufsiz=0x10000
    dofastboot=0
    emmc_android_boot=setenv eval_bootargs setenv bootargs $bootargs; run eval_bootargs; setenv mmcdev 1; setenv fdt_part 3; setenv boot_part 9; if test $reboot_image = recovery; then setenv boot_part 8; setenv reboot_image boot; saveenv; fi;setenv machid fe6; mmc dev $mmcdev; mmc rescan; part start mmc ${mmcdev} ${fdt_part} fdt_start; part size mmc ${mmcdev} ${fdt_part} fdt_size; part start mmc ${mmcdev} ${boot_part} boot_start; part size mmc ${mmcdev} ${boot_part} boot_size; mmc read ${fdtaddr} ${fdt_start} ${fdt_size}; mmc read ${loadaddr} ${boot_start} ${boot_size}; echo Booting from eMMC ...; bootm $loadaddr $loadaddr $fdtaddr;
    envboot=mmc dev ${mmcdev}; if mmc rescan; then echo SD/MMC found on device ${mmcdev};if run loadbootscript; then run bootscript;else if run loadbootenv; then echo Loaded env from ${bootenvfile};run importbootenv;fi;if test -n $uenvcmd; then echo Running uenvcmd ...;run uenvcmd;fi;fi;fi;
    fdt_addr_r=0x88000000
    fdtaddr=0x88000000
    fdtfile=undefined
    findfdt=if test $board_name = omap5_uevm; then setenv fdtfile omap5-uevm.dtb; fi; if test $board_name = dra7xx; then setenv fdtfile dra7-evm.dtb; fi;if test $board_name = dra72x-revc; then setenv fdtfile dra72-evm-revc.dtb; fi;if test $board_name = dra72x; then setenv fdtfile dra72-evm.dtb; fi;if test $board_name = dra71x; then setenv fdtfile dra71-evm.dtb; fi;if test $board_name = dra76x; then setenv fdtfile dra76-evm.dtb; fi;if test $board_name = beagle_x15; then setenv fdtfile am57xx-beagle-x15.dtb; fi;if test $board_name = beagle_x15_revb1; then setenv fdtfile am57xx-beagle-x15-revb1.dtb; fi;if test $board_name = am57xx_evm; then setenv fdtfile am57xx-evm.dtb; fi;if test $board_name = am57xx_evm_reva3; then setenv fdtfile am57xx-evm-reva3.dtb; fi;if test $board_name = am572x_idk && test $idk_lcd = no; then setenv fdtfile am572x-idk.dtb; fi;if test $board_name = am572x_idk && test $idk_lcd = osd101t2045; then setenv fdtfile am572x-idk-lcd-osd.dtb; fi;if test $board_name = am572x_idk && test $idk_lcd = osd101t2587; then setenv fdtfile am572x-idk-lcd-osd101t2587.dtb; fi;if test $board_name = am571x_idk && test $idk_lcd = no; then setenv fdtfile am571x-idk.dtb; fi;if test $board_name = am571x_idk && test $idk_lcd = osd101t2045; then setenv fdtfile am571x-idk-lcd-osd.dtb; fi;if test $board_name = am571x_idk && test $idk_lcd = osd101t2587; then setenv fdtfile am571x-idk-lcd-osd101t2587.dtb; fi;if test $board_findfdt != undefined; then run board_findfdt; fi;if test $fdtfile = undefined; then echo WARNING: Could not determine device tree to use; fi;
    finduuid=part uuid mmc ${bootpart} uuid
    fit_bootfile=fitImage.itb
    fit_loadaddr=0x88000000
    importbootenv=echo Importing environment from mmc${mmcdev} ...; env import -t ${loadaddr} ${filesize}
    kernel_addr_r=0x82000000
    loadaddr=0x82000000
    loadbootenv=fatload mmc ${mmcdev} ${loadaddr} ${bootenvfile}
    loadbootscript=fatload mmc ${mmcdev} ${loadaddr} boot.scr
    loadfdt=load ${devtype} ${bootpart} ${fdtaddr} ${bootdir}/${fdtfile}
    loadfit=run args_fit; bootm ${loadaddr}#${fdtfile};
    loadimage=load mmc ${bootpart} ${loadaddr} ${bootdir}/${bootfile}
    mmcboot=if mmc dev ${mmcdev}; then setenv devtype mmc; if mmc rescan; then echo SD/MMC found on device ${mmcdev};if run loadimage; then run loadfdt; echo Booting from mmc${mmcdev} ...; run args_mmc; bootz ${loadaddr} - ${fdtaddr}; fi; fi; fi;
    mmcdev=0
    mmcloados=run args_mmc; if test ${boot_fdt} = yes || test ${boot_fdt} = try; then if run loadfdt; then bootz ${loadaddr} - ${fdtaddr}; else if test ${boot_fdt} = try; then bootz; else echo WARN: Cannot load the DT; fi; fi; else bootz; fi;
    mmcrootfstype=ext4 rootwait
    netargs=setenv bootargs console=${console} ${optargs} root=/dev/nfs nfsroot=${serverip}:${rootpath},${nfsopts} rw ip=dhcp
    netboot=echo Booting from network ...; setenv autoload no; dhcp; run netloadimage; run netloadfdt; run netargs; bootz ${loadaddr} - ${fdtaddr}
    netloadfdt=tftp ${fdtaddr} ${fdtfile}
    netloadimage=tftp ${loadaddr} ${bootfile}
    nfsopts=nolock
    partitions=uuid_disk=${uuid_gpt_disk};name=rootfs,start=2MiB,size=-,uuid=${uuid_gpt_rootfs}
    partitions_android=uuid_disk=${uuid_gpt_disk};name=xloader,start=128K,size=256K,uuid=${uuid_gpt_xloader};name=bootloader,size=2304K,uuid=${uuid_gpt_bootloader};name=environment,size=256K,uuid=${uuid_gpt_environment};name=misc,size=128K,uuid=${uuid_gpt_misc};name=reserved,size=384K,uuid=${uuid_gpt_reserved};name=efs,size=16M,uuid=${uuid_gpt_efs};name=crypto,size=16K,uuid=${uuid_gpt_crypto};name=recovery,size=30M,uuid=${uuid_gpt_recovery};name=boot,size=10M,uuid=${uuid_gpt_boot};name=system,size=768M,uuid=${uuid_gpt_system};name=vendor,size=256M,uuid=${uuid_gpt_vendor};name=cache,size=256M,uuid=${uuid_gpt_cache};name=ipu1,size=8M,uuid=${uuid_gpt_ipu1};name=ipu2,size=8M,uuid=${uuid_gpt_ipu2};name=dsp1,size=8M,uuid=${uuid_gpt_dsp1};name=dsp2,size=8M,uuid=${uuid_gpt_dsp2};name=userdata,size=-,uuid=${uuid_gpt_userdata}
    pxefile_addr_r=0x80100000
    ramdisk_addr_r=0x88080000
    rdaddr=0x88080000
    reboot_image=boot
    rootpath=/export/rootfs
    scriptaddr=0x80000000
    soc=omap5
    static_ip=${ipaddr}:${serverip}:${gatewayip}:${netmask}:${hostname}::off
    update_to_fit=setenv loadaddr ${fit_loadaddr}; setenv bootfile ${fit_bootfile}
    usbtty=cdc_acm
    vendor=ti
    vram=16M
    
    Environment size: 7102/131067 bytes
    =>
    
    
    Hi Yordan,

    Thank you for your quick reply, attached file contains the complete log. Thank you.

    With best regards,

    H.M. Owais

  • Hi,

    can you check if you have "dra7-evm-infoadas.dtb" in /boot directory on the 2nd partition of the SD card?

    Regards,
    Yordan
  • I have copied that file into that particular folder from the sdk boot folder, it has initialized the kernel but got stuck after several seconds. What possibly can be the reason of having these issues although I followed the userguide properly. I believe, there may be some other files are missing. Thank you.



    With best regards,
    H.M. Owais
  • Hi,

    the default DTBs for a particular build config are defined in vision_sdk/apps/configs/tda2xx_evm_linux_all/cfg.mk as:

    DEFAULT_DTB := dra7-evm-infoadas.dtb dra7-evm-infoadas-lcd-lg.dtb

    then "make linux_install" command should copy them from "ti_components/os_tools/linux/kernel/omap/arch/arm/boot/dts/" (the kernel source) to "ti_components/os_tools/linux/targetfs/boot/" (the rootfs) from where they should go to the SD card when it is created. I am not sure where could be the problem in your case.

    Can you copy dra7-evm-infoadas.dtb from "ti_components/os_tools/linux/kernel/omap/arch/arm/boot/dts/" to the /boot directory on the SD card and see if it works?

    Regards,
    Yordan
  • Hi,

    can you attach the log where the kernel stops?

    regards,
    Yordan
  • Hi Yordan,

    I repeated the procredure again, building from the beginning and checking that every file should be perfectly copied. Moreover, this time I copied prebuild binaries, tidsk given at the ti website. I successfully reached the root and tried to run the apps.out. However, when I run it, I can't see any  usecase main display to access demos instead I get this strange log which keeps on giving me attaching file to processing units. Can you check what's wrong with my system? I have attached the file which contains complete log.

    root@dra7xx-evm:/opt/vision_sdk# source ./vision_sdk_load.sh
    insmod: ERROR: could not insert module ./bin/memcache.ko: File exists
    insmod: ERROR: could not load module ./bin/cmemk.ko: No such file or directory
    mknod: /dev/memcache: File exists
    ./disableDssInterruptsOnA15.sh: line 11: COMMANDS: command not found
    ./disableDssInterruptsOnA15.sh: line 12: COMMANDS: command not found
    ./disableDssInterruptsOnA15.sh: line 13: COMMANDS: command not found
    ./disableDssInterruptsOnA15.sh: line 14: COMMANDS: command not found
    ./disableDssInterruptsOnA15.sh: line 15: COMMANDS: command not found
    ./disableDssInterruptsOnA15.sh: line 16: COMMANDS: command not found
    ./disableDssInterruptsOnA15.sh: line 17: COMMANDS: command not found
    ./disableDssInterruptsOnA15.sh: line 18: COMMANDS: command not found
    ./disableDssInterruptsOnA15.sh: line 19: COMMANDS: command not found
    updated  value is
    
    
    COMMANDS
    
            ### WARNING ###: use the following [read | write | set bit | clear bit | dump] commands at your own risk!
            No address check done, may generate:
              - bus error (invalid or not accessible <physical address>,
              - platform crash/hang (bad <value>).
    
                Read any OMAP memory address (register), given its <physical address> or <name> as listed in TRM.
    
                Write <value> at any OMAP memory address (register), given its <physical address> or <name> as listed in TRM.
    
                Set bit at <position> into any OMAP memory address (register), given its <physical address> or <name> as listed in TRM.
    
                Clear bit at <position> into any OMAP memory address (register), given its <physical address> or <name> as listed in TRM.
    
                Dump a range of OMAP memory addresses, from <start address> to <end address>.
                Note all addresses within given range must be valid and accessible.
    
            ### WARNING ###: use the following I2C [read | write] commands at your own risk!
            No address check done, may generate:
              - I2C bus error (invalid or not accessible <physical address>,
              - platform crash/hang (bad <value>).
    
                Read I2C register at address <addr> from I2C chip at <chip-addr> on I2C <bus>.
    
                Write <value> in I2C register at address <addr> from I2C chip at <chip-addr> on I2C <bus>.
    root@dra7xx-evm:/opt/vision_sdk# ./apps.out
     [HOST]  OSA: MEM: 0: Mapped 0xa0100000 to 0xb697f000 of size 0x00100000
     [HOST]  OSA: MEM: 1: Mapped 0x84203000 to 0xa3d7f000 of size 0x12c00000
     [HOST]  OSA: MEM: 2: Mapped 0xa0200000 to 0xa3cbf000 of size 0x00040000
     [HOST]  OSA: MEM: 3: Mapped 0xa02c0000 to 0xa3cff000 of size 0x00080000
     [HOST]  OSA: MEM: 4: Mapped 0x00000000 to 0x00000000 of size 0x00000000
     [HOST]  OSA: IPU1-0 Remote Log Shared Memory @ 0xa0200000
     [HOST]  OSA: HOST Remote Log Shared Memory @ 0xa024f140
     [HOST]  OSA: DSP1 Remote Log Shared Memory @ 0xa02769e0
     [HOST]  OSA: DSP2 Remote Log Shared Memory @ 0xa029e280
     [HOST]  OSA: EVE1 Remote Log Shared Memory @ 0xa02c5b20
     [HOST]  OSA: EVE2 Remote Log Shared Memory @ 0xa02ed3c0
     [HOST]  OSA: EVE3 Remote Log Shared Memory @ 0xa0314c60
     [HOST]  OSA: EVE4 Remote Log Shared Memory @ 0xa033c500
     [HOST]  OSA: IPU2 Remote Log Shared Memory @ 0xa0363da0
     [HOST] [IPU1-0]   1957.479259 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [IPU1-0]   1958.479289 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [IPU1-0]   1959.479320 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [IPU1-0]   1960.479350 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [IPU1-0]   1961.479381 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [IPU1-0]   1962.479411 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [IPU1-0]   1963.479442 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [IPU1-0]   1964.479442 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [HOST  ]   1964.546391 s:  SYSTEM: System A15 Init in progress !!!
     [HOST] [DSP1  ]   1957.570853 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP1  ]   1958.570883 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP1  ]   1959.570914 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP1  ]   1960.570944 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP1  ]   1961.570975 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP1  ]   1962.571005 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP1  ]   1963.571036 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP2  ]   1956.710852 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP2  ]   1957.710882 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP2  ]   1958.710882 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP2  ]   1959.710913 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP2  ]   1960.710943 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP2  ]   1961.710974 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP2  ]   1962.711004 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP2  ]   1963.711035 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP1  ]   1964.571066 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP2  ]   1964.711065 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [IPU1-0]   1965.479472 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP1  ]   1965.571066 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP2  ]   1965.711096 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [IPU1-0]   1966.479503 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP1  ]   1966.571097 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP2  ]   1966.711096 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [IPU1-0]   1967.479533 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP1  ]   1967.571127 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP2  ]   1967.711126 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [IPU1-0]   1968.479564 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP1  ]   1968.571158 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP2  ]   1968.711157 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [IPU1-0]   1969.479594 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP1  ]   1969.571188 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP2  ]   1969.711187 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [IPU1-0]   1970.479625 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP1  ]   1970.571219 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP2  ]   1970.711218 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [IPU1-0]   1971.479655 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP1  ]   1971.571249 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP2  ]   1971.711248 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [IPU1-0]   1972.479686 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP1  ]   1972.571280 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP2  ]   1972.711279 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [IPU1-0]   1973.479686 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP1  ]   1973.571280 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP2  ]   1973.711309 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [IPU1-0]   1974.479716 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP1  ]   1974.571310 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP2  ]   1974.711340 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [IPU1-0]   1975.479747 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP1  ]   1975.571341 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP2  ]   1975.711340 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [IPU1-0]   1976.479777 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP1  ]   1976.571371 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP2  ]   1976.711370 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [IPU1-0]   1977.479808 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP1  ]   1977.571402 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP2  ]   1977.711401 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [IPU1-0]   1978.479838 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP1  ]   1978.571432 s:  SYSTEM: Attaching to [IPU2] ...
     [HOST] [DSP2  ]   1978.711431 s:  SYSTEM: Attaching to [IPU2] ...
    
    

  • Hi Hafiz,

    as the original issue was resolved, can you close this thread and open a new one for the apps.out issue.
    It is useful to have separate threads for the different issues for the purpose of searching.

    Regards,
    Yordan