Part Number: AM3354
Other Parts Discussed in Thread: AM3352, TPS65910
Tool/software: Linux
Dear TI Team,
In our custom board, we are seeing below log prints even though we do not connect any hub to our USB1 port. Can you pls. tell us if there is any wrong configuration for our board?
Note: We tied ID pin to GND by default.
Log Snippet:
[ 18.056915] hub 1-0:1.0: USB hub found
[ 18.094326] hub 1-0:1.0: 1 port detected
[ 18.133148] am335x-phy-driver 47401b00.usb-phy: 47401b00.usb-phy supply vcc not found, using dummy regulator
[ 18.292167] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 18.356795] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2
[ 18.426202] hub 2-0:1.0: USB hub found
[ 18.471817] hub 2-0:1.0: 1 port detected
Logs:
switch to partitions #0, OK
mmc1(part 0) is current device
Scanning mmc 1:1...
switch to partitions #0, OK
mmc1(part 0) is current device
SD/MMC found on device 1
3858944 bytes read in 341 ms (10.8 MiB/s)
38203 bytes read in 12 ms (3 MiB/s)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8df15000, end 8df2153a ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.14.67-gd315a9bb00 (oe-user@oe-host) (gcc version 7.2.1 20171011 (Linaro GCC 7.2-2017.11)) #1 PREEMPT Sat Oct 6 03:26:15 UTC 2018
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] OF: fdt: Machine model: TI AM335x EVM-SK
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] cma: Reserved 48 MiB at 0x8a800000
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (sgx neon)
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 64960
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=PARTUUID=f4069e7b-01 rw rootfstype=ext4 rootwait
[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 197272K/262144K available (8192K kernel code, 318K rwdata, 2536K rodata, 1024K init, 275K bss, 15720K reserved, 49152K cma-reserved, 0K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xd0800000 - 0xff800000 ( 752 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0900000 (9184 kB)
[ 0.000000] .init : 0xc0c00000 - 0xc0d00000 (1024 kB)
[ 0.000000] .data : 0xc0d00000 - 0xc0d4fb08 ( 319 kB)
[ 0.000000] .bss : 0xc0d4fb08 - 0xc0d948a4 ( 276 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000020] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[ 0.000050] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[ 0.000065] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000298] timer_probe: no matching timers found
[ 0.000565] Console: colour dummy device 80x30
[ 0.000600] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000609] This ensures that you still see kernel messages. Please
[ 0.000617] update your kernel commandline.
[ 0.000654] Calibrating delay loop... 597.60 BogoMIPS (lpj=2988032)
[ 0.118723] pid_max: default: 32768 minimum: 301
[ 0.118966] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.118986] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.119972] CPU: Testing write buffer coherency: ok
[ 0.120900] Setting up static identity map for 0x80100000 - 0x80100060
[ 0.121107] Hierarchical SRCU implementation.
[ 0.121569] EFI services will not be available.
[ 0.123388] devtmpfs: initialized
[ 0.134132] random: get_random_u32 called from bucket_table_alloc+0x8c/0x1ac with crng_init=0
[ 0.134724] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.135100] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.135139] futex hash table entries: 256 (order: -1, 3072 bytes)
[ 0.139825] pinctrl core: initialized pinctrl subsystem
[ 0.140713] DMI not present or invalid.
[ 0.141220] NET: Registered protocol family 16
[ 0.144100] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.162633] omap_hwmod: debugss: _wait_target_disable failed
[ 0.217304] cpuidle: using governor ladder
[ 0.217352] cpuidle: using governor menu
[ 0.223303] OMAP GPIO hardware version 0.1
[ 0.238411] No ATAGs?
[ 0.238436] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.255988] edma 49000000.edma: TI EDMA DMA engine driver
[ 0.257414] reg-fixed-voltage fixedregulator2: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_wl12xx_gpio, deferring probe
[ 0.261429] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, deferring probe
[ 0.261622] media: Linux media interface: v0.10
[ 0.261679] Linux video capture interface: v2.00
[ 0.261818] pps_core: LinuxPPS API ver. 1 registered
[ 0.261831] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.261860] PTP clock support registered
[ 0.261906] EDAC MC: Ver: 3.0.0
[ 0.262492] dmi: Firmware registration failed.
[ 0.263032] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.263488] Advanced Linux Sound Architecture Driver Initialized.
[ 0.264942] clocksource: Switched to clocksource timer1
[ 0.276031] NET: Registered protocol family 2
[ 0.276970] TCP established hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.277017] TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.277054] TCP: Hash tables configured (established 2048 bind 2048)
[ 0.277178] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.277206] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.277418] NET: Registered protocol family 1
[ 0.277969] RPC: Registered named UNIX socket transport module.
[ 0.277986] RPC: Registered udp transport module.
[ 0.277995] RPC: Registered tcp transport module.
[ 0.278004] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.279156] hw perfevents: no interrupt-affinity property for /pmu, guessing.
[ 0.279315] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[ 0.281222] workingset: timestamp_bits=14 max_order=16 bucket_order=2
[ 0.287155] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.288110] NFS: Registering the id_resolver key type
[ 0.288172] Key type id_resolver registered
[ 0.288183] Key type id_legacy registered
[ 0.288242] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.290904] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
[ 0.290934] io scheduler noop registered
[ 0.290945] io scheduler deadline registered
[ 0.291235] io scheduler cfq registered (default)
[ 0.291250] io scheduler mq-deadline registered
[ 0.291261] io scheduler kyber registered
[ 0.293172] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[ 0.361440] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.365540] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 30, base_baud = 3000000) is a 8250
[ 0.995151] console [ttyS0] enabled
[ 1.000013] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 31, base_baud = 3000000) is a 8250
[ 1.010097] 481a6000.serial: ttyS3 at MMIO 0x481a6000 (irq = 32, base_baud = 3000000) is a 8250
[ 1.020098] 481a8000.serial: ttyS4 at MMIO 0x481a8000 (irq = 33, base_baud = 3000000) is a 8250
[ 1.031235] omap_rng 48310000.rng: Random Number Generator ver. 20
[ 1.039994] panel panel: found backlight
[ 1.044355] OF: graph: no port node found in /ocp/lcdc@4830e000
[ 1.050747] OF: graph: no port node found in /ocp/lcdc@4830e000
[ 1.057335] OF: graph: no port node found in /ocp/lcdc@4830e000
[ 1.063296] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 1.069996] [drm] No driver support for vblank timestamp query.
[ 1.123191] Console: switching to colour frame buffer device 60x34
[ 1.147104] tilcdc 4830e000.lcdc: fb0: frame buffer device
[ 1.153391] [drm] Initialized tilcdc 1.0.0 20121205 for 4830e000.lcdc on minor 0
[ 1.175702] brd: module loaded
[ 1.187399] loop: module loaded
[ 1.196065] libphy: Fixed MDIO Bus: probed
[ 1.275007] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000
[ 1.282734] davinci_mdio 4a101000.mdio: detected phy mask fffffffc
[ 1.291430] libphy: 4a101000.mdio: probed
[ 1.295609] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver Micrel KSZ8041RNLI
[ 1.304645] davinci_mdio 4a101000.mdio: phy[1]: device 4a101000.mdio:01, driver Micrel KSZ8041RNLI
[ 1.314868] cpsw 4a100000.ethernet: Detected MACID = fc:69:47:be:c5:fb
[ 1.321850] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4
[ 1.328330] cpsw 4a100000.ethernet: ALE Table size 1024
[ 1.333662] cpsw 4a100000.ethernet: cpts: overflow check period 500 (jiffies)
[ 1.342686] i2c /dev entries driver
[ 1.346861] IR NEC protocol handler initialized
[ 1.351456] IR RC5(x/sz) protocol handler initialized
[ 1.356571] IR RC6 protocol handler initialized
[ 1.361122] IR JVC protocol handler initialized
[ 1.365691] IR Sony protocol handler initialized
[ 1.370338] IR SANYO protocol handler initialized
[ 1.375080] IR Sharp protocol handler initialized
[ 1.379804] IR MCE Keyboard/mouse protocol handler initialized
[ 1.385679] IR XMP protocol handler initialized
[ 1.392251] cpuidle: enable-method property 'ti,am3352' found operations
[ 1.399735] sdhci: Secure Digital Host Controller Interface driver
[ 1.406038] sdhci: Copyright(c) Pierre Ossman
[ 1.413149] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.419902] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.430289] NET: Registered protocol family 10
[ 1.436630] Segment Routing with IPv6
[ 1.440463] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 1.447445] NET: Registered protocol family 17
[ 1.452257] Key type dns_resolver registered
[ 1.456995] omap_voltage_late_init: Voltage driver support not added
[ 1.495215] tps65910 0-002d: No interrupt support, no core IRQ
[ 1.503393] vrtc: supplied by vbat
[ 1.510816] vio: supplied by vbat
[ 1.515824] vdd1: supplied by vbat
[ 1.521204] vdd2: supplied by vbat
[ 1.525108] random: fast init done
[ 1.531579] vdig1: supplied by vbat
[ 1.536620] vdig2: supplied by vbat
[ 1.541648] vpll: supplied by vbat
[ 1.546628] vdac: supplied by vbat
[ 1.551564] vaux1: supplied by vbat
[ 1.556602] vaux2: supplied by vbat
[ 1.561615] vaux33: supplied by vbat
[ 1.566788] vmmc: supplied by vbat
[ 1.571720] vbb: supplied by vbat
[ 1.576824] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 1.742862] omap_hsmmc 48060000.mmc: card claims to support voltages below defined range
[ 1.763070] mmc0: new high speed SDIO card at address 0001
[ 1.795892] hctosys: unable to open rtc device (rtc0)
[ 1.801581] lis3_reg: disabling
[ 1.804749] vwl1837: disabling
[ 1.808257] ALSA device list:
[ 1.812351] No soundcards found.
[ 1.819117] Waiting for root device PARTUUID=f4069e7b-01...
[ 1.870471] mmc1: new high speed MMC card at address 0001
[ 1.877663] mmcblk1: mmc1:0001 4FTE4R 3.64 GiB
[ 1.882528] mmcblk1boot0: mmc1:0001 4FTE4R partition 1 4.00 MiB
[ 1.888775] mmcblk1boot1: mmc1:0001 4FTE4R partition 2 4.00 MiB
[ 1.894973] mmcblk1rpmb: mmc1:0001 4FTE4R partition 3 512 KiB
[ 1.902228] mmcblk1: p1
[ 1.948491] EXT4-fs (mmcblk1p1): mounted filesystem with ordered data mode. Opts: (null)
[ 1.956878] VFS: Mounted root (ext4 filesystem) on device 179:1.
[ 1.967878] devtmpfs: mounted
[ 1.972557] Freeing unused kernel memory: 1024K
[ 2.187007] systemd[1]: System time before build time, advancing clock.
[ 2.238833] systemd[1]: systemd 234 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN default-hierarchy=hybrid)
[ 2.260619] systemd[1]: Detected architecture arm.
Welcome to Arago 2018.08!
[ 2.297025] systemd[1]: Set hostname to <am335x-evm>.
[ 2.628765] systemd[1]: /lib/systemd/system/gadget-init.service:15: Unknown lvalue 'ExecStopPre' in section 'Service'
[ 2.898683] random: systemd: uninitialized urandom read (16 bytes read)
[ 2.906438] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
[ OK ] Started Dispatch Password Requests to Console Directory Watch.
[ 2.979699] random: systemd: uninitialized urandom read (16 bytes read)
[ 2.987590] systemd[1]: Listening on udev Control Socket.
[ OK ] Listening on udev Control Socket.
[ 3.016020] random: systemd: uninitialized urandom read (16 bytes read)
[ 3.023560] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 3.058428] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 3.089637] systemd[1]: Created slice System Slice.
[ OK ] Created slice System Slice.
[ 3.126236] systemd[1]: Reached target Slices.
[ OK ] Reached target Slices.
Mounting Kernel Debug File System...
Mounting POSIX Message Queue File System...
[ OK ] Listening on /dev/initctl Compatibility Named Pipe.
[ OK ] Created slice system-getty.slice.
[ OK ] Listening on Process Core Dump Socket.
[ OK ] Reached target Swap.
Mounting Temporary Directory (/tmp)...
[ OK ] Listening on Journal Socket.
Starting Load Kernel Modules...
[ OK ] Listening on Syslog Socket.
[ 3.443836] cryptodev: loading out-of-tree module taints kernel.
[ 3.465497] cryptodev: driver 1.9 loaded.
Starting Journal Service...
[ 3.494615] usbcore: registered new interface driver usbfs
[ 3.514397] usbcore: registered new interface driver hub
[ 3.545396] usbcore: registered new device driver usb
[ OK ] Created slice system-serial\x2dgetty.slice.
[ 3.559565] usbcore: registered new interface driver usbserial
[ OK ] Listening on udev Kernel Socket.
[ 3.606093] usbcore: registered new interface driver ftdi_sio
[ 3.611953] usbserial: USB Serial support registered for FTDI USB Serial Device
[ OK ] Started Forward Password Requests to Wall Directory Watch.
[ OK ] Reached target Paths.
[ OK ] Reached target Remote File Systems.
Starting Remount Root and Kernel File Systems...
[ OK ] Mounted Kernel Debug File System.
[ 3.816395] EXT4-fs (mmcblk1p1): re-mounted. Opts: (null)
[ OK ] Mounted POSIX Message Queue File System.
[ OK ] Mounted Temporary Directory (/tmp).
[ OK ] Started Journal Service.
[ OK ] Started Load Kernel Modules.
[ OK ] Started Remount Root and Kernel File Systems.
Starting udev Coldplug all Devices...
Starting Create Static Device Nodes in /dev...
Starting Apply Kernel Variables...
Mounting Kernel Configuration File System...
Starting Flush Journal to Persistent Storage...
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Started Create Static Device Nodes in /dev.
[ OK ] Started Apply Kernel Variables.
[ 4.467445] systemd-journald[67]: Received request to flush runtime journal from PID 1
Starting udev Kernel Device Manager...
[ OK ] Reached target Local File Systems (Pre).
Mounting /media/ram...
Mounting /var/volatile...
[ OK ] Mounted /var/volatile.
[ OK ] Mounted /media/ram.
[ OK ] Started Flush Journal to Persistent Storage.
[ OK ] Started udev Kernel Device Manager.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
[ OK ] Started Load/Save Random Seed.
[ OK ] Started Create Volatile Files and Directories.
Starting Update UTMP about System Boot/Shutdown...
Starting Network Time Synchronization...
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Time Synchronized.
[ OK ] Created slice system-systemd\x2dbacklight.slice.
Starting Load/Save Screen Backlight…ightness of backlight:backlight...
[ 6.786445] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
[ 6.863841] omap_rtc 44e3e000.rtc: already running
[ OK ] Found device /dev/ttyS0.
[ 6.916565] omap_rtc 44e3e000.rtc: registered as rtc0
[ OK ] Started udev Coldplug all Devices.
[ OK ] Started Load/Save Screen Backlight Brightness of backlight:backlight.
[ OK ] Reached target System Initialization.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
Starting Network Service...
[ OK ] Listening on dropbear.socket.
[ OK ] Started Daily rotation of log files.
[ OK ] Listening on RPCbind Server Activation Socket.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
[ OK ] Started Periodic Command Scheduler.
[ OK ] Started D-Bus System Message Bus.
[ 8.085190] omap_hwmod: pruss: _wait_target_ready failed: -16
[ 8.215158] pruss-soc-bus 4a326004.pruss-soc-bus: use pm_runtime_put_sync_suspend() in driver?
[ 8.317006] pruss-soc-bus 4a326004.pruss-soc-bus: couldn't enable module
[ 8.374262] remoteproc remoteproc0: wkup_m3 is available
[ 8.415275] pruss-soc-bus: probe of 4a326004.pruss-soc-bus failed with error -16
[ 8.425314] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[ 8.545864] [drm] Initialized pvr 1.14.3699939 20110701 for 56000000.sgx on minor 1
[ 8.598873] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[ 8.658580] remoteproc remoteproc0: powering up wkup_m3
[ 8.675272] omap-aes 53500000.aes: will run requests pump with realtime priority
[ 8.683639] PM: Cannot get wkup_m3_ipc handle
[ 8.757166] PM: Cannot get wkup_m3_ipc handle
[ OK ] Started Hardware RNG Entropy Gatherer Daemon.
[ 9.029060] remoteproc remoteproc0: Booting fw image am335x-pm-firmware.elf, size 224628
[ 9.078395] random: crng init done
[ 9.078406] random: 7 urandom warning(s) missed due to ratelimiting
Starting uim-sysfs.service...
[ 9.273878] remoteproc remoteproc0: remote processor wkup_m3 is now up
[ 9.273902] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x192
Starting RPC Bind Service...
Starting Login Service...
[ OK ] Reached target Containers.
[ OK ] Started Job spooling tools.
Starting Avahi mDNS/DNS-SD Stack...
[ OK ] Started Kernel Logging Service.
Starting Print notice about GPLv3 packages...
[ OK ] Started System Logging Service.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target Timers.
[ OK ] Started Network Service.
[ OK ] Started RPC Bind Service.
[ 10.599119] net eth0: initializing cpsw version 1.12 (0)
[ 10.785657] Micrel KSZ8041RNLI 4a101000.mdio:00: attached PHY driver [Micrel KSZ8041RNLI] (mii_bus:phy_addr=4a101000.mdio:00, irq=POLL)
[ 11.029881] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ OK ] Started Login Service.
[ OK ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
[ OK ] Reached target Network.
Starting Lightning Fast Webserver With Light System Requirements...
Starting Simple Network Management Protocol (SNMP) Daemon....
Starting Permit User Sessions...
Starting Enable and configure wl18xx bluetooth stack...
[ OK ] Started Redis In-Memory Data Store.
Starting Wait for Network to be Configured...
Starting Network Name Resolution...
[ OK ] Started Lightning Fast Webserver With Light System Requirements.
[ OK ] Started Permit User Sessions.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyS0.
[ OK ] Started Network Name Resolution.
[ OK ] Reached target Host and Network Name Lookups.
[ OK ] Started NFS status monitor for NFSv2/3 locking..
U-Boot SPL 2018.01-00451-g3714995-dirty (Jan 21 2019 - 16:22:33)
Trying to boot from MMC2
U-Boot 2018.01-00451-g3714995-dirty (Jan 21 2019 - 16:22:33 +0300)
CPU : AM335X-GP rev 2.1
Model: TI AM335x EVM-SK
DRAM: 256 MiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
** Bad device mmc 0 **
Using default environment
<ethaddr> not set. Validating first E-fuse MAC
Net: cpsw
Hit any key to stop autoboot: 0
switch to partitions #0, OK
mmc1(part 0) is current device
Scanning mmc 1:1...
switch to partitions #0, OK
mmc1(part 0) is current device
SD/MMC found on device 1
3858944 bytes read in 334 ms (11 MiB/s)
38052 bytes read in 11 ms (3.3 MiB/s)
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8df15000, end 8df214a3 ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Linux version 4.14.67-gd315a9bb00 (mehmetk@vkdijd19743u) (gcc version 7.2.1 20171011 (Linaro GCC 7.2-2017.11)) #3 PREEMPT Tue Feb 12 12:47:04 AST 2019
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] OF: fdt: Machine model: TI AM335x EVM-SK
[ 0.000000] Memory policy: Data cache writeback
[ 0.000000] efi: Getting EFI parameters from FDT:
[ 0.000000] efi: UEFI not found.
[ 0.000000] cma: Reserved 48 MiB at 0x8a800000
[ 0.000000] CPU: All CPU(s) started in SVC mode.
[ 0.000000] AM335X ES2.1 (sgx neon)
[ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 64960
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=PARTUUID=35a240cd-01 rw rootfstype=ext4 rootwait
[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 197272K/262144K available (8192K kernel code, 319K rwdata, 2480K rodata, 1024K init, 275K bss, 15720K reserved, 49152K cma-reserved, 0K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xd0800000 - 0xff800000 ( 752 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0900000 (9184 kB)
[ 0.000000] .init : 0xc0c00000 - 0xc0d00000 (1024 kB)
[ 0.000000] .data : 0xc0d00000 - 0xc0d4fc08 ( 320 kB)
[ 0.000000] .bss : 0xc0d4fc08 - 0xc0d949b4 ( 276 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Tasks RCU enabled.
[ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz
[ 0.000022] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns
[ 0.000051] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns
[ 0.000065] OMAP clocksource: timer1 at 24000000 Hz
[ 0.000299] timer_probe: no matching timers found
[ 0.000561] Console: colour dummy device 80x30
[ 0.000597] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000606] This ensures that you still see kernel messages. Please
[ 0.000614] update your kernel commandline.
[ 0.000653] Calibrating delay loop... 597.60 BogoMIPS (lpj=2988032)
[ 0.118727] pid_max: default: 32768 minimum: 301
[ 0.118970] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.118990] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.119976] CPU: Testing write buffer coherency: ok
[ 0.120904] Setting up static identity map for 0x80100000 - 0x80100060
[ 0.121112] Hierarchical SRCU implementation.
[ 0.121571] EFI services will not be available.
[ 0.123398] devtmpfs: initialized
[ 0.134177] random: get_random_u32 called from bucket_table_alloc+0x8c/0x1ac with crng_init=0
[ 0.134775] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3
[ 0.135144] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.135177] futex hash table entries: 256 (order: -1, 3072 bytes)
[ 0.139919] pinctrl core: initialized pinctrl subsystem
[ 0.140811] DMI not present or invalid.
[ 0.141312] NET: Registered protocol family 16
[ 0.144196] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.162723] omap_hwmod: debugss: _wait_target_disable failed
[ 0.217403] cpuidle: using governor ladder
[ 0.217453] cpuidle: using governor menu
[ 0.223373] OMAP GPIO hardware version 0.1
[ 0.237983] No ATAGs?
[ 0.238005] hw-breakpoint: debug architecture 0x4 unsupported.
[ 0.255625] edma 49000000.edma: TI EDMA DMA engine driver
[ 0.257046] reg-fixed-voltage fixedregulator2: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_wl12xx_gpio, deferring probe
[ 0.261064] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, deferring probe
[ 0.261261] media: Linux media interface: v0.10
[ 0.261330] Linux video capture interface: v2.00
[ 0.261468] pps_core: LinuxPPS API ver. 1 registered
[ 0.261481] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.261510] PTP clock support registered
[ 0.261556] EDAC MC: Ver: 3.0.0
[ 0.262134] dmi: Firmware registration failed.
[ 0.262668] omap-mailbox 480c8000.mailbox: omap mailbox rev 0x400
[ 0.263110] Advanced Linux Sound Architecture Driver Initialized.
[ 0.264578] clocksource: Switched to clocksource timer1
[ 0.275665] NET: Registered protocol family 2
[ 0.276606] TCP established hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.276653] TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.276690] TCP: Hash tables configured (established 2048 bind 2048)
[ 0.276815] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.276841] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.277052] NET: Registered protocol family 1
[ 0.277609] RPC: Registered named UNIX socket transport module.
[ 0.277631] RPC: Registered udp transport module.
[ 0.277641] RPC: Registered tcp transport module.
[ 0.277650] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.278804] hw perfevents: no interrupt-affinity property for /pmu, guessing.
[ 0.278961] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available
[ 0.280879] workingset: timestamp_bits=14 max_order=16 bucket_order=2
[ 0.286831] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.287803] NFS: Registering the id_resolver key type
[ 0.287858] Key type id_resolver registered
[ 0.287869] Key type id_legacy registered
[ 0.287926] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.290588] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
[ 0.290616] io scheduler noop registered
[ 0.290627] io scheduler deadline registered
[ 0.290912] io scheduler cfq registered (default)
[ 0.290927] io scheduler mq-deadline registered
[ 0.290938] io scheduler kyber registered
[ 0.292838] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568
[ 0.361452] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.365592] 44e09000.serial: ttyS0 at MMIO 0x44e09000 (irq = 30, base_baud = 3000000) is a 8250
[ 0.995764] console [ttyS0] enabled
[ 1.000606] 48022000.serial: ttyS1 at MMIO 0x48022000 (irq = 31, base_baud = 3000000) is a 8250
[ 1.010673] 481a6000.serial: ttyS3 at MMIO 0x481a6000 (irq = 32, base_baud = 3000000) is a 8250
[ 1.021783] omap_rng 48310000.rng: Random Number Generator ver. 20
[ 1.030510] panel panel: found backlight
[ 1.035031] OF: graph: no port node found in /ocp/lcdc@4830e000
[ 1.041282] OF: graph: no port node found in /ocp/lcdc@4830e000
[ 1.047875] OF: graph: no port node found in /ocp/lcdc@4830e000
[ 1.053837] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 1.060537] [drm] No driver support for vblank timestamp query.
[ 1.113719] Console: switching to colour frame buffer device 60x34
[ 1.137642] tilcdc 4830e000.lcdc: fb0: frame buffer device
[ 1.143933] [drm] Initialized tilcdc 1.0.0 20121205 for 4830e000.lcdc on minor 0
[ 1.166098] brd: module loaded
[ 1.177805] loop: module loaded
[ 1.186486] libphy: Fixed MDIO Bus: probed
[ 1.192261] qcaspi spi0.0: ver=0.2.7-i, clkspeed=10000000, burst_len=5000, pluggable=0
[ 1.200512] qcaspi spi0.0: Using random MAC address: 52:32:a2:02:b9:ae
[ 1.207234] qcaspi spi0.0: Invalid signature (0xFFFF)
[ 1.212362] qcaspi: probe of spi0.0 failed with error -14
[ 1.218176] qcaspi spi1.0: ver=0.2.7-i, clkspeed=10000000, burst_len=5000, pluggable=0
[ 1.226269] qcaspi spi1.0: Using random MAC address: 9e:81:1d:cb:99:ee
[ 1.232915] qcaspi spi1.0: Invalid signature (0xFFFF)
[ 1.238087] qcaspi: probe of spi1.0 failed with error -14
[ 1.314611] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000
[ 1.322323] davinci_mdio 4a101000.mdio: detected phy mask fffffffc
[ 1.331012] libphy: 4a101000.mdio: probed
[ 1.335196] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver Micrel KSZ8041RNLI
[ 1.344230] davinci_mdio 4a101000.mdio: phy[1]: device 4a101000.mdio:01, driver Micrel KSZ8041RNLI
[ 1.354453] cpsw 4a100000.ethernet: Detected MACID = c8:df:84:97:1b:26
[ 1.361407] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4
[ 1.367879] cpsw 4a100000.ethernet: ALE Table size 1024
[ 1.373187] cpsw 4a100000.ethernet: cpts: overflow check period 500 (jiffies)
[ 1.382253] i2c /dev entries driver
[ 1.386454] IR NEC protocol handler initialized
[ 1.391016] IR RC5(x/sz) protocol handler initialized
[ 1.396167] IR RC6 protocol handler initialized
[ 1.400718] IR JVC protocol handler initialized
[ 1.405287] IR Sony protocol handler initialized
[ 1.409926] IR SANYO protocol handler initialized
[ 1.414679] IR Sharp protocol handler initialized
[ 1.419405] IR MCE Keyboard/mouse protocol handler initialized
[ 1.425281] IR XMP protocol handler initialized
[ 1.431834] cpuidle: enable-method property 'ti,am3352' found operations
[ 1.439337] sdhci: Secure Digital Host Controller Interface driver
[ 1.445612] sdhci: Copyright(c) Pierre Ossman
[ 1.452685] sdhci-pltfm: SDHCI platform and OF driver helper
[ 1.459382] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.469697] NET: Registered protocol family 10
[ 1.476068] Segment Routing with IPv6
[ 1.479859] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[ 1.486918] NET: Registered protocol family 17
[ 1.491756] Key type dns_resolver registered
[ 1.496491] omap_voltage_late_init: Voltage driver support not added
[ 1.534859] tps65910 0-002d: No interrupt support, no core IRQ
[ 1.543179] vrtc: supplied by vbat
[ 1.550577] vio: supplied by vbat
[ 1.555599] vdd1: supplied by vbat
[ 1.560835] random: fast init done
[ 1.564433] vdd2: supplied by vbat
[ 1.571499] vdig1: supplied by vbat
[ 1.576570] vdig2: supplied by vbat
[ 1.581591] vpll: supplied by vbat
[ 1.586556] vdac: supplied by vbat
[ 1.591510] vaux1: supplied by vbat
[ 1.596568] vaux2: supplied by vbat
[ 1.601578] vaux33: supplied by vbat
[ 1.606728] vmmc: supplied by vbat
[ 1.611692] vbb: supplied by vbat
[ 1.616791] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz
[ 1.782463] omap_hsmmc 48060000.mmc: card claims to support voltages below defined range
[ 1.802818] mmc0: new high speed SDIO card at address 0001
[ 1.835517] hctosys: unable to open rtc device (rtc0)
[ 1.841244] lis3_reg: disabling
[ 1.844415] vwl1837: disabling
[ 1.847893] ALSA device list:
[ 1.851962] No soundcards found.
[ 1.858739] Waiting for root device PARTUUID=35a240cd-01...
[ 1.910087] mmc1: new high speed MMC card at address 0001
[ 1.917255] mmcblk1: mmc1:0001 4FTE4R 3.64 GiB
[ 1.922089] mmcblk1boot0: mmc1:0001 4FTE4R partition 1 4.00 MiB
[ 1.928356] mmcblk1boot1: mmc1:0001 4FTE4R partition 2 4.00 MiB
[ 1.934517] mmcblk1rpmb: mmc1:0001 4FTE4R partition 3 512 KiB
[ 1.941795] mmcblk1: p1
[ 2.365130] EXT4-fs (mmcblk1p1): recovery complete
[ 2.370364] EXT4-fs (mmcblk1p1): mounted filesystem with ordered data mode. Opts: (null)
[ 2.378998] VFS: Mounted root (ext4 filesystem) on device 179:1.
[ 2.388523] devtmpfs: mounted
[ 2.393288] Freeing unused kernel memory: 1024K
[ 2.570018] systemd[1]: System time before build time, advancing clock.
[ 2.618391] systemd[1]: systemd 234 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT -GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN2 -IDN default-hierarchy=hybrid)
[ 2.640158] systemd[1]: Detected architecture arm.
Welcome to Arago 2018.08!
[ 2.676647] systemd[1]: Set hostname to <am335x-evm>.
[ 3.024475] systemd[1]: /lib/systemd/system/gadget-init.service:15: Unknown lvalue 'ExecStopPre' in section 'Service'
[ 3.299946] random: systemd: uninitialized urandom read (16 bytes read)
[ 3.307365] systemd[1]: Listening on Journal Socket (/dev/log).
[ OK ] Listening on Journal Socket (/dev/log).
[ 3.345551] random: systemd: uninitialized urandom read (16 bytes read)
[ 3.352924] systemd[1]: Listening on Syslog Socket.
[ OK ] Listening on Syslog Socket.
[ 3.384956] random: systemd: uninitialized urandom read (16 bytes read)
[ 3.395530] systemd[1]: Created slice User and Session Slice.
[ OK ] Created slice User and Session Slice.
[ 3.425123] systemd[1]: Reached target Swap.
[ OK ] Reached target Swap.
[ 3.455705] systemd[1]: Listening on udev Kernel Socket.
[ OK ] Listening on udev Kernel Socket.
[ 3.508531] systemd[1]: Listening on Process Core Dump Socket.
[ OK ] Listening on Process Core Dump Socket.
[ OK ] Created slice System Slice.
[ OK ] Created slice system-serial\x2dgetty.slice.
Mounting Temporary Directory (/tmp)...
[ OK ] Created slice system-getty.slice.
Mounting POSIX Message Queue File System...
[ OK ] Started Dispatch Password Requests to Console Directory Watch.
Mounting Kernel Debug File System...
[ OK ] Listening on udev Control Socket.
[ OK ] Listening on Network Service Netlink Socket.
[ OK ] Reached target Remote File Systems.
[ OK ] Listening on /dev/initctl Compatibility Named Pipe.
[ OK ] Started Forward Password Requests to Wall Directory Watch.
[ OK ] Reached target Paths.
[ OK ] Listening on Journal Socket.
Starting Remount Root and Kernel File Systems...
Starting Load Kernel Modules...
Starting Journal Service...
[ 4.131727] EXT4-fs (mmcblk1p1): re-mounted. Opts: (null)
[ 4.160116] cryptodev: loading out-of-tree module taints kernel.
[ 4.165835] cryptodev: driver 1.9 loaded.
[ 4.207613] usbcore: registered new interface driver usbfs
[ 4.207679] usbcore: registered new interface driver hub
[ 4.218930] usbcore: registered new device driver usb
[ OK ] Reached target Slices.
[ 4.240680] usbcore: registered new interface driver usbserial
[ OK ] Mounted Kernel Debug File System.
[ 4.287643] usbcore: registered new interface driver ftdi_sio
[ OK ] Mounted POSIX Message Queue File System.
[ 4.315542] usbserial: USB Serial support registered for FTDI USB Serial Device
[ OK ] Mounted Temporary Directory (/tmp).
[ OK ] Started Remount Root and Kernel File Systems.
[ OK ] Started Load Kernel Modules.
Starting Apply Kernel Variables...
Mounting Kernel Configuration File System...
Starting Rebuild Hardware Database...
Starting Create System Users...
[ OK ] Mounted Kernel Configuration File System.
[ OK ] Started Journal Service.
[ OK ] Started Apply Kernel Variables.
[ OK ] Started Create System Users.
Starting Create Static Device Nodes in /dev...
Starting Flush Journal to Persistent Storage...
[ OK ] Started Create Static Device Nodes in /dev.
[ 4.935672] systemd-journald[72]: Received request to flush runtime journal from PID 1
Starting udev Kernel Device Manager...
[ OK ] Reached target Local File Systems (Pre).
Mounting /var/volatile...
Mounting /media/ram...
[ OK ] Mounted /var/volatile.
[ OK ] Mounted /media/ram.
[ OK ] Started Flush Journal to Persistent Storage.
Starting Load/Save Random Seed...
[ OK ] Reached target Local File Systems.
Starting Create Volatile Files and Directories...
Starting Rebuild Journal Catalog...
Starting Rebuild Dynamic Linker Cache...
[ OK ] Started udev Kernel Device Manager.
[ OK ] Started Load/Save Random Seed.
[ OK ] Started Create Volatile Files and Directories.
Starting Network Time Synchronization...
Starting Update UTMP about System Boot/Shutdown...
[ OK ] Started Rebuild Journal Catalog.
[ OK ] Started Update UTMP about System Boot/Shutdown.
[ OK ] Started Network Time Synchronization.
[ OK ] Reached target System Time Synchronized.
[ OK ] Started Rebuild Dynamic Linker Cache.
[ OK ] Started Rebuild Hardware Database.
Starting Update is Completed...
Starting udev Coldplug all Devices...
[ OK ] Started Update is Completed.
[ OK ] Created slice system-systemd\x2dbacklight.slice.
[ 10.194345] omap_wdt: OMAP Watchdog Timer Rev 0x01: initial timeout 60 sec
Starting Load/Save Screen Backlight…ightness of backlight:backlight...
[ OK ] Found device /dev/ttyS0.
[ 10.412118] omap_rtc 44e3e000.rtc: registered as rtc0
[ OK ] Started udev Coldplug all Devices.
[ OK ] Started Load/Save Screen Backlight Brightness of backlight:backlight.
[ OK ] Reached target System Initialization.
[ OK ] Listening on RPCbind Server Activation Socket.
[ OK ] Listening on dropbear.socket.
Starting Network Service...
[ OK ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[ OK ] Listening on D-Bus System Message Bus Socket.
[ OK ] Reached target Sockets.
[ OK ] Reached target Basic System.
[ OK ] Started D-Bus System Message Bus.
[ 11.490145] omap_hwmod: pruss: _wait_target_ready failed: -16
[ 11.563934] pruss-soc-bus 4a326004.pruss-soc-bus: use pm_runtime_put_sync_suspend() in driver?
[ 11.699568] pruss-soc-bus 4a326004.pruss-soc-bus: couldn't enable module
[ 11.786351] pruss-soc-bus: probe of 4a326004.pruss-soc-bus failed with error -16
[ 11.794342] omap-sham 53100000.sham: hw accel on OMAP rev 4.3
[ 11.858930] remoteproc remoteproc0: wkup_m3 is available
[ 11.904061] omap-aes 53500000.aes: OMAP AES hw accel rev: 3.2
[ 11.915058] omap-aes 53500000.aes: will run requests pump with realtime priority
[ 11.971918] [drm] Initialized pvr 1.14.3699939 20110701 for 56000000.sgx on minor 1
[ 12.216231] remoteproc remoteproc0: powering up wkup_m3
[ 12.224229] PM: Cannot get wkup_m3_ipc handle
[ 12.304091] remoteproc remoteproc0: Booting fw image am335x-pm-firmware.elf, size 224628
[ 12.304363] remoteproc remoteproc0: remote processor wkup_m3 is now up
[ 12.304396] wkup_m3_ipc 44e11324.wkup_m3_ipc: CM3 Firmware Version = 0x192
[ 12.451633] random: crng init done
[ 12.451643] random: 7 urandom warning(s) missed due to ratelimiting
[ OK ] Started Hardware RNG Entropy Gatherer Daemon.
Starting Login Service...
[ OK ] Started Periodic Command Scheduler.
Starting uim-sysfs.service...
[ OK ] Started System Logging Service.
[ OK ] Reached target Containers.
[ OK ] Started Job spooling tools.
[ 13.495070] net eth0: initializing cpsw version 1.12 (0)
Starting RPC Bind Service...
[ 13.665359] Micrel KSZ8041RNLI 4a101000.mdio:00: attached PHY driver [Micrel KSZ8041RNLI] (mii_bus:phy_addr=4a101000.mdio:00, irq=POLL)
Starting Avahi mDNS/DNS-SD Stack...
[ OK ] Started Kernel Logging Service.
[ 13.958169] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
Starting Print notice about GPLv3 packages...
[ OK ] Started Daily rotation of log files.
[ OK ] Started Daily Cleanup of Temporary Directories.
[ OK ] Reached target Timers.
[ OK ] Started Network Service.
[ OK ] Started RPC Bind Service.
[ OK ] Found device /dev/ttyS3.
[ OK ] Started Avahi mDNS/DNS-SD Stack.
[ OK ] Started Login Service.
[ OK ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
[ OK ] Reached target Network.
Starting Simple Network Management Protocol (SNMP) Daemon....
Starting Permit User Sessions...
Starting Lightning Fast Webserver With Light System Requirements...
[ OK ] Started Redis In-Memory Data Store.
Starting Enable and configure wl18xx bluetooth stack...
Starting Network Name Resolution...
Starting Wait for Network to be Configured...
[ OK ] Started Permit User Sessions.
[ OK ] Started Lightning Fast Webserver With Light System Requirements.
[ OK ] Started Getty on tty1.
[ OK ] Started Serial Getty on ttyS3.
[ OK ] Started Serial Getty on ttyS0.
[ OK ] Started Network Name Resolution.
[ 19.432720] TI-am335x-tsc 44e0d000.tscadc:tsc: ti,charge-delay not specified
[ 19.555281] input: ti-tsc as /devices/platform/ocp/44e0d000.tscadc/44e0d000.tscadc:tsc/input/input0
[ 19.677615] PM: bootloader does not support rtc-only!
[ OK ] Started Enable and configure wl18xx bluetooth stack.
[ OK ] Started Simple Network Management Protocol (SNMP) Daemon..
[ OK ] Started uim-sysfs.service.
[ 20.657319] am335x-phy-driver 47401300.usb-phy: 47401300.usb-phy supply vcc not found, using dummy regulator
[ 20.796879] am335x-phy-driver 47401b00.usb-phy: 47401b00.usb-phy supply vcc not found, using dummy regulator
[ 20.914327] musb-hdrc musb-hdrc.0: MUSB HDRC host driver
[ 21.024849] musb-hdrc musb-hdrc.0: new USB bus registered, assigned bus number 1
[ 21.108902] hub 1-0:1.0: USB hub found
[ 21.140508] hub 1-0:1.0: 1 port detected
[ 21.193329] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 21.313222] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 2
[ 21.391564] hub 2-0:1.0: USB hub found
[ 21.425736] hub 2-0:1.0: 1 port detected
[ 22.381697] wl18xx_driver wl18xx.0.auto: Direct firmware load for ti-connectivity/wl1271-nvs.bin failed with error -2
[ 22.875927] wlcore: wl18xx HW: 183x or 180x, PG 2.2 (ROM 0x11)
[ 23.026563] wlcore: loaded
[ 23.963957] wlcore: PHY firmware version: Rev 8.2.0.0.240
[ 24.119745] wlcore: firmware booted (Rev 8.9.0.0.76)
[ 24.168508] IPv6: ADDRCONF(NETDEV_UP): wlan0: link is not ready
_____ _____ _ _
| _ |___ ___ ___ ___ | _ |___ ___ |_|___ ___| |_
| | _| .'| . | . | | __| _| . | | | -_| _| _|
|__|__|_| |__,|_ |___| |__| |_| |___|_| |___|___|_|
|___| |___|
Arago Project http://arago-project.org am335x-evm ttyS0
Arago 2018.08 am335x-evm ttyS0
am335x-evm login: ***************************************************************
***************************************************************
NOTICE: This file system contains the following GPLv3 packages:
autoconf
bash-dev
bash
binutils
cifs-utils
cpio
cpp-symlinks
cpp
dosfstools
elfutils
findutils
g++-symlinks
g++
gawk
gcc-symlinks
gcc
gdb
gdbserver
gettext
gstreamer1.0-libav
gzip
hidapi
libdw1
libelf1
libgdbm-compat4
libgdbm-dev
libgdbm4
libgettextlib
libgettextsrc
libgmp10
libidn11
libmavconn
libmpc3
libmpfr4
libreadline-dev
libreadline7
libunistring2
m4-dev
m4
make
mavlink
mavros-extras
mavros-msgs
mavros
nettle
python3-pycairo
socketcan-interface
which
If you do not wish to distribute GPLv3 components please remove
the above packages prior to distribution. This can be done using
the opkg remove command. i.e.:
opkg remove <package>
Where <package> is the name printed in the list above
NOTE: If the package is a dependency of another package you
will be notified of the dependent packages. You should
use the --force-removal-of-dependent-packages option to
also remove the dependent packages as well
***************************************************************
***************************************************************
[ 26.435556] PVR_K: UM DDK-(3699939) and KM DDK-(3699939) match. [ OK ]
[ 27.604667] NOHZ: local_softirq_pending 202
[ 27.608938] NOHZ: local_softirq_pending 202
[ 27.613186] NOHZ: local_softirq_pending 202
[ 27.694671] NOHZ: local_softirq_pending 40
[ 34.874863] NOHZ: local_softirq_pending 02
[ 38.594883] NOHZ: local_softirq_pending 02
[ 44.174883] NOHZ: local_softirq_pending 02
[ 47.894884] NOHZ: local_softirq_pending 02
[ 51.614883] NOHZ: local_softirq_pending 02
[ 57.194884] NOHZ: local_softirq_pending 02
Thanks,
Regards,
Zafer Çalışkan