This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365 EVM: NFS Issues

Other Parts Discussed in Thread: TVP7002

Hi,

I'm making better progress. The kernel is now booting over TFTP but begins choking on the NFS mount. It seems to be trying to obtain port numbers from the NFS server and I'm wondering if my client and server are compatible. Another issue is that it seems to be attempting to talk to a server at 0.0.0.0 and I doubt that's going to work. I'm not sure which server it is talking about.

At least my issues are becoming somewhat more generic :)

M365 EVM :>printenv
bootdelay=4
baudrate=115200
bootfile="uImage"
rootpath=/home/kenny/Development/Gauge/Shared
setboot=setenv bootargs $(bootargs) video=dm36x:output=$(videostd)
nfshost=192.168.1.201
bootargs=console=ttyS0,115200n8 noinitrd rw ip=dhcp root=/dev/nfs nfsroot=$(nfshos
t):$(rootpath),nolock mem=76M video=davincifb:vid0=OFF:vid1=OFF:osd0=720x576x16,40
50K dm365_imp.oper_mode=0 davinci_capture.device_type=4
serverip=192.168.1.201
bootcmd=dhcp;bootm
stdin=serial
stdout=serial
stderr=serial
ethaddr=00:0C:0C:A0:02:b5
ver=U-Boot 1.3.4 (Aug 23 2009 - 14:30:46)

Environment size: 552/262140 bytes

 

DM36x initialization passed!
TI UBL Version: 1.50
Booting Catalog Boot Loader
BootMode = NAND
Starting NAND Copy...
Valid magicnum, 0xA1ACED66, found in block 0x00000019.
   DONE
Jumping to entry point at 0x81080000.


U-Boot 1.3.4 (Aug 23 2009 - 14:30:46)

I2C:   ready
DRAM:  128 MB
NAND:  NAND device: Manufacturer ID: 0x2c, Chip ID: 0xd3 (Micron NAND 1GiB 3,3V
 8-bit)
Bad block table found at page 524224, version 0x01
Bad block table found at page 524160, version 0x01
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xd3 (Micron NAND 1GiB 3,3V 8-bit)
Bad block table found at page 524224, version 0x01
Bad block table found at page 524160, version 0x01
2048 MiB
In:    serial
Out:   serial
Err:   serial
Ethernet PHY: GENERIC @ 0x00
Hit any key to stop autoboot:  0
BOOTP broadcast 1
DHCP client bound to address 192.168.1.5
TFTP from server 192.168.1.201; our IP address is 192.168.1.5
Filename 'uImage'.
Load address: 0x80700000
Loading: #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         #################################################################
         ###########
done
Bytes transferred = 2050140 (1f485c hex)
## Booting kernel from Legacy Image at 80700000 ...
   Image Name:   Linux-2.6.18_pro500-davinci_evm-
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2050076 Bytes =  2 MB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux............................................................
............................................................................. d
one, booting the kernel.
Linux version 2.6.18_pro500-davinci_evm-arm_v5t_le (kenny@Ubuntu) (gcc version
4.2.0 (MontaVista 4.2.0-16.0.32.0801914 2008-08-30)) #1 PREEMPT Sun Aug 30 15:2
7:04 PDT 2009
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
Machine: DaVinci DM365 EVM
Memory policy: ECC disabled, Data cache writeback
DaVinci DM0365 variant 0x0
PLL0: fixedrate: 24000000, commonrate: 121500000, vpssrate: 243000000
PLL0: vencrate_sd: 27000000, ddrrate: 243000000 mmcsdrate: 121500000
PLL1: armrate: 297000000, voicerate: 20482758, vencrate_hd: 74250000
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
Built 1 zonelists.  Total pages: 19456
Kernel command line: console=ttyS0,115200n8 noinitrd rw ip=dhcp root=/dev/nfs n
fsroot=$(nfshost):$(rootpath),nolock mem=76M video=davincifb:vid0=OFF:vid1=OFF:
osd0=720x576x16,4050K dm365_imp.oper_mode=0 davinci_capture.device_type=4
PID hash table entries: 512 (order: 9, 2048 bytes)
Clock event device timer0_0 configured with caps set: 07
Console: colour dummy device 80x30
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 76MB = 76MB total
Memory: 72576KB available (3525K code, 712K data, 200K init)
Security Framework v1.0.0 initialized
Capability LSM initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
NET: Registered protocol family 16
MUX: initialized SPI0_SCLK
MUX: initialized SPI0_SDO)
MUX: initialized SPI0_SDI
MUX: initialized SPI0_SDENA0
DaVinci: 104 gpio irqs
MUX: initialized GPIO20
MUX: initialized I2C_SCL
DM365 IPIPE initialized in Continuous mode
Generic PHY: Registered new driver
ch0 default output "COMPOSITE", mode "NTSC"
VPBE Encoder Initialized
LogicPD encoder initialized
Avnetlcd encoder initialized
dm365_afew_hw_init
SCSI subsystem initialized
usbcore: registered new driver usbfs
usbcore: registered new driver hub
NET: Registered protocol family 2
IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
TCP established hash table entries: 4096 (order: 2, 16384 bytes)
TCP bind hash table entries: 2048 (order: 1, 8192 bytes)
TCP: Hash tables configured (established 4096 bind 2048)
TCP reno registered
VFS: Disk quotas dquot_6.5.1
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
squashfs: version 3.1 (2006/08/19) Phillip Lougher
JFFS2 version 2.2. (NAND) (C) 2001-2006 Red Hat, Inc.
yaffs Aug 30 2009 15:23:25 Installing.
SGI XFS with no debug enabled
Initializing Cryptographic API
io scheduler noop registered
io scheduler anticipatory registered (default)
davincifb davincifb.0: dm_osd0_fb: Initial window configuration is invalid.
davincifb davincifb.0: dm_osd0_fb: 720x576x16@0,0 with framebuffer size 4050KB
davincifb davincifb.0: dm_vid0_fb: 0x0x16@0,0 with framebuffer size 1020KB
davincifb davincifb.0: dm_osd1_fb: 720x480x4@0,0 with framebuffer size 675KB
davincifb davincifb.0: dm_vid1_fb: 0x0x16@0,0 with framebuffer size 1020KB
DAVINCI-WDT: DaVinci Watchdog Timer: heartbeat 60 sec
facedetect major#: 253, minor# 0
facedetect driver registered
imp serializer initialized
davinci_previewer initialized
davinci_resizer initialized
Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO map 0x1c20000 mem 0xfbc20000 (irq = 40) is a 16550A
serial8250.0: ttyS1 at MMIO map 0x1d06000 mem 0xfbd06000 (irq = 41) is a 16550A
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize
Davinci EMAC MII Bus: probed
MAC address is 00:0e:99:02:c9:09
TI DaVinci EMAC Linux version updated 4.0
netconsole: not configured, aborting
Linux video capture interface: v2.00
vpfe_init
starting ccdc_reset...<7>
End of ccdc_reset...<5>vpfe_probe
vpfe ccdc capture vpfe ccdc capture.1: vpif_register_decoder: decoder = MT9T001
vpfe ccdc capture vpfe ccdc capture.1: vpif_register_decoder: decoder = MT9P031
TVP514X : nummber of channels = 1
vpfe ccdc capture vpfe ccdc capture.1: vpif_register_decoder: decoder = TVP514X
Trying to register davinci display video device.
layer=c40bb600,layer->video_dev=c40bb760
Trying to register davinci display video device.
layer=c40bb400,layer->video_dev=c40bb560
davinci_init:DaVinci V4L2 Display Driver V1.0 loaded
vpfe ccdc capture vpfe ccdc capture.1: vpif_register_decoder: decoder = TVP7002
af major#: 250, minor# 0
AF Driver initialized
aew major#: 249, minor# 0
AEW Driver initialized
i2c /dev entries driver
nand_davinci nand_davinci.0: Using 4-bit hardware ECC
NAND device: Manufacturer ID: 0x2c, Chip ID: 0xd3 (Micron NAND 1GiB 3,3V 8-bit)
2 NAND chips detected
Creating 5 MTD partitions on "nand_davinci.0":
0x00000000-0x003c0000 : "bootloader"
0x003c0000-0x00400000 : "params"
0x00400000-0x00800000 : "kernel"
0x00800000-0x20800000 : "filesystem1"
0x20800000-0x80000000 : "filesystem2"
nand_davinci nand_davinci.0: hardware revision: 2.3
dm_spi.0: davinci SPI Controller driver at 0xc501e000 (irq = 42) use_dma=0
Initializing USB Mass Storage driver...
usbcore: registered new driver usb-storage
USB Mass Storage support registered.
usbcore: registered new driver usbhid
drivers/usb/input/hid-core.c: v2.6:USB HID core driver
musb_hdrc: version 6.0, cppi-dma, host, debug=0
MUX: initialized GPIO33
musb_hdrc musb_hdrc: No DMA interrupt line
musb_hdrc: USB Host mode controller at c5074000 using DMA, IRQ 12
musb_hdrc musb_hdrc: MUSB HDRC host driver
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
usb usb1: configuration #1 chosen from 1 choice
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
mice: PS/2 mouse device common for all mice
davinci-mmc davinci-mmc.0: Supporting 4-bit mode
davinci-mmc davinci-mmc.0: Using DMA mode
Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50
 2006 UTC).
ASoC version 0.13.1
AIC3X Audio Codec 0.2
asoc: aic3x <-> davinci-i2s mapping ok
ALSA device list:
  #0: DaVinci DM365 EVM (aic3x)
IPv4 over IPv4 tunneling driver
TCP bic registered
NET: Registered protocol family 1
NET: Registered protocol family 17
drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
Time: timer0_1 clocksource has been installed.
Clock event device timer0_0 configured with caps set: 08
Switched to high resolution mode on CPU 0
Sending DHCP requests ..., OK
IP-Config: Got DHCP answer from 0.0.0.0, my address is 192.168.1.4
IP-Config: Complete:
      device=eth0, addr=192.168.1.4, mask=255.255.255.0, gw=192.168.1.1,
     host=192.168.1.4, domain=, nis-domain=(none),
     bootserver=0.0.0.0, rootserver=0.0.0.0, rootpath=
Looking up port of RPC 100003/2 on 0.0.0.0
portmap: server 0.0.0.0 not responding, timed out
Root-NFS: Unable to get nfsd port number from server, using default
Looking up port of RPC 100005/1 on 0.0.0.0
portmap: server 0.0.0.0 not responding, timed out
Root-NFS: Unable to get mountd port number from server, using default
mount: server 0.0.0.0 not responding, timed out
Root-NFS: Server returned error -5 while mounting /tftpboot/$(nfshost):$(rootpa
th)
VFS: Unable to mount root fs via NFS, trying floppy.
VFS: Cannot open root device "nfs" or unknown-block(2,0)
Please append a correct "root=" boot option
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)

  • Leon from Leopard Imaging suggested that I explicitly enter the nfshost and rootpath rather than referencing them through a variable. The instructions for Ubuntu show the use of variables. Nonetheless it now works.

    bootargs=console=ttyS0,115200n8 noinitrd rw ip=dhcp root=/dev/nfs nfsroot=$(nfshos
    t):$(rootpath),nolock mem=76M video=davincifb:vid0=OFF:vid1=OFF:osd0=720x576x16,40
    50K dm365_imp.oper_mode=0 davinci_capture.device_type=4