This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C6678: OpenMP project build error

Part Number: TMS320C6678

Tool/software: Code Composer Studio


**** Build of configuration Debug for project image_processing_openmp_evmc6678l ****

"C:\\ti\\ccsv8\\utils\\bin\\gmake" -k all

Webpage Convert
C:/ti/ccsv8/utils/gmake/gmake -C ../webpages/tool/php -j 4
makefile:182: recipe for target 'pre-build' failed
process_begin: CreateProcess(NULL, C:/ti/ccsv8/utils/gmake/gmake -C ../webpages/tool/php -j 4, ...) failed.
make (e=2): 系统找不到指定的文件。

gmake[1]: [pre-build] Error 2 (ignored)

Building file: "../image_processing_openmp_evmc6678l.cfg"
Invoking: XDCtools
"C:/ti/xdctools_3_23_04_60/xs" --xdcpath="C:/ti/bios_6_33_06_50/packages;C:/ti/imglib_c66x_3_1_1_0/packages;C:/ti/omp_1_01_03_02/packages;C:/ti/ipc_3_50_03_04/packages;C:/ti/pdk_C6678_1_1_2_6/packages;C:/ti/ndk_3_40_01_01/packages;C:/ti/mcsdk_2_01_02_06;C:/ti/mcsdk_2_01_02_06/demos;C:/ti/ccsv8/ccs_base;C:/ti/uia_2_30_01_02/packages;C:/ti/openmp_dsp_c667x_2_06_02_01/packages;" xdc.tools.configuro -o configPkg -t ti.targets.elf.C66 -p ti.omp.examples.platforms.evm6678 -r debug -b "C:/ti/mcsdk_2_01_02_06/demos/image_processing/openmp/evmc6678l/platform/config.bld" -c "C:/ti/C6000 Code Generation Tools 7.4.0" --compileOptions "--gcc" "../image_processing_openmp_evmc6678l.cfg"
making package.mak (because of package.bld) ...
configuring image_processing_openmp_evmc6678l.xe66 from package/cfg/image_processing_openmp_evmc6678l_pe66.cfg ...
subdir_rules.mk:12: recipe for target 'build-125481039-inproc' failed
"ti/sdo/ipc/interfaces/ITransport.xdc", line 42: unrecognized attribute (@DirectCall)
js: "C:/ti/mcsdk_2_01_02_06/demos/image_processing/openmp/evmc6678l/image_processing_openmp_evmc6678l.cfg", line 122: xdc.services.global.XDCException: xdc.PACKAGE_REPARSE_FAILED: C:\ti\ipc_3_50_03_04\packages\ti\sdo\ipc\package.xdc found along the package path, but its package files are incompatible with the current tools and could not be regenerated (InternalError: parser failed (pass 2)). The package 'ti.sdo.ipc' must be rebuilt with the current tools.
"./package/cfg/image_processing_openmp_evmc6678l_pe66.cfg", line 204
"./package/cfg/image_processing_openmp_evmc6678l_pe66.cfg", line 283
"./package/cfg/image_processing_openmp_evmc6678l_pe66.cfg", line 191
gmake.exe: *** [package/cfg/image_processing_openmp_evmc6678l_pe66.xdl] Error 1
gmake.exe: *** [package/cfg/image_processing_openmp_evmc6678l_pe66.xdl] Deleting file `package/cfg/image_processing_openmp_evmc6678l_pe66.h'
gmake.exe: *** [package/cfg/image_processing_openmp_evmc6678l_pe66.xdl] Deleting file `package/cfg/image_processing_openmp_evmc6678l_pe66.c'
js: "C:/ti/xdctools_3_23_04_60/packages/xdc/tools/Cmdr.xs", line 51: Error: xdc.tools.configuro: configuration failed due to earlier errors (status = 2); 'linker.cmd' deleted.
gmake[2]: *** [build-125481039-inproc] Error 1
gmake[1]: *** [build-125481039] Error 2
gmake[1]: Target 'main-build' not remade because of errors.
subdir_rules.mk:9: recipe for target 'build-125481039' failed
gmake: *** [all] Error 2
makefile:151: recipe for target 'all' failed

**** Build Finished ****

I didn't modify anything about the project, so what is the problem?

Thanks !!!