This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TDA2EVM5777: VSDK 3.06 - not able to visualize output of nullSrc decode display usecase

Part Number: TDA2EVM5777

Tool/software: Linux

Hello,

This is my environment - Ubuntu 16.04 LTS, Vision SDK Linux 03_06_00_00, boot mode is SD card.

Following the Linux User Guide, I built the Vision SDK. Now I am attempting to visualize the output of UC_nullSrc-decode-display/h264. The required input stream files are copied to SD card -> rootfs -> /home directory. But when I execute the use-case, I see a solid green display and the following messages on the UART console:

 [HOST] [HOST  ]  =========================================
 [HOST] [HOST  ]  Chains Run-time Codec Type Selection Menu
 [HOST] [HOST  ]  =========================================
 [HOST] [HOST  ]  
 [HOST] [HOST  ]  Enter '0' for MJPEG 
 [HOST] [HOST  ]  
 [HOST] [HOST  ]  Enter '1' for H.264 
 [HOST] [HOST  ]  
 [HOST] [HOST  ]  Enter Choice: 
 [HOST] [HOST  ]  
1
 [HOST] [HOST  ]    219.351796 s:  IPC_OUT_0   : Create in progress !!!
 [HOST] [HOST  ]    219.351888 s:  IPC_OUT_0   : Create Done !!!
 [HOST] [IPU2  ]    219.352040 s:  IPC_IN_0   : Create in progress !!!
 [HOST] [IPU2  ]    219.353199 s:  IPC_IN_0   : Create Done !!!
 [HOST] [IPU2  ]    219.353687 s:  DECODE: Create in progress ... !!!
 [HOST] [IPU2  ]    219.785274 s:  DECODE: Creating CH0 of 1920 x 1080 [1] [0],target bitrate = 10000 Kbps ... 
 [HOST] [IPU2  ]    219.786128 s:  DECODE: All CH Create ... DONE !!!
 [HOST] [IPU2  ]    219.788080 s:  DECODE: Create ... DONE !!!
 [HOST] [IPU2  ]    219.788568 s:  VPE: Create in progress !!!
 [HOST] [IPU2  ]    220.021960 s:  VPE: Loading Down-scaling Co-effs
 [HOST] [IPU2  ]    220.022204 s:  VPE: Co-effs Loading ... DONE !!!
 [HOST] [IPU2  ]    220.022448 s:  VPE: Create Done !!!
 [HOST] [IPU2  ]    220.022845 s:  DISPLAY: Create in progress !!!
 [HOST] [IPU2  ]    220.023485 s:  DISPLAY: Create Done !!!
 [HOST] [DSP1  ]    220.124168 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1023 
 [HOST] [DSP1  ]    220.124199 s:  SYSTEM: Heap = LOCAL_L2             @ 0x00800000, Total size = 227264 B (221 KB), Free size = 227264 B (221 KB)
 [HOST] [DSP1  ]    220.124229 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 524288 B (512 KB), Free size = 516016 B (503 KB)
 [HOST] [DSP2  ]    220.124473 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1023 
 [HOST] [DSP2  ]    220.124504 s:  SYSTEM: Heap = LOCAL_L2             @ 0x00800000, Total size = 227264 B (221 KB), Free size = 227264 B (221 KB)
 [HOST] [DSP2  ]    220.124534 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 524288 B (512 KB), Free size = 516016 B (503 KB)
 [HOST] [EVE1  ]    220.125053 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1023 
 [HOST] [EVE1  ]    220.125358 s:  SYSTEM: Heap = LOCAL_L2             @ 0x40020000, Total size = 22528 B (22 KB), Free size = 22528 B (22 KB)
 [HOST] [EVE1  ]    220.125876 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 262144 B (256 KB), Free size = 254160 B (248 KB)
 [HOST] [EVE2  ]    220.126944 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1023 
 [HOST] [EVE2  ]    220.127249 s:  SYSTEM: Heap = LOCAL_L2             @ 0x40020000, Total size = 22528 B (22 KB), Free size = 22528 B (22 KB)
 [HOST] [EVE2  ]    220.127798 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 262144 B (256 KB), Free size = 254160 B (248 KB)
 [HOST] [EVE3  ]    220.128804 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1023 
 [HOST] [HOST  ]    220.137223 s: 
 [HOST] [HOST  ]  
 [HOST] [HOST  ]  ====================
 [HOST] [HOST  ]  Chains Run-time Menu
 [HOST] [HOST  ]  ====================
 [HOST] [HOST  ]  
 [HOST] [HOST  ]  0: Stop Chain
 [HOST] [HOST  ]  
 [HOST] [HOST  ]  p: Print Performance Statistics 
 [HOST] [HOST  ]  
 [HOST] [HOST  ]  Enter Choice: 
 [HOST] [HOST  ]  
 [HOST] [EVE3  ]    220.129201 s:  SYSTEM: Heap = LOCAL_L2             @ 0x40020000, Total size = 22528 B (22 KB), Free size = 22528 B (22 KB)
 [HOST] [EVE3  ]    220.129750 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 262144 B (256 KB), Free size = 254160 B (248 KB)
 [HOST] [EVE4  ]    220.130787 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1023 
 [HOST] [EVE4  ]    220.131092 s:  SYSTEM: Heap = LOCAL_L2             @ 0x40020000, Total size = 22528 B (22 KB), Free size = 22528 B (22 KB)
 [HOST] [EVE4  ]    220.131641 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 262144 B (256 KB), Free size = 254160 B (248 KB)
 [HOST] [IPU2  ]    220.132495 s:  SYSTEM: SW Message Box Msg Pool, Free Msg Count = 1023 
 [HOST] [IPU2  ]    220.132617 s:  SYSTEM: Heap = LOCAL_DDR            @ 0x00000000, Total size = 262144 B (256 KB), Free size = 247896 B (242 KB)
 [HOST] [IPU2  ]    220.132800 s:  SYSTEM: Heap = SR_OCMC              @ 0x00000000, Total size = 0 B (0 KB), Free size = 0 B (0 KB)
 [HOST] [IPU2  ]    220.132953 s:  SYSTEM: Heap = SR_DDR_CACHED        @ 0x84203000, Total size = 314572800 B (300 MB), Free size = 258926592 B (246 MB)
 [HOST] [IPU2  ]    220.133136 s:  SYSTEM: Heap = SR_DDR_NON_CACHED    @ 0xa0100000, Total size = 1045376 B (0 MB), Free size = 851840 B (0 MB)
 [HOST] [IPU2  ]    220.133593 s:  DISPLAY: Start in progress !!!
 [HOST] [IPU2  ]    220.133654 s:  DISPLAY: Start Done !!!
 ASSERT (nullSrcLink_tsk.c|NullSrcLink_fillData|202)

What am I doing wrong here?

 

Thank you.