Part Number: AM5716
Hi,
MPU connects EMIF directly (not via L3_MAIN interconnect) in "Figure 2-1. Interconnect Overview" of TRM(spruhz7h.pdf).
1) Could you please tell me why direct path exists between MPU and EMIF? Does it mean to prevent bus contention in L3_MAIN interconnect?
2) Could you please tell me which address MPU accesses if MPU accesses EMIF directly?
Should I use Q10(0x02 8000 0000-0x02 BFFF FFFF) and Q11(0x02 C000 0000-0x02 FFFF FFFF) instead of Q2(0x8000 0000-0xBFFF FFFF) and Q3(0xC000 0000-0xFFFF FFFF) in Table 2-8?
3) There is described 3 EMIF1_SDRAM_CS0 area (Q8: 0x02 0000 0000-0x023FFF FFFF, Q10: 0x02 8000 0000-0x02 BFFF FFFF, Q11: 0x02 C000 0000-0x02 FFFF FFFF) in Table 2-8. Could you please tell me the difference between Q8 and Q10/11?
Best Regards,
Masa.O