Other Parts Discussed in Thread: PROFIBUS
Hi,
We have bought idk am5728 and we use Linux RT of you realeses.
Please provide us an example of how to use profibus dpv0, even a simple one of how to read via profibus.
Thanks in advance
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
You also have the PRU ICSS Industrial firmware, right? If not you can download and install it from here:
See also the developers guide:
For linux see:
Best Regards,
Yordan
My linux RT version is
Linux am57xx-evm 4.19.38-rt19-g1224cd679e #1 SMP PREEMPT RT Sat Jul 6 20:40:03 UTC 2019 armv7l GNU/Linux
I cannot install your recommendations and I get error:
sh: ./PRU-ICSS-Profibus_Master-01.00.01.00-Linux-x86-Install.bin: cannot execute binary file: Exec format error
I googled it and it mentions that I want to run a 64-bit program in a 32 bit system.
Could you please advice me on that?
Thanks in Advance
Angelos Athanasiadis said:My linux RT version is
Linux am57xx-evm 4.19.38-rt19-g1224cd679e #1 SMP PREEMPT RT Sat Jul 6 20:40:03 UTC 2019 armv7l GNU/Linux
I cannot install your recommendations and I get error:
sh: ./PRU-ICSS-Profibus_Master-01.00.01.00-Linux-x86-Install.bin: cannot execute binary file: Exec format error
I googled it and it mentions that I want to run a 64-bit program in a 32 bit system.
Could you please advice me on that?
Thanks in Advance
Hi,
Do you have any feedback on this issue?
Thanks
Hi Angelos,
We don't have a Profibus version for RT Linux, instead, we have the Profibus master/slave with TI-RTOS:
http://processors.wiki.ti.com/index.php/PRU_ICSS_Profibus_Master
http://processors.wiki.ti.com/index.php/PRU_ICSS_Profibus_Slave
Regards,
Garrett
Hi,
We use linux RT to the idk. Could we maybe use at the same time TI-RTOS to c66 in order to implement profibus there?
If yes, could you provide us a link or some advice on the matter?
Thanks in advance
Angelos,
Yes, it's possible to use C66x with TI-RTOS for profibus. The discussion on porting EtherCAT to DSP may help: https://e2e.ti.com/support/processors/f/791/p/695117/2586331#pi320966=1
Regards,
Garrett