Part Number: TMDXIDK57X-LCD
Tool/software: TI C/C++ Compiler
Hello everyone,
I am trying to add a probe to a pad in GStreamer in the following code, I can successfully compile and run the code on my vbox Ubuntu, but when I try to run it on my IDK nothing happens and LCD remains black,
#include <gst/gst.h>
#include <iostream>
static GstPadProbeReturn cb_onProbe(GstPad * Ipad , GstPadProbeInfo* Iinfo , gpointer userData ){
std::cout << "cb\n";
}
int main(int argc , char* argv[]){
GstElement *myPipeline, *myTextOverlay , *myVideoSrc, *myVideoSink , *myCapsFilters;
GMainLoop * myLoop;
GstCaps *myCaps;
GstPad * mySrcPad ;
gst_init(&argc , &argv);
myVideoSrc = gst_element_factory_make("videotestsrc", "mySrcVid");
myVideoSink = gst_element_factory_make("autovideosink", "mySinkVid");
myTextOverlay = gst_element_factory_make("textoverlay", "myTxtOvr");
myCapsFilters = gst_element_factory_make("capsfilter", "myCpsFltr");
myPipeline = gst_pipeline_new("myPipe");
if( !myPipeline || !myTextOverlay || !myVideoSrc || !myVideoSink || !myCapsFilters){
std::cout << "failed to create some elements!!\n";
return -1;
}
myCaps = gst_caps_new_simple("video/x-raw",
"width",G_TYPE_INT, 640,
"height",G_TYPE_INT, 480,
"framerate",GST_TYPE_FRACTION, 1,1,
NULL
);
g_object_set(G_OBJECT(myCapsFilters) , "caps" , myCaps , NULL);
gst_bin_add_many(GST_BIN(myPipeline) , myVideoSrc ,myCapsFilters, myTextOverlay ,myVideoSink, NULL );
if(gst_element_link_many(myVideoSrc , myCapsFilters , myTextOverlay ,myVideoSink, NULL) != true){
std::cout << "failed to link some elements!!\n";
return -1;
}
g_object_set(myTextOverlay , "text", "my text", NULL);
mySrcPad = gst_element_get_static_pad(myVideoSrc , "src");
gst_pad_add_probe(mySrcPad , GST_PAD_PROBE_TYPE_BUFFER , (GstPadProbeCallback)cb_onProbe, NULL , NULL );
GstStateChangeReturn retVal = gst_element_set_state(myPipeline , GST_STATE_PLAYING);
if(retVal == GST_STATE_CHANGE_FAILURE){
std::cout << "failed to playing!\n";
return -1;
}
myLoop = g_main_loop_new(NULL, false);
std::cout << "running...\n";
g_main_loop_run(myLoop);
return 0;
}
even if I comment the line with gst_pad_add_probe (line 50), the program works correctly in IDK (without calling the callback function). I'm using processor sdk linux rt 4.9.
any help would be appriciated,
B.R,
Alex.