Part Number: TDA2EVM5777
Other Parts Discussed in Thread: DRA742, DRA752
Tool/software: TI C/C++ Compiler
Hi,
I'm trying to boot custom board which is based on TDA2x EVM board.
Sometimes, it goes to mount root file system but seems like wait infinitely some task. (it doesn't show root login prompt)
And it often shows kernel panic messages.
I attached my kernel log.
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpuset
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4.4.84 (yoo@yoo-VirtualBox) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #75 SMP PREEMPT Mon Oct 7 15:28:56 KST 2019
[ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[ 0.000000] Machine model: TI DRA742
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000040300000, size 3 MiB
[ 0.000000] Reserved memory: initialized node cmem@40300000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: regions without no-map are not yet supported
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 80 MiB
[ 0.000000] Reserved memory: initialized node ipu2_cma@95800000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x000000009e000000, size 32 MiB
[ 0.000000] Reserved memory: initialized node ipu1_cma@9d000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: regions without no-map are not yet supported
[ 0.000000] Reserved memory: created CMA memory pool at 0x00000000a1000000, size 32 MiB
[ 0.000000] Reserved memory: initialized node dsp1_cma@99000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x00000000a3000000, size 32 MiB
[ 0.000000] Reserved memory: initialized node dsp2_cma@9f000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: regions without no-map are not yet supported
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a9000000, size 32 MiB
[ 0.000000] Reserved memory: initialized node cmem@A9000000, compatible id shared-dma-pool
[ 0.000000] cma: Reserved 64 MiB at 0x00000000bbc00000
[ 0.000000] Forcing write-allocate cache policy for SMP
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] OMAP4: Map 0x00000000bfd00000 to fe600000 for dram barrier
[ 0.000000] DRA752 ES1.1
[ 0.000000] PERCPU: Embedded 11 pages/cpu @ef62a000 s14912 r8192 d21952 u45056
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 251456
[ 0.000000] Kernel command line: console=ttyO0,115200n8 vram=16M root=PARTUUID=a760f24c-02 rw rootwait ip=none mem=1024M cma=64M
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 353148K/1012736K available (6671K kernel code, 320K rwdata, 2396K rodata, 336K init, 290K bss, 413828K reserved, 245760K cma-reserved, 193536K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc08e302c (9069 kB)
[ 0.000000] .init : 0xc08e4000 - 0xc0938000 ( 336 kB)
[ 0.000000] .data : 0xc0938000 - 0xc0988220 ( 321 kB)
[ 0.000000] .bss : 0xc098a000 - 0xc09d2880 ( 291 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 32.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] ti_dt_clocks_register: failed to lookup clock node gmac_gmii_ref_clk_div
[ 0.000000] OMAP clockevent source: timer1 at 32786 Hz
[ 0.000000] Architected cp15 timer(s) running at 6.14MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
[ 0.000005] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
[ 0.000015] Switching to timer-based delay loop, resolution 162ns
[ 0.000331] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[ 0.000339] OMAP clocksource: 32k_counter at 32768 Hz
[ 0.000782] Console: colour dummy device 80x30
[ 0.000798] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000804] This ensures that you still see kernel messages. Please
[ 0.000809] update your kernel commandline.
[ 0.000823] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
[ 0.000835] pid_max: default: 32768 minimum: 301
[ 0.000934] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000944] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001485] Initializing cgroup subsys io
[ 0.001501] Initializing cgroup subsys memory
[ 0.001525] Initializing cgroup subsys devices
[ 0.001538] Initializing cgroup subsys freezer
[ 0.001548] Initializing cgroup subsys perf_event
[ 0.001560] Initializing cgroup subsys pids
[ 0.001587] CPU: Testing write buffer coherency: ok
[ 0.001785] /cpus/cpu@0 missing clock-frequency property
[ 0.001802] /cpus/cpu@1 missing clock-frequency property
[ 0.001812] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.001848] Setting up static identity map for 0x80008380 - 0x800083e0
[ 0.080068] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[ 0.080137] Brought up 2 CPUs
[ 0.080150] SMP: Total of 2 processors activated (24.59 BogoMIPS).
[ 0.080156] CPU: All CPU(s) started in HYP mode.
[ 0.080162] CPU: Virtualization extensions available.
[ 0.080537] devtmpfs: initialized
[ 0.109629] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[ 0.110600] omap_hwmod: l3_main_2 using broken dt data from ocp
[ 0.313684] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.313705] futex hash table entries: 512 (order: 3, 32768 bytes)
[ 0.318769] pinctrl core: initialized pinctrl subsystem
[ 0.319630] NET: Registered protocol family 16
[ 0.320610] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.350239] cpuidle: using governor ladder
[ 0.380260] cpuidle: using governor menu
[ 0.388795] OMAP GPIO hardware version 0.1
[ 0.395239] irq: no irq domain found for /ocp/l4@4a000000/scm@2000/pinmux@1400 !
[ 0.418548] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[ 0.418559] hw-breakpoint: maximum watchpoint size is 8 bytes.
[ 0.419033] omap4_sram_init:Unable to allocate sram needed to handle errata I688
[ 0.419042] omap4_sram_init:Unable to get sram pool needed to handle errata I688
[ 0.419629] OMAP DMA hardware revision 0.0
[ 0.461517] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver (LinkedList1/2/3 supported)
[ 0.462644] edma 43300000.edma: memcpy is disabled
[ 0.467335] edma 43300000.edma: TI EDMA DMA engine driver
[ 0.471678] omap-iommu 40d01000.mmu: 40d01000.mmu registered
[ 0.471854] omap-iommu 40d02000.mmu: 40d02000.mmu registered
[ 0.472022] omap-iommu 58882000.mmu: 58882000.mmu registered
[ 0.472175] omap-iommu 55082000.mmu: 55082000.mmu registered
[ 0.472463] omap-iommu 41501000.mmu: 41501000.mmu registered
[ 0.472651] omap-iommu 41502000.mmu: 41502000.mmu registered
[ 0.475621] palmas 0-0058: IRQ missing: skipping irq request
[ 0.491074] palmas 0-0058: Muxing GPIO 2e, PWM 0, LED 0
[ 0.552726] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
[ 0.553147] omap_i2c 48060000.i2c: bus 2 rev0.12 at 400 kHz
[ 0.553337] media: Linux media interface: v0.10
[ 0.553389] Linux video capture interface: v2.00
[ 0.553432] pps_core: LinuxPPS API ver. 1 registered
[ 0.553439] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.553464] PTP clock support registered
[ 0.553514] EDAC MC: Ver: 3.0.0
[ 0.554266] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
[ 0.554563] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400
[ 0.554881] Advanced Linux Sound Architecture Driver Initialized.
[ 0.555736] clocksource: Switched to clocksource arch_sys_counter
[ 0.566198] NET: Registered protocol family 2
[ 0.566691] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.566754] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.566879] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.566927] UDP hash table entries: 512 (order: 2, 16384 bytes)
[ 0.566958] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[ 0.567164] NET: Registered protocol family 1
[ 0.567428] RPC: Registered named UNIX socket transport module.
[ 0.567438] RPC: Registered udp transport module.
[ 0.567444] RPC: Registered tcp transport module.
[ 0.567450] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.568438] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
[ 0.578433] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.579085] NFS: Registering the id_resolver key type
[ 0.579114] Key type id_resolver registered
[ 0.579122] Key type id_legacy registered
[ 0.579180] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.580451] bounce: pool size: 64 pages
[ 0.580598] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247)
[ 0.580613] io scheduler noop registered
[ 0.580626] io scheduler deadline registered
[ 0.580659] io scheduler cfq registered (default)
[ 0.584388] pinctrl-single 4a003400.pinmux: 282 pins at pa fc003400 size 1128
[ 0.587568] PCI host bridge /ocp/axi@0/pcie_rc@51000000 ranges:
[ 0.587580] No bus range found for /ocp/axi@0/pcie_rc@51000000, using [bus 00-ff]
[ 0.587613] IO 0x20003000..0x20012fff -> 0x00000000
[ 0.587634] MEM 0x20013000..0x2fffffff -> 0x20013000
[ 0.617563] dra7-pcie 51000000.pcie_rc: link is not up
[ 0.617733] dra7-pcie 51000000.pcie_rc: PCI host bridge to bus 0000:00
[ 0.617746] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 0.617756] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
[ 0.617766] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
[ 0.618170] PCI: bus0: Fast back to back transfers disabled
[ 0.618297] PCI: bus1: Fast back to back transfers enabled
[ 0.618380] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff]
[ 0.618394] pci 0000:00:00.0: BAR 1: assigned [mem 0x20020000-0x2002ffff]
[ 0.618406] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 0.618631] pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt
[ 0.679068] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.682432] 4806a000.serial: ttyS0 at MMIO 0x4806a000 (irq = 301, base_baud = 3000000) is a 8250
[ 1.672836] console [ttyS0] enabled
[ 1.677231] 4806c000.serial: ttyS1 at MMIO 0x4806c000 (irq = 302, base_baud = 3000000) is a 8250
[ 1.686933] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 303, base_baud = 3000000) is a 8250
[ 1.696907] [drm] Initialized drm 1.1.0 20060810
[ 1.702406] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 1.709091] [drm] No driver support for vblank timestamp query.
[ 1.715217] [drm] Initialized vdrm 1.0.0 20110917 on minor 0
[ 1.728130] loop: module loaded
[ 1.731619] vmemexp device MAJOR num = 245
[ 1.735791] vmemexp class registered
[ 1.739509] /dev/vmemexp device registered
[ 1.743625] ioctl DBUFIOC_EXPORT_VIRTMEM = -1072899120
[ 1.752179] m25p80 spi32766.0: s25fl256s1 (32768 Kbytes)
[ 1.757597] 7 ofpart partitions found on MTD device spi32766.0
[ 1.763456] Creating 7 MTD partitions on "spi32766.0":
[ 1.768635] 0x000000000000-0x000000040000 : "QSPI.SPL"
[ 1.774766] 0x000000040000-0x000000140000 : "QSPI.u-boot"
[ 1.781146] 0x000000140000-0x0000001c0000 : "QSPI.u-boot-spl-os"
[ 1.788097] 0x0000001c0000-0x0000001d0000 : "QSPI.u-boot-env"
[ 1.794758] 0x0000001d0000-0x0000001e0000 : "QSPI.u-boot-env.backup1"
[ 1.802155] 0x0000001e0000-0x0000009e0000 : "QSPI.kernel"
[ 1.808502] 0x0000009e0000-0x000002000000 : "QSPI.file-system"
[ 1.816277] libphy: Fixed MDIO Bus: probed
[ 1.865768] davinci_mdio 48485000.mdio: davinci mdio revision 1.6
[ 1.871891] davinci_mdio 48485000.mdio: detected phy mask fffffffb
[ 1.880227] libphy: 48485000.mdio: probed
[ 1.884258] davinci_mdio 48485000.mdio: phy[2]: device 48485000.mdio:02, driver unknown
[ 1.892956] cpsw 48484000.ethernet: Detected MACID = 7c:66:9d:ee:81:8c
[ 1.899650] cpsw 48484000.ethernet: cpts: overflow check period 800
[ 1.906669] cpsw 48484000.ethernet: cpsw: Detected MACID = 7c:66:9d:ee:81:8d
[ 1.915244] mousedev: PS/2 mouse device common for all mice
[ 1.921432] i2c /dev entries driver
[ 1.930412] evm_3v3_sw: supplied by sysen1
[ 1.976856] ledtrig-cpu: registered to indicate activity on CPUs
[ 1.997513] davinci-mcasp 48468000.mcasp: ERRATA i868 workaround is enabled
[ 2.004707] davinci-mcasp 4847c000.mcasp: invalid tdm slots: 0
[ 2.012187] NET: Registered protocol family 10
[ 2.027538] sit: IPv6 over IPv4 tunneling driver
[ 2.032723] NET: Registered protocol family 17
[ 2.037532] Key type dns_resolver registered
[ 2.041948] omap_voltage_late_init: Voltage driver support not added
[ 2.048843] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 2.055051] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 2.061747] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 2.067996] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 2.076165] Power Management for TI OMAP4+ devices.
[ 2.081209] Unable to handle kernel NULL pointer dereference at virtual address 00000188
[ 2.089358] pgd = c0003000
[ 2.092074] [00000188] *pgd=80000080004003, *pmd=00000000
[ 2.097546] Internal error: Oops: a06 [#1] PREEMPT SMP ARM
[ 2.103049] Modules linked in:
[ 2.106121] CPU: 0 PID: 1 Comm: swapper/0 Not tainted 4.4.84 #75
[ 2.112150] Hardware name: Generic DRA74X (Flattened Device Tree)
[ 2.118265] task: ef078000 ti: ef062000 task.ti: ef062000
[ 2.123687] PC is at omap3_dpll_allow_idle+0x4/0x7c
[ 2.128585] LR is at omap2_clk_enable_autoidle_all+0x48/0xc0
[ 2.134264] pc : [<c0520ec8>] lr : [<c051e8a4>] psr: a0000113
[ 2.134264] sp : ef063e88 ip : ef063e88 fp : ef063ea4
[ 2.145788] r10: 00000000 r9 : c08e4600 r8 : 000000b2
[ 2.151030] r7 : eeb1f880 r6 : c0978fd4 r5 : c0978fcc r4 : ef023c00
[ 2.157583] r3 : c0520ec4 r2 : ef0027c0 r1 : 000001a8 r0 : ef023c00
[ 2.164136] Flags: NzCv IRQs on FIQs on Mode SVC_32 ISA ARM Segment kernel
[ 2.171471] Control: 30c5387d Table: 80003000 DAC: fffffffd
[ 2.177236] Process swapper/0 (pid: 1, stack limit = 0xef062210)
[ 2.183265] Stack: (0xef063e88 to 0xef064000)
[ 2.187637] 3e80: c093d6f0 c08e6b5c c093d6f0 eeb1f880 ef063eb4 ef063ea8
[ 2.195848] 3ea0: c08ed8c8 c051e868 ef063ecc ef063eb8 c08e6b84 c08ed8b4 c093d6f0 c08e6b5c
[ 2.204056] 3ec0: ef063f4c ef063ed0 c000982c c08e6b68 ef063ef4 ef063ee0 c08e461c c02b90fc
[ 2.212265] 3ee0: ef643018 c06abdfc ef063f4c ef063ef8 c004fc2c c08e460c ef063f34 c0826c78
[ 2.220476] 3f00: c0826cc4 c082666c 00000007 00000007 00000000 c08e0e4c c081c284 00000000
[ 2.228684] 3f20: 00000478 c098a000 c098a000 c09339b8 c0925838 000000b2 c08e4600 00000008
[ 2.236894] 3f40: ef063f94 ef063f50 c08e4f68 c00097a0 00000007 00000007 00000000 c08e4600
[ 2.245102] 3f60: 03000741 c08e0e4c 406a8109 c098a000 c0684f60 00000000 00000000 00000000
[ 2.253311] 3f80: 00000000 00000000 ef063fac ef063f98 c0684f78 c08e4da0 00000000 c0684f60
[ 2.261521] 3fa0: 00000000 ef063fb0 c000fb88 c0684f6c 00000000 00000000 00000000 00000000
[ 2.269730] 3fc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000
[ 2.277940] 3fe0: 00000000 00000000 00000000 00000000 00000013 00000000 00264428 11168530
[ 2.286148] Backtrace:
[ 2.288612] [<c051e85c>] (omap2_clk_enable_autoidle_all) from [<c08ed8c8>] (dra7xx_init_late+0x20/0x24)
[ 2.298040] r7:eeb1f880 r6:c093d6f0 r5:c08e6b5c r4:c093d6f0
[ 2.303749] [<c08ed8a8>] (dra7xx_init_late) from [<c08e6b84>] (init_machine_late+0x28/0x98)
[ 2.312136] [<c08e6b5c>] (init_machine_late) from [<c000982c>] (do_one_initcall+0x98/0x1e4)
[ 2.320517] r5:c08e6b5c r4:c093d6f0
[ 2.324120] [<c0009794>] (do_one_initcall) from [<c08e4f68>] (kernel_init_freeable+0x1d4/0x268)
[ 2.332849] r10:00000008 r9:c08e4600 r8:000000b2 r7:c0925838 r6:c09339b8 r5:c098a000
[ 2.340740] r4:c098a000
[ 2.343289] [<c08e4d94>] (kernel_init_freeable) from [<c0684f78>] (kernel_init+0x18/0xf4)
[ 2.351496] r10:00000000 r9:00000000 r8:00000000 r7:00000000 r6:00000000 r5:c0684f60
[ 2.359386] r4:c098a000
[ 2.361934] [<c0684f60>] (kernel_init) from [<c000fb88>] (ret_from_fork+0x14/0x2c)
[ 2.369529] r5:c0684f60 r4:00000000
[ 2.373130] Code: e263301f e1a00330 e89da830 e1a0c00d (e92dd8f0)
[ 2.379331] ---[ end trace 7829fa0c9fa85dd3 ]---
[ 2.383977] Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b
[ 2.383977]
[ 2.393148] CPU1: stopping
[ 2.395866] CPU: 1 PID: 6 Comm: kworker/u4:0 Tainted: G D 4.4.84 #75
[ 2.403375] Hardware name: Generic DRA74X (Flattened Device Tree)
[ 2.409493] Workqueue: kmmcd mmc_rescan
[ 2.413346] Backtrace:
[ 2.415813] [<c00131d4>] (dump_backtrace) from [<c00133d0>] (show_stack+0x18/0x1c)
[ 2.423411] r7:ef09bce0 r6:20000193 r5:00000000 r4:c0957810
[ 2.429123] [<c00133b8>] (show_stack) from [<c02b21a8>] (dump_stack+0x8c/0xa0)
[ 2.436377] [<c02b211c>] (dump_stack) from [<c0016520>] (handle_IPI+0x184/0x198)
[ 2.443799] r7:ef09bce0 r6:00000000 r5:00000001 r4:c0935424
[ 2.449506] [<c001639c>] (handle_IPI) from [<c00094c4>] (gic_handle_irq+0x78/0x7c)
[ 2.457102] r7:fa212000 r6:ef09bce0 r5:fa21200c r4:c093a8ec
[ 2.462806] [<c000944c>] (gic_handle_irq) from [<c0013ec0>] (__irq_svc+0x40/0x74)
[ 2.470317] Exception stack(0xef09bce0 to 0xef09bd28)
[ 2.475389] bce0: 0000140b 00000000 df54e710 c050239c c09bd428 00001803 031a2956 066665b0
[ 2.483596] bd00: ef09bde0 00000000 00000001 ef09bd3c ef09bd40 ef09bd30 c0016f30 c05023a8
[ 2.491803] bd20: a0000013 ffffffff
[ 2.495300] r9:00000000 r8:ef09bde0 r7:ef09bd14 r6:ffffffff r5:a0000013 r4:c05023a8
[ 2.503114] [<c050239c>] (arch_counter_get_cntpct) from [<c0016f30>] (arch_timer_read_counter_long+0x1c/0x20)
[ 2.513070] [<c0016f14>] (arch_timer_read_counter_long) from [<c02aff78>] (__timer_delay+0x54/0x64)
[ 2.522151] [<c02aff24>] (__timer_delay) from [<c02affb0>] (__timer_const_udelay+0x28/0x2c)
[ 2.530533] r7:066665b0 r6:c09577f8 r5:eeaf8800 r4:000001e6
[ 2.536242] [<c02aff88>] (__timer_const_udelay) from [<c04e4f2c>] (__mmc_start_request+0x88/0xdc)
[ 2.545149] [<c04e4ea4>] (__mmc_start_request) from [<c04e5078>] (mmc_start_request+0xf8/0x120)
[ 2.553878] r9:00000000 r8:00000008 r7:00000000 r6:eeaf8800 r5:eeaf8800 r4:ef09bde0
[ 2.561687] [<c04e4f80>] (mmc_start_request) from [<c04e5138>] (__mmc_start_req+0x50/0x70)
[ 2.569981] r5:ef09bdf0 r4:ef09bde0
[ 2.573582] [<c04e50e8>] (__mmc_start_req) from [<c04e56e8>] (mmc_wait_for_cmd+0x60/0x8c)
[ 2.581789] r7:00000000 r6:00000000 r5:eeaf8800 r4:ef09be2c
[ 2.587496] [<c04e5688>] (mmc_wait_for_cmd) from [<c04f00d4>] (mmc_io_rw_direct_host+0x9c/0x138)
[ 2.596313] r6:eeaf8800 r5:00000c08 r4:80000c08
[ 2.600967] [<c04f0038>] (mmc_io_rw_direct_host) from [<c04f05d4>] (sdio_reset+0x5c/0x64)
[ 2.609173] r10:ef09c000 r9:00000000 r8:c06f5bd4 r7:c06f5bc8 r6:eeaf8800 r5:00061a80
[ 2.617065] r4:eeaf8800
[ 2.619612] [<c04f0578>] (sdio_reset) from [<c04e7cb0>] (mmc_rescan+0x274/0x318)
[ 2.627032] r4:eeaf8a58
[ 2.629584] [<c04e7a3c>] (mmc_rescan) from [<c004a6b4>] (process_one_work+0x124/0x3f4)
[ 2.637528] r9:00000000 r8:ef32d200 r7:00000000 r6:ef09c000 r5:ef092100 r4:eeaf8a58
[ 2.645337] [<c004a590>] (process_one_work) from [<c004a9d0>] (worker_thread+0x4c/0x524)
[ 2.653456] r10:ef09c000 r9:ef092100 r8:00000088 r7:ef09a000 r6:ef09c014 r5:ef092118
[ 2.661345] r4:ef09c000
[ 2.663895] [<c004a984>] (worker_thread) from [<c0050508>] (kthread+0x100/0x118)
[ 2.671316] r10:00000000 r9:00000000 r8:c004a984 r7:ef092100 r6:ef09a000 r5:ef05f740
[ 2.679204] r4:00000000
[ 2.681753] [<c0050408>] (kthread) from [<c000fb88>] (ret_from_fork+0x14/0x2c)
[ 2.688999] r8:00000000 r7:00000000 r6:00000000 r5:c0050408 r4:ef05f740
[ 2.695760] ---[ end Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b
[ 2.695760]
The point of occuring error message is not fixed.(sometimes rcu_preempt, of_fdt_raw_init, or others)
How can i resolve this problem?
I'm using mmc device 0 which indicates SD card. (it doesn't have eMMC);
Thanks and Regards,
Yoo