This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA72XEVM: Traditional Qt SDK approach with Yocto gives "Could not load spec_pre.prf" in TI SDK

Part Number: DRA72XEVM


I am trying to generate and use a Qt SDK with extra packages in Arago Distro for my Jacinto 6 ES1.0 board using Processor SDK 5.00.

Traditionally with Yocto, you either use "inherit populate_sdk_qt5" in a recipe or simply do "bitbake meta-toolchain-qt5" in order to generate a Qt SDK.

Then you would install the SDK to a location and source the "environment-setup" script and then continue doing "qmake" and "make".

For various boards including Yocto reference boards I have used this approach and did not encounter any problems.

I can see that these approaches are not working out of the box for the TI SDK, TI implemented their own version of dealing with the SDK packages.

Noticing this, I decided to use "bitbake meta-arago-toolchain-tisdk", but modify sdk packagegroups.

I added my regular packages to meta-arago-extras/recipes-core/packagegroups/packagegroup-arago-standalone-sdk-target.bb

I added qt-based extra packages to meta-arago-extras/recipes-core/packagegroups/packagegroup-arago-qte-toolchain-target.bb

Compiling and installing SDK, then sourcing "/usr/local/arago-2018.10/environment-setup"; I get the following error when I try to run "qmake" in a project.

Cannot find feature spec_pre.prf

Furthermore, I noticed some anomalities with "qmake -query" in the sourced environment. The environment points to the the folders that are not in the actual SDK sysroot, but rather in recipe-sysroot host.

qmake -query
QT_SYSROOT:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot
QT_INSTALL_PREFIX:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr
QT_INSTALL_PREFIX/raw:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr
QT_INSTALL_ARCHDATA:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib
QT_INSTALL_ARCHDATA/raw:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib
QT_INSTALL_ARCHDATA/get:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib
QT_INSTALL_ARCHDATA/src:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib
QT_INSTALL_DATA:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/share
QT_INSTALL_DATA/raw:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/share
QT_INSTALL_DATA/get:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/share
QT_INSTALL_DATA/src:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/share
QT_INSTALL_DOCS:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/share/doc
QT_INSTALL_DOCS/raw:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/share/doc
QT_INSTALL_DOCS/get:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/share/doc
QT_INSTALL_DOCS/src:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/share/doc
QT_INSTALL_HEADERS:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/include
QT_INSTALL_HEADERS/raw:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/include
QT_INSTALL_HEADERS/get:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/include
QT_INSTALL_HEADERS/src:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/include
QT_INSTALL_LIBS:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib
QT_INSTALL_LIBS/raw:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib
QT_INSTALL_LIBS/get:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib
QT_INSTALL_LIBS/src:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib
QT_INSTALL_LIBEXECS:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib/libexec
QT_INSTALL_LIBEXECS/raw:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib/libexec
QT_INSTALL_LIBEXECS/get:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib/libexec
QT_INSTALL_LIBEXECS/src:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib/libexec
QT_INSTALL_BINS:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/bin
QT_INSTALL_BINS/raw:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/bin
QT_INSTALL_BINS/get:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/bin
QT_INSTALL_BINS/src:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/bin
QT_INSTALL_TESTS:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/share/tests
QT_INSTALL_TESTS/raw:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/share/tests
QT_INSTALL_TESTS/get:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/share/tests
QT_INSTALL_TESTS/src:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/share/tests
QT_INSTALL_PLUGINS:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib/plugins
QT_INSTALL_PLUGINS/raw:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib/plugins
QT_INSTALL_PLUGINS/get:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib/plugins
QT_INSTALL_PLUGINS/src:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib/plugins
QT_INSTALL_IMPORTS:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib/imports
QT_INSTALL_IMPORTS/raw:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib/imports
QT_INSTALL_IMPORTS/get:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib/imports
QT_INSTALL_IMPORTS/src:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib/imports
QT_INSTALL_QML:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib/qml
QT_INSTALL_QML/raw:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib/qml
QT_INSTALL_QML/get:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib/qml
QT_INSTALL_QML/src:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib/qml
QT_INSTALL_TRANSLATIONS:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/share/translations
QT_INSTALL_TRANSLATIONS/raw:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/share/translations
QT_INSTALL_TRANSLATIONS/get:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/share/translations
QT_INSTALL_TRANSLATIONS/src:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/share/translations
QT_INSTALL_CONFIGURATION:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/etc
QT_INSTALL_CONFIGURATION/raw:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/etc
QT_INSTALL_EXAMPLES:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/share/examples
QT_INSTALL_EXAMPLES/raw:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/share/examples
QT_INSTALL_EXAMPLES/get:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/share/examples
QT_INSTALL_EXAMPLES/src:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/share/examples
QT_INSTALL_DEMOS:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/share/examples
QT_INSTALL_DEMOS/raw:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/share/examples
QT_INSTALL_DEMOS/get:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/share/examples
QT_INSTALL_DEMOS/src:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/share/examples
QT_HOST_PREFIX:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr
QT_HOST_DATA:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib
QT_HOST_BINS:/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/bin
QT_HOST_LIBS:/projects/jacinto6bsp/ti-processor-sdk-linux-automotive-dra7xx-evm-5_00_00_01/yocto-layers/build/arago-tmp-external-linaro-toolchain/work/x86_64-nativesdk-arago-linux/nativesdk-qtbase/5.12.5+gitAUTOINC+abfb1b8665-r0/recipe-sysroot/tmp/xxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxxx/yyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyyy/sysroots/x86_64-arago-linux/usr/lib
QMAKE_SPEC:linux-oe-g++
QMAKE_XSPEC:linux-oe-g++
QMAKE_VERSION:3.1
QT_VERSION:5.12.5

To be honest, this seems a bit different to me than your usual Yocto SDK, that is why I need to get some expert help.

How do I make use of these info and get rid of the annoying "spec_pre.prf" error. Thank you very much in advance.