This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6748: USB0_VBUS overvoltage & esd protection

Part Number: TMS320C6748
Other Parts Discussed in Thread: TPS65070

Hi

We are looking for the right/best solution for protecting the USB0_VBUS pin against over/under voltage (usb device mode only)

and we need some more information on this pin than those available in the technical datasheet (eg. SPRS947), like:

- USB0_VBUS Maximum Input current

- Does USB0_VBUS include clamping diodes?

- If yes, what is the maximum clamping current

- Is possible to have an internal schematic diagram for this input

Regards,

Bruno