This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: Processor recommendation



Hi,

Looking for the microcontroller from TI which is similar to mimxrt1050 from NXP. Please find my requirements below and do suggest the best one.

* Dual Core(Optional) High speed  
* Security (secure boot,trust zone and data encryption), HSM, Cryptography
* protocols(TCP/HTTP/HTTPS/MQTP)
* Free RTOS if it is micro controller 
* Standard RTOS (like eCos, LynxOS, QNX, WindowsCE, RTLinux etc.) or Linux OS if it is a processor(Processor internal memory 128MB with L1 and L2 Cache)
* Min 2 CAN interface.
* Min 20 GPIO
* PWM IN and OUT 
* Min 6-8 UARTS
* Min 1 SPI
* Min 1 I2C Master
Awaiting for your response.
Thanks & Regards,
Chiranjeevi.