This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/AM3352: Wakeup source configuration

Part Number: AM3352

Tool/software: Code Composer Studio

Hi

Now I have a problem of how to register the wake up source for AM3352,in my project,I use SYS/BIOS.The PDK I using is "pdk_am335x_1_0_14",in this package,under the directory "ti/drv/pm",I can't find the related function that registers wake up source for AM335x.Also,under the directory "ti/starterware/examples/pm",it doesn't have the function to register wake up source.I need a help,what should I do to toregister a wakeup function.Perhaps,you can give me demo project of AM335x power management.

Thank you!