Part Number: TDA4VM
Hi everyone,
I am trying to run the slave as it is described here in spidev. With the following configurations in the device tree.
In:
k3-j731e-main.dtsi:
main_spi6: spi@2160000 {
compatible = "ti,am654-mcspi","ti,omap4-mcspi";
reg = <0x0 0x2160000 0x0 0x400>;
interrupts = <GIC_SPI 190 IRQ_TYPE_LEVEL_HIGH>;
clocks = <&k3_clks 272 1>;
power-domains = <&k3_pds 272 TI_SCI_PD_EXCLUSIVE>;
#address-cells = <1>;
#size-cells = <0>;
spi-slave;
compatible = "spi-slave-time";
};
};
But sadly the slave device does not work as intented and in the Linux I receive the following error. (using dmesg)
[ 4.867325] spi_slave spi3: /interconnect@100000/spi@2160000/spidev@6 is not called 'slave'
[ 4.875665] spi_slave spi3: Failed to create SPI device for /interconnect@100000/spi@2160000/spidev@6
Is there a Driver available for the Slave "spidev" or I should use another way to make it work.
Thanks,
Pouyan