Hi experts,
Is it possible to use IPC between ARM((A15_0 & A15_1) of AM5728?
I'm using ipc_3_50_04_07, but I didn't see any use cases for these.
Best regards,
Sasaki
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sasaki-san,
What is your use case? Are you running RTOS?
In the case of RTOS running on both cores, we can use semaphores, events and mailboxes to communicate between tasks (tasks are implemented as threads in SYS/BIOS). Below is an example I imported from SYS/BIOS.
Does this help?
Regards,
Mike
/* * ======== event.c ======== * The event example shows how to use the ti.sysbios.knl.Event module. * The ti.sysbios.knl.Event module solves the "Wait on Multiple" problem. * In this example a reader task waits on several events. It needs to wake * up when events with Ids Event_Id_0 and Event_Id_1 occur or Event_Id_2 * occurs. The ti.sysbios.knl.Event module provides an Event_pend() API that * allows a task to specify an AND mask and an OR mask. These masks determine * which event(s) must occur before returning from Event_pend(). * * In this example the event related to Event_Id_0 is posted by a Clock * Instance using a call to Event_post(). This is an example of Explicit * posting of events. * Event_Id_1 is posted from within a Semaphore Instance. This is an example * of Implicit posting of events. This is useful when a task needs to wait on * a semaphore and an event which is explicitly posted. * Event_id_2 is posted from within a Mailbox Instance. This is also an * example of Implicit posting of events. */ #include <xdc/std.h> #include <xdc/runtime/System.h> #include <ti/sysbios/BIOS.h> #include <ti/sysbios/knl/Clock.h> #include <ti/sysbios/knl/Task.h> #include <ti/sysbios/knl/Event.h> #include <ti/sysbios/knl/Semaphore.h> #include <ti/sysbios/knl/Mailbox.h> #include <xdc/cfg/global.h> #define NUMMSGS 3 /* number of messages */ #define TIMEOUT 12 /* timeout value */ typedef struct MsgObj { Int id; /* writer task id */ Char val; /* message value */ } MsgObj, *Msg; Clock_Handle clk1, clk2; Event_Handle evt; Mailbox_Handle mbx; Semaphore_Handle sem; Void clk0Fxn(UArg arg0); Void clk1Fxn(UArg arg0); Void reader(UArg arg0, UArg arg1); Void writer(UArg arg0, UArg arg1); /* * ======== main ======== */ Int main() { Clock_Params clkParams; Task_Params tskParams; Mailbox_Params mbxParams; Semaphore_Params semParams; /* Create a one-shot Clock Instance with timeout = 5 system time units */ Clock_Params_init(&clkParams); clkParams.startFlag = TRUE; clk1 = Clock_create(clk0Fxn, 5, &clkParams, NULL); /* Create an one-shot Clock Instance with timeout = 10 system time units */ Clock_Params_init(&clkParams); clkParams.startFlag = TRUE; clk2 = Clock_create(clk1Fxn, 10, &clkParams, NULL); /* create an Event Instance */ evt = Event_create(NULL, NULL); /* create a Semaphore Instance */ Semaphore_Params_init(&semParams); semParams.mode = Semaphore_Mode_BINARY; semParams.event = evt; semParams.eventId = Event_Id_01; sem = Semaphore_create(0, &semParams, NULL); /* create a Mailbox Instance */ Mailbox_Params_init(&mbxParams); mbxParams.readerEvent = evt; mbxParams.readerEventId = Event_Id_02; mbx = Mailbox_create(sizeof(MsgObj), 2, &mbxParams, NULL); /* create a writer task */ Task_Params_init(&tskParams); tskParams.priority = 1; tskParams.arg0 = (UArg) mbx; Task_create(writer, &tskParams, NULL); /* create a reader task */ Task_create(reader, &tskParams, NULL); BIOS_start(); /* does not return */ return(0); } /* * ======== clk0Fxn ======= */ Void clk0Fxn(UArg arg0) { /* Explicit posting of Event_Id_00 by calling Event_post() */ Event_post(evt, Event_Id_00); } /* * ======== clk1Fxn ======= */ Void clk1Fxn(UArg arg0) { /* Implicit posting of Event_Id_01 by Sempahore_post() */ Semaphore_post(sem); } /* * ======== reader ======== */ Void reader(UArg arg0, UArg arg1) { MsgObj msg; UInt posted; for (;;) { /* wait for (Event_Id_00 & Event_Id_01) | Event_Id_02 */ posted = Event_pend(evt, Event_Id_00 + Event_Id_01, /* andMask */ Event_Id_02, /* orMask */ TIMEOUT); if (posted == 0) { System_printf("Timeout expired for Event_pend()\n"); break; } if ((posted & Event_Id_00) && (posted & Event_Id_01)) { if (Semaphore_pend(sem, BIOS_NO_WAIT)) { System_printf("Explicit posting of Event_Id_00 and Implicit posting of Event_Id_01\n"); } else { System_printf("Semaphore not available. Test failed!\n"); } break; } else if (posted & Event_Id_02) { System_printf("Implicit posting of Event_Id_02\n"); if (Mailbox_pend(mbx, &msg, BIOS_NO_WAIT)) { /* print value */ System_printf("read id = %d and val = '%c'.\n",msg.id, msg.val); } else { System_printf("Mailbox not available. Test failed!\n"); } } else { System_printf("Unknown Event\n"); break; } } BIOS_exit(0); } /* * ======== writer ======== */ Void writer(UArg arg0, UArg arg1) { MsgObj msg; Int i; for (i=0; i < NUMMSGS; i++) { /* fill in value */ msg.id = i; msg.val = i + 'a'; System_printf("writing message id = %d val = '%c' ...\n", msg.id, msg.val); /* enqueue message */ Mailbox_post(mbx, &msg, TIMEOUT); } System_printf("writer done.\n"); }
Hi Mike-san,
Thank you for useful information.
Michael Erdahl said:What is your use case? Are you running RTOS?
My customer plans to use a non-SMP(AMP) configuration that implements RTOS on A15_0 and A15_1 respectively.
Is there an example that runs RTOS on each core and passes data to each other?
Best regards,
Sasaki