Other Parts Discussed in Thread: UNIFLASH
Please let me know if possible to use the latest UniFlash V6.0.0 software to program a QSPI NOR FLASH on a AM572x custom board. We are using the same device as the idkAM572x (i.e. S25FL256S).
Thanks,
Dave
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
uniflash_5.0.0
Please note that S25FL256S config reg quad bit not volatile,you can set S25FL256S config reg quad bit to 0,And to ensure that read backe correct ,then with flash writer write QSPI NOR FLASH.
My solution
/** * \file S25FL.c * * \brief Flash specific driver implementation. * */ /* * Copyright (C) 2014 - 2019 Texas Instruments Incorporated - http://www.ti.com/ * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the * distribution. * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS * "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT * LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR * A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT * OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, * SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT * LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, * DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY * THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT * (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE * OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * */ #include "S25FL.h" #include <ti/drv/spi/SPI.h> #include <ti/drv/spi/soc/QSPI_v1.h> /*! * @brief Flash object containing flash attributes. */ S25FL_Object s25flObject = {NULL, 4, S25FL_FLASH_SECTOR_SIZE, S25FL_FLASH_BLOCK_SIZE, S25FL_FLASH_DEVICE_SIZE, S25FL_FLASH_DEVICE_ID}; static bool SF25FL_ConfigMode_Write(uint32_t dstOffstAddr, unsigned char* srcAddr, uint32_t length, S25FL_Handle flashHandle); /* * ======== SF25FL_close ======== */ void SF25FL_close(S25FL_Handle handle) { SPI_close(handle->spiHandle); } /* * ======== SF25FL_open ======== */ S25FL_Handle SF25FL_open(unsigned int index, SPI_Params *params) { S25FL_Handle s25flHandle; s25flHandle = &s25flObject; /* Open SPI driver for SF25FL */ s25flHandle->spiHandle = SPI_open(index, params); return s25flHandle; } SPI_Transaction transaction; /* SPI transaction structure */ /* * ======== SF25FL_bufferWrite ======== */ bool SF25FL_bufferWrite(S25FL_Handle flashHandle, S25FL_Transaction* flashTransaction) { bool retVal = false; /* return value */ SPI_Handle handle = flashHandle->spiHandle; /* SPI handle */ uint32_t dstOffstAddr; /* Flash offset address */ uint8_t *srcAddr; /* Address of data buffer */ uint32_t length; /* data length in bytes */ uint32_t transferType; uint8_t transferCmd; QSPI_v1_Object *object; #ifdef SPI_DMA_ENABLE QSPI_HwAttrs *hwAttrs; #endif uint32_t offsetValue; uint32_t segLen = 1; uint32_t remainSize; /* Get the pointer to the object and hwAttrs */ object = (QSPI_v1_Object *)(handle->object); #ifdef SPI_DMA_ENABLE hwAttrs = (QSPI_HwAttrs *)(handle->hwAttrs); #endif /* Copy flash transaction parameters to local variables */ dstOffstAddr = flashTransaction->address; srcAddr = flashTransaction->data; length = flashTransaction->dataSize; if(QSPI_OPER_MODE_CFG == object->qspiMode) { offsetValue = *((uint32_t *)dstOffstAddr); /* * Config mode write supports 256 bytes at a time. So if the length is * greater than 256, then multiple transactions have to be performed till * all the bytes are written. */ while(length > 256) { SF25FL_ConfigMode_Write(dstOffstAddr, srcAddr, 256, flashHandle); *((uint32_t *)dstOffstAddr) += 256; srcAddr += 256; length -= 256; } if(length > 0) { SF25FL_ConfigMode_Write(dstOffstAddr, srcAddr, length, flashHandle); } *((uint32_t *)dstOffstAddr) = offsetValue; } if(QSPI_OPER_MODE_MMAP == object->qspiMode) { #ifdef SPI_DMA_ENABLE if (hwAttrs->dmaEnable) { segLen = 128; } #endif remainSize = length; while (remainSize > 0) { /* Write enable */ S25FLFlash_WriteEnable(flashHandle); /* Perform the transfer */ transaction.txBuf = (unsigned char *)dstOffstAddr; transaction.rxBuf = srcAddr; if (remainSize < segLen) { transaction.count = remainSize; } else { transaction.count = segLen; } transferType = SPI_TRANSACTION_TYPE_WRITE; if (dstOffstAddr > 0xFFFFFFU) { transferCmd = QSPI_LIB_CMD_PAGE_PRG_4B; } else { transferCmd = QSPI_LIB_CMD_PAGE_PRG; } SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); SPI_control(handle, SPI_V1_CMD_MMAP_TRANSFER_CMD, (void *)&transferCmd); retVal = SPI_transfer(handle, &transaction); dstOffstAddr += segLen; srcAddr += segLen; remainSize -= transaction.count; /* Check flash status for completion */ while ((FlashStatus(flashHandle) & 0x1U)); } } return retVal; } bool SF25FL_bufferRead(S25FL_Handle flashHandle, S25FL_Transaction* flashTransaction) { bool retVal = false; /* return value */ SPI_Handle handle = flashHandle->spiHandle; /* SPI handle */ unsigned char writeVal[4]; /* data to be written */ uint32_t addrLengthInBytes = 3U; /* Flash address length in bytes */ uint32_t readCmd = 0U; /* Read command */ uint32_t numDummyBits = 0U; /* Number of dummy bits */ uint32_t frameLength = 0U; /* Frame length */ uint32_t dstOffstAddr; /* Flash offset address */ unsigned char *srcAddr; /* Address of data buffer */ uint32_t length; /* data length in bytes */ /* unsigned int *tempPtr = (unsigned int *)&writeVal[0]; */ /* temp pointer */ unsigned int frmLength; unsigned int transferType; unsigned char transferCmd; QSPI_v1_Object *object; uint32_t offsetValue; /* Get the pointer to the object and hwAttrs */ object = handle->object; /* Copy flash transaction parameters to local variables */ dstOffstAddr = (uint32_t)flashTransaction->data; srcAddr = (unsigned char *)flashTransaction->address; length = flashTransaction->dataSize; if(QSPI_OPER_MODE_CFG == object->qspiMode) { offsetValue = *((uint32_t *)srcAddr); addrLengthInBytes = 3U; if(offsetValue > 0xFFFFFF) { /* Enter 32 bit addressing mode */ addrLengthInBytes = 4; } switch(object->rxLines) { case QSPI_RX_LINES_SINGLE: { if(offsetValue > 0xFFFFFF) { readCmd = QSPI_LIB_CMD_READ_SINGLE_4B; } else { readCmd = QSPI_LIB_CMD_READ_SINGLE; } numDummyBits = 0U; /* total transaction frame length in number of words (bytes)*/ frameLength = length + 1 + addrLengthInBytes; break; } case QSPI_RX_LINES_DUAL: { if(offsetValue > 0xFFFFFF) { readCmd = QSPI_LIB_CMD_READ_DUAL_4B; } else { readCmd = QSPI_LIB_CMD_READ_DUAL; } numDummyBits = 8U; /* total transaction frame length in number of words (bytes)*/ frameLength = length + 1 + 1 + addrLengthInBytes; break; } case QSPI_RX_LINES_QUAD: { if(offsetValue > 0xFFFFFF) { readCmd = QSPI_LIB_CMD_READ_QUAD_4B; } else { readCmd = QSPI_LIB_CMD_READ_QUAD; } numDummyBits = 8U; /* total transaction frame length in number of words (bytes)*/ frameLength = length + 1 + 1 + addrLengthInBytes; break; } default: break; } /* total transaction frame length */ frmLength = frameLength; SPI_control(handle, SPI_V1_CMD_SETFRAMELENGTH, (void *)&frmLength); /* Write read command */ writeVal[0] = readCmd; transaction.txBuf = (unsigned char *)&writeVal[0]; transaction.rxBuf = NULL; transaction.count = 1; transferType = SPI_TRANSACTION_TYPE_WRITE; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); /* Write Address Bytes */ /* *tempPtr = (unsigned int)srcAddr; */ /* transaction.txBuf = (unsigned char *)tempPtr; */ transaction.txBuf = (unsigned char *)srcAddr; transaction.rxBuf = NULL; transaction.count = addrLengthInBytes; transferType = SPI_TRANSACTION_TYPE_WRITE; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); /* Write dummy bits for fast read if required */ if(0 != numDummyBits) { writeVal[0] = 0U; transaction.txBuf = (unsigned char *)&writeVal[0]; transaction.rxBuf = NULL; transaction.count = (numDummyBits >> 3); /* In bytes */ transferType = SPI_TRANSACTION_TYPE_WRITE; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); } /* Read the actual flash data */ transaction.txBuf = NULL; transaction.rxBuf = (unsigned char *)dstOffstAddr; transaction.count = length; transferType = SPI_TRANSACTION_TYPE_READ; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); } if(QSPI_OPER_MODE_MMAP == object->qspiMode) { switch(object->rxLines) { case QSPI_RX_LINES_SINGLE: { if(flashTransaction->address > 0xFFFFFF) { readCmd = QSPI_LIB_CMD_READ_SINGLE_4B; } else { readCmd = QSPI_LIB_CMD_READ_SINGLE; } break; } case QSPI_RX_LINES_DUAL: { if(flashTransaction->address > 0xFFFFFF) { readCmd = QSPI_LIB_CMD_READ_DUAL_4B; } else { readCmd = QSPI_LIB_CMD_READ_DUAL; } break; } case QSPI_RX_LINES_QUAD: { if(flashTransaction->address > 0xFFFFFF) { readCmd = QSPI_LIB_CMD_READ_QUAD_4B; } else { readCmd = QSPI_LIB_CMD_READ_QUAD; } break; } default: break; } /* Perform the transfer */ transaction.txBuf = srcAddr; transaction.rxBuf = (uint8_t *)dstOffstAddr; transaction.count = length; transferType = SPI_TRANSACTION_TYPE_READ; transferCmd = (unsigned char)readCmd; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); SPI_control(handle, SPI_V1_CMD_MMAP_TRANSFER_CMD, (void *)&transferCmd); retVal = SPI_transfer(handle, &transaction); } return retVal; } bool S25FLFlash_WriteEnable(S25FL_Handle flashHandle) { SPI_Handle handle = flashHandle->spiHandle; /* SPI handle */ bool retVal = false; /* return value */ unsigned char writeVal; /* data to be written */ unsigned int operMode; /* temp variable to hold mode */ unsigned int rxLines; /* temp variable to hold rx lines */ unsigned int frmLength; unsigned int transferType; QSPI_v1_Object *object; unsigned int rxLinesArg; /* Get the pointer to the object and hwAttrs */ object = handle->object; /* These operations require the qspi to be configured in the following mode only: tx/rx single line and config mode. */ /* Save the current mode and rxLine configurations */ operMode = object->qspiMode; rxLines = object->rxLines; /* Update the mode and rxLines with the required values */ SPI_control(handle, SPI_V1_CMD_SETCONFIGMODE, NULL); rxLinesArg = QSPI_RX_LINES_SINGLE; SPI_control(handle, SPI_V1_CMD_SETRXLINES, (void *)&rxLinesArg); /* transaction frame length in words (bytes) */ frmLength = 1; SPI_control(handle, SPI_V1_CMD_SETFRAMELENGTH, (void *)&frmLength); /* Write enable command */ writeVal = QSPI_LIB_CMD_WRITE_ENABLE; /* Update transaction parameters */ transaction.txBuf = (unsigned char *)&writeVal; transaction.rxBuf = NULL; transaction.count = 1; transferType = SPI_TRANSACTION_TYPE_WRITE; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); /* Restore operating mode and rx Lines */ object->qspiMode = operMode; SPI_control(handle, SPI_V1_CMD_SETRXLINES, (void *)&rxLines); return retVal; } bool S25FLFlash_Enable4ByteAddrMode(S25FL_Handle flashHandle, bool enable4ByteMode) { SPI_Handle handle = flashHandle->spiHandle; /* SPI handle */ bool retVal = false; /* return value */ unsigned char writeVal; /* data to be written */ unsigned int operMode; /* temp variable to hold mode */ unsigned int rxLines; /* temp variable to hold rx lines */ unsigned int transferType; QSPI_v1_Object *object; unsigned int rxLinesArg; /* Get the pointer to the object and hwAttrs */ object = handle->object; /* These operations require the qspi to be configured in the following mode only: tx/rx single line and config mode. */ /* Save the current mode and rxLine configurations */ operMode = object->qspiMode; rxLines = object->rxLines; /* Update the mode and rxLines with the required values */ SPI_control(handle, SPI_V1_CMD_SETCONFIGMODE, NULL); rxLinesArg = QSPI_RX_LINES_SINGLE; SPI_control(handle, SPI_V1_CMD_SETRXLINES, (void *)&rxLinesArg); /* Command to control the 4 byte mode */ if (true == enable4ByteMode) { writeVal = QSPI_LIB_CMD_ENTER_4_BYTE_ADDR; } else { writeVal = QSPI_LIB_CMD_EXIT_4_BYTE_ADDR; } /* Write 4 byte enable/disable command to flash */ transaction.count = 1U; /* Frame length in bytes */ transaction.txBuf = (unsigned char *)&writeVal; /* Value to be written */ transaction.rxBuf = NULL; /* Nothing to read */ transaction.arg = NULL; /* Not applicable */ transferType = SPI_TRANSACTION_TYPE_WRITE; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); /* Restore operating mode and rx Lines */ object->qspiMode = operMode; SPI_control(handle, SPI_V1_CMD_SETRXLINES, (void *)&rxLines); return retVal; } uint32_t FlashStatus(S25FL_Handle flashHandle) { SPI_Handle handle = flashHandle->spiHandle; /* SPI handle */ bool retVal = false; /* return value */ unsigned char writeVal; /* data to be written */ uint32_t rxData = 0U; /* received data */ unsigned int operMode; /* temp variable to hold mode */ unsigned int rxLines; /* temp variable to hold rx lines */ unsigned int frmLength; unsigned int transferType; QSPI_v1_Object *object; unsigned int rxLinesArg; /* Get the pointer to the object and hwAttrs */ object = handle->object; /* These operations require the qspi to be configured in the following mode only: tx/rx single line and config mode. */ /* Save the current mode and rxLine configurations */ operMode = object->qspiMode; rxLines = object->rxLines; /* Update the mode and rxLines with the required values */ SPI_control(handle, SPI_V1_CMD_SETCONFIGMODE, NULL); rxLinesArg = QSPI_RX_LINES_SINGLE; SPI_control(handle, SPI_V1_CMD_SETRXLINES, (void *)&rxLinesArg); /* Total transaction frame length in words (bytes) */ frmLength = 1 + 1; SPI_control(handle, SPI_V1_CMD_SETFRAMELENGTH, (void *)&frmLength); /* Write Address Bytes */ writeVal = QSPI_LIB_CMD_READ_STATUS_REG; transaction.txBuf = (unsigned char *)&writeVal; transaction.rxBuf = NULL; transaction.count = 1U; transferType = SPI_TRANSACTION_TYPE_WRITE; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); if(retVal == false) { /* Error */ } /* Read the status register */ transaction.txBuf = NULL; transaction.rxBuf = (unsigned char *)&rxData; transaction.count = 1U; transferType = SPI_TRANSACTION_TYPE_READ; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); if(retVal == false) { /* Error */ } /* Restore operating mode and rx Lines */ object->qspiMode = operMode; SPI_control(handle, SPI_V1_CMD_SETRXLINES, (void *)&rxLines); return (rxData & 0xFF); } #if defined(SOC_AM574x) || defined (SOC_AM571x) || defined (SOC_AM572x) || defined (SOC_DRA72x) || defined (SOC_DRA75x) || defined (SOC_DRA78x) bool S25FLFlash_QuadModeEnable(S25FL_Handle flashHandle) { SPI_Transaction transaction; /* SPI transaction structure */ SPI_Handle handle = flashHandle->spiHandle; /* SPI handle */ unsigned char writeVal = 0U; /* data to be written */ uint32_t norStatus; /* flash status value */ uint32_t configReg; /* configuration register value */ uint32_t data; /* data to be written */ bool retVal = false; /* return value */ unsigned int operMode; /* temp variable to hold mode */ unsigned int rxLines; /* temp variable to hold rx lines */ unsigned int frmLength; unsigned int transferType; QSPI_v1_Object *object; unsigned int rxLinesArg; /* Get the pointer to the object and hwAttrs */ object = (QSPI_v1_Object *)handle->object; /* These operations require the qspi to be configured in the following mode only: tx/rx single line and config mode. */ /* Save the current mode and rxLine configurations */ operMode = object->qspiMode; rxLines = object->rxLines; /* Update the mode and rxLines with the required values */ SPI_control(handle, SPI_V1_CMD_SETCONFIGMODE, NULL); rxLinesArg = QSPI_RX_LINES_SINGLE; SPI_control(handle, SPI_V1_CMD_SETRXLINES, (void *)&rxLinesArg); /* Set transfer length in bytes: Reading status register */ //frmLength = 1 ; //SPI_control(handle, SPI_V1_CMD_SETFRAMELENGTH, (void *)&frmLength); /* Read command register */ /* writeVal = QSPI_LIB_CMD_WRITE_ENABLE; transaction.txBuf = (unsigned char *)&writeVal; transaction.rxBuf = NULL; transaction.count = 1; transferType = SPI_TRANSACTION_TYPE_WRITE; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction);*/ /* Set transfer length in bytes: Reading status register */ frmLength = 1 + 1; SPI_control(handle, SPI_V1_CMD_SETFRAMELENGTH, (void *)&frmLength); /* Read Status register */ writeVal = QSPI_LIB_CMD_READ_STATUS_REG; transaction.txBuf = (unsigned char *)&writeVal; transaction.rxBuf = NULL; transaction.count = 1; transferType = SPI_TRANSACTION_TYPE_WRITE; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); transaction.txBuf = NULL; transaction.rxBuf = (unsigned char *)&norStatus; transaction.count = 1; transferType = SPI_TRANSACTION_TYPE_READ; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); /* Set transfer length in bytes: Reading status register */ frmLength = 1 + 1; SPI_control(handle, SPI_V1_CMD_SETFRAMELENGTH, (void *)&frmLength); /* Read command register */ writeVal = QSPI_LIB_CMD_QUAD_RD_CMD_REG; transaction.txBuf = (unsigned char *)&writeVal; transaction.rxBuf = NULL; transaction.count = 1; transferType = SPI_TRANSACTION_TYPE_WRITE; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); transaction.txBuf = NULL; transaction.rxBuf = (unsigned char *)&configReg; transaction.count = 1; transferType = SPI_TRANSACTION_TYPE_READ; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); //while(1) { /* Set transfer length in bytes: Reading status register */ frmLength = 1 ; SPI_control(handle, SPI_V1_CMD_SETFRAMELENGTH, (void *)&frmLength); /* Read command register */ writeVal = QSPI_LIB_CMD_WRITE_ENABLE; transaction.txBuf = (unsigned char *)&writeVal; transaction.rxBuf = NULL; transaction.count = 1; transferType = SPI_TRANSACTION_TYPE_WRITE; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); /* Set 2nd bit of configuration register to 1 to enable quad mode */ configReg &=0xff; configReg |= (QSPI_FLASH_QUAD_ENABLE_VALUE << QSPI_FLASH_QUAD_ENABLE_BIT); //data = (QSPI_LIB_CMD_WRITE_STATUS_REG << 16) | ((norStatus&0xff) << 8) | configReg; data = (configReg<<16)|((norStatus&0xff) << 8)|QSPI_LIB_CMD_WRITE_STATUS_REG; //data = (QSPI_LIB_CMD_WRITE_STATUS_REG << 8) | (((norStatus&0xff)|0x06)) ; /* Set transfer length in bytes */ frmLength = 3; SPI_control(handle, SPI_V1_CMD_SETFRAMELENGTH, (void *)&frmLength); transaction.txBuf = (unsigned char *)&data; transaction.rxBuf = NULL; transaction.count = 3; transferType = SPI_TRANSACTION_TYPE_WRITE; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); //object->qspiParams.dataSize=24; retVal = SPI_transfer(handle, &transaction); //object->qspiParams.dataSize=8; /* Wait till the status register is being written */ while (1U == (FlashStatus(flashHandle) & 0x1U)); /* Set transfer length in bytes: Reading status register */ frmLength = 1 + 1; SPI_control(handle, SPI_V1_CMD_SETFRAMELENGTH, (void *)&frmLength); /* Read Status register */ writeVal = QSPI_LIB_CMD_READ_STATUS_REG; transaction.txBuf = (unsigned char *)&writeVal; transaction.rxBuf = NULL; transaction.count = 1; transferType = SPI_TRANSACTION_TYPE_WRITE; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); transaction.txBuf = NULL; transaction.rxBuf = (unsigned char *)&norStatus; transaction.count = 1; transferType = SPI_TRANSACTION_TYPE_READ; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); /* Set transfer length in bytes: Reading status register */ frmLength = 1 + 1; SPI_control(handle, SPI_V1_CMD_SETFRAMELENGTH, (void *)&frmLength); /* Read command register */ writeVal = QSPI_LIB_CMD_QUAD_RD_CMD_REG; transaction.txBuf = (unsigned char *)&writeVal; transaction.rxBuf = NULL; transaction.count = 1; transferType = SPI_TRANSACTION_TYPE_WRITE; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); transaction.txBuf = NULL; transaction.rxBuf = (unsigned char *)&configReg; transaction.count = 1; transferType = SPI_TRANSACTION_TYPE_READ; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); /* Set transfer length in bytes: Reading status register */ frmLength = 1 ; SPI_control(handle, SPI_V1_CMD_SETFRAMELENGTH, (void *)&frmLength); /* Read command register */ writeVal = 0x04; transaction.txBuf = (unsigned char *)&writeVal; transaction.rxBuf = NULL; transaction.count = 1; transferType = SPI_TRANSACTION_TYPE_WRITE; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); /* Set transfer length in bytes: Reading status register */ frmLength = 1 + 1; SPI_control(handle, SPI_V1_CMD_SETFRAMELENGTH, (void *)&frmLength); /* Read Status register */ writeVal = QSPI_LIB_CMD_READ_STATUS_REG; transaction.txBuf = (unsigned char *)&writeVal; transaction.rxBuf = NULL; transaction.count = 1; transferType = SPI_TRANSACTION_TYPE_WRITE; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); transaction.txBuf = NULL; transaction.rxBuf = (unsigned char *)&norStatus; transaction.count = 1; transferType = SPI_TRANSACTION_TYPE_READ; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); } /* Restore operating mode and rx Lines */ object->qspiMode = operMode; SPI_control(handle, SPI_V1_CMD_SETRXLINES, (void *)&rxLines); return retVal; } #endif #if defined(SOC_AM437x) bool S25FLFlash_QuadModeEnable(S25FL_Handle flashHandle) { SPI_Handle handle = flashHandle->spiHandle; /* SPI handle */ unsigned char writeVal = 0U; /* data to be written */ uint32_t norStatus; /* flash status value */ bool retVal = false; /* return value */ unsigned int operMode; /* temp variable to hold mode */ unsigned int rxLines; /* temp variable to hold rx lines */ unsigned int frmLength; unsigned int transferType; QSPI_v1_Object *object; unsigned int rxLinesArg; /* Get the pointer to the object and hwAttrs */ object = handle->object; /* These operations require the qspi to be configured in the following mode only: tx/rx single line and config mode. */ /* Save the current mode and rxLine configurations */ operMode = object->qspiMode; rxLines = object->rxLines; /* Update the mode and rxLines with the required values */ SPI_control(handle, SPI_V1_CMD_SETCONFIGMODE, NULL); rxLinesArg = QSPI_RX_LINES_SINGLE; SPI_control(handle, SPI_V1_CMD_SETRXLINES, (void *)&rxLinesArg); /* Set transfer length in bytes: Reading status register */ frmLength = 1 + 1; SPI_control(handle, SPI_V1_CMD_SETFRAMELENGTH, (void *)&frmLength); /* Read Status register */ writeVal = 0x05U; //QSPI_LIB_CMD_READ_STATUS_REG; //Cmd for AM437x transaction.txBuf = (unsigned char *)&writeVal; transaction.rxBuf = NULL; transaction.count = 1; transferType = SPI_TRANSACTION_TYPE_WRITE; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); transaction.txBuf = NULL; transaction.rxBuf = (unsigned char *)&norStatus; transaction.count = 1; transferType = SPI_TRANSACTION_TYPE_READ; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); /* Flash write enable */ S25FLFlash_WriteEnable(flashHandle); /* Set transfer length in bytes: Reading status register */ frmLength = 1 + 1; SPI_control(handle, SPI_V1_CMD_SETFRAMELENGTH, (void *)&frmLength); /* Read command register */ writeVal = 0x01U; //QSPI_LIB_CMD_QUAD_RD_CMD_REG; transaction.txBuf = (unsigned char *)&writeVal; transaction.rxBuf = NULL; transaction.count = 1; transferType = SPI_TRANSACTION_TYPE_WRITE; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); /* Set status register 6th bit to 1 for Quad enable * Write this value to the status register. */ norStatus &= ~(1U << 0x6U); norStatus |= (0x1U << 0x6U); transaction.txBuf = (unsigned char *)&norStatus; transaction.rxBuf = NULL; transaction.count = 1; transferType = SPI_TRANSACTION_TYPE_WRITE; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); /* Wait till the status register is being written */ while (1U == (FlashStatus(flashHandle) & 0x1U)); /* Restore operating mode and rx Lines */ object->qspiMode = operMode; SPI_control(handle, SPI_V1_CMD_SETRXLINES, (void *)&rxLines); return retVal; } #endif bool S25FLFlash_BlockErase(S25FL_Handle flashHandle, unsigned int blockNumber) { uint32_t eraseAddr; /* Flash erase address */ uint32_t writeVal; /* data to be written */ SPI_Handle handle = flashHandle->spiHandle; /* SPI handle */ unsigned int addrLenInBytes = 3; /* address length in bytes */ bool retVal = false; /* return value */ unsigned int operMode; /* temp variable to hold mode */ unsigned int rxLines; /* temp variable to hold rx lines */ unsigned int frmLength; unsigned int transferType; QSPI_v1_Object *object; unsigned int rxLinesArg; uint32_t tempAddr; /* Get the pointer to the object and hwAttrs */ object = handle->object; /* Compute flash erase address based on the block size */ eraseAddr = blockNumber * flashHandle->blockSize; /* These operations require the qspi to be configured in the following mode only: tx/rx single line and config mode. */ /* Save the current mode and rxLine configurations */ operMode = object->qspiMode; rxLines = object->rxLines; /* Update the mode and rxLines with the required values */ SPI_control(handle, SPI_V1_CMD_SETCONFIGMODE, NULL); rxLinesArg = QSPI_RX_LINES_SINGLE; SPI_control(handle, SPI_V1_CMD_SETRXLINES, (void *)&rxLinesArg); if(eraseAddr > 0xFFFFFF) { /* Enter 4 byte addressing mode */ addrLenInBytes = 4; } tempAddr = ((eraseAddr & 0xFF000000) >> 24) | ((eraseAddr & 0x00FF0000) >> 8) | ((eraseAddr & 0x0000FF00) << 8) | ((eraseAddr & 0x000000FF) << 24); if(addrLenInBytes == 3) { tempAddr = (tempAddr >> 8) & 0x00FFFFFF; } /* Flash write enable */ S25FLFlash_WriteEnable(flashHandle); /*total transaction frame length */ frmLength = 1 + addrLenInBytes; SPI_control(handle, SPI_V1_CMD_SETFRAMELENGTH, ((void *)&frmLength)); /* Block erase command */ if(eraseAddr > 0xFFFFFF) { writeVal = QSPI_LIB_CMD_BLOCK_ERASE_4B; } else { writeVal = QSPI_LIB_CMD_BLOCK_ERASE; } transaction.txBuf = (unsigned char *)&writeVal; transaction.rxBuf = NULL; transaction.count = 1; transferType = SPI_TRANSACTION_TYPE_WRITE; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); /* Send erase address */ writeVal = tempAddr; transaction.txBuf = (unsigned char *)&writeVal; transaction.rxBuf = NULL; transaction.count = addrLenInBytes; transferType = SPI_TRANSACTION_TYPE_WRITE; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); /* Check flash status for write completion */ while (1U == (FlashStatus(flashHandle) & 0x1U)); /* Restore operating mode and rx Lines */ object->qspiMode = operMode; SPI_control(handle, SPI_V1_CMD_SETRXLINES, (void *)&rxLines); return retVal; } void FlashPrintId(S25FL_Handle flashHandle) { uint32_t writeVal; /* data to be written */ SPI_Handle handle = flashHandle->spiHandle; /* SPI handle */ bool retVal = false; /* return value */ unsigned char mfgId = 0; /* manufacture ID value */ unsigned char deviceId = 0; /* device ID value */ unsigned int operMode; /* temp variable to hold mode */ unsigned int rxLines; /* temp variable to hold rx lines */ unsigned int frmLength; unsigned int transferType; QSPI_v1_Object *object; unsigned int rxLinesArg; /* Get the pointer to the object and hwAttrs */ object = handle->object; /* These operations require the qspi to be configured in the following mode only: tx/rx single line and config mode. */ /* Save the current mode and rxLine configurations */ operMode = object->qspiMode; rxLines = object->rxLines; /* Update the mode and rxLines with the required values */ SPI_control(handle, SPI_V1_CMD_SETCONFIGMODE, NULL); rxLinesArg = QSPI_RX_LINES_SINGLE; SPI_control(handle, SPI_V1_CMD_SETRXLINES, (void *)&rxLinesArg); /* Total transaction frame length in bytes */ frmLength = 1 + 3 + 2; /* cmd + address + read data */ SPI_control(handle, SPI_V1_CMD_SETFRAMELENGTH, (void *)&frmLength); /* Write Command */ writeVal = QSPI_LIB_CMD_READ_MFG_ID; transaction.txBuf = (unsigned char *)&writeVal; transaction.rxBuf = NULL; transaction.count = 1; transferType = SPI_TRANSACTION_TYPE_WRITE; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); if(retVal == false) { /* Error */ } /* Write Address Bytes */ writeVal = 0x0U; transaction.txBuf = (unsigned char *)&writeVal; transaction.rxBuf = NULL; transaction.count = 3; transferType = SPI_TRANSACTION_TYPE_WRITE; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); /* Read Manufacturer ID * The manufacturer ID is of 1 byte(8 bits) */ transaction.txBuf = NULL; transaction.rxBuf = &mfgId; transaction.count = 1; transferType = SPI_TRANSACTION_TYPE_READ; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); /* Read Device ID */ transaction.txBuf = NULL; transaction.rxBuf = &deviceId; transaction.count = 1; transferType = SPI_TRANSACTION_TYPE_READ; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); /* Note - This ID is the device ID of the flash device. * This ID is read from the flash */ /* Restore operating mode and rx Lines */ object->qspiMode = operMode; SPI_control(handle, SPI_V1_CMD_SETRXLINES, (void *)&rxLines); } static bool SF25FL_ConfigMode_Write(uint32_t dstOffstAddr, unsigned char* srcAddr, uint32_t length, S25FL_Handle flashHandle) { bool retVal = false; /* return value */ SPI_Handle handle = flashHandle->spiHandle; /* SPI handle */ uint32_t addrLengthInBytes = 3U; /* Flash addr length in bytes */ unsigned int frmLength; unsigned char writeVal[4]; /* data to be written to QSPI */ unsigned int transferType; uint32_t offsetValue; addrLengthInBytes = 3U; /* Flash address length in bytes */ offsetValue = *((uint32_t *)dstOffstAddr); /* Extract address word length from the flash's destination offst addr*/ if(offsetValue > 0xFFFFFF) { /* Enter 32 bit addressing mode */ addrLengthInBytes = 4; } /* Write Enable */ S25FLFlash_WriteEnable(flashHandle); /* total transaction frame length in number of words (bytes)*/ frmLength = 1 + addrLengthInBytes + length; SPI_control(handle, SPI_V1_CMD_SETFRAMELENGTH, ((void *)&frmLength)); /* Send Flash write command */ writeVal[0] = QSPI_LIB_CMD_PAGE_PRG; /* Flash write command */ transaction.txBuf = (unsigned char *)&writeVal[0]; transaction.rxBuf = NULL; transaction.count = 1U; transferType = SPI_TRANSACTION_TYPE_WRITE; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); /* Send flash address offset to which data has to be written */ transaction.txBuf = (unsigned char *)dstOffstAddr; transaction.rxBuf = NULL; transaction.count = addrLengthInBytes; transferType = SPI_TRANSACTION_TYPE_WRITE; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); /* Write buffer data to flash */ transaction.txBuf = (unsigned char *)srcAddr; transaction.rxBuf = NULL; transaction.count = length; transferType = SPI_TRANSACTION_TYPE_WRITE; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); /* Check flash status for write completion */ while ((FlashStatus(flashHandle) & 0x1U)); return retVal; } bool S25FLFlash_WriteDis(S25FL_Handle flashHandle) { SPI_Handle handle = flashHandle->spiHandle; /* SPI handle */ bool retVal = false; /* return value */ unsigned int frmLength; unsigned char writeVal = 0U; /* data to be written */ unsigned int transferType; /* transaction frame length in words (bytes) */ frmLength = 1; SPI_control(handle, SPI_V1_CMD_SETFRAMELENGTH, (void *)&frmLength); /* Write enable command */ writeVal = 0x04; /* Update transaction parameters */ transaction.txBuf = (unsigned char *)&writeVal; transaction.rxBuf = NULL; transaction.count = 1; transferType = SPI_TRANSACTION_TYPE_WRITE; SPI_control(handle, SPI_V1_CMD_TRANSFERMODE_RW, (void *)&transferType); retVal = SPI_transfer(handle, &transaction); }
Thanks for your help! I'll compare with my implementation. Perhaps I'll use FlashWriter for programming as it looks like UniFlash may not support custom AM572x boards.
Regards,
Dave
Hi Dave,
All the source for the target uniflash utility is provided with the PDK. If you dig into the code, you'll find the board specific files are in the path <pdk root>/packages/ti/board/src/<board>. There you can update the necessary clock, pinmux, etc, then rebuild the uniflash target program. From there, you should be able to use the TI host uniflash utility.
Regards,
Mike