Other Parts Discussed in Thread: OMAP-L137
Hi,
I am using the OMAPL137 EVM, and i got some how erased the flash.
I used the flashing steps as given in site "http://processors.wiki.ti.com/index.php/Serial_Boot_and_Flash_Loading_Utility_for_OMAP-L137" .
I am using the linux for flashing and the steps i follow are first i erase and then i flash using the command flash_dsp and give all the three input files.
the format i follow is
"mono ./sfh_OMAP-L137.exe <Command> [-targetType <Target>] [-flashType <FlashType>] [<Options>] [<InputFiles>]"
target type will be "OMAPL_v1" and flashtype will be "SPI_MEM" and in options i am setting the baud rate as 230400.
But after flashing i am not getting any thing on the minicom after making the BOOT pin adjustments.
I am taking care of the BOOT pin each time i flash and boot.
and if the BOOT pin is in the UART2 BOOT mode then it shows "BOOTME" prompt only once, is this causes any problem? Does the BOOTME prompt becoming continuously?
i took the dsp_ubl.bin, arm_ubl.bin, u-boot.bin from the folder in the PSP installation package.
Flashing is going on fine but when i reboot the board i am not getting any thingon the console.
Please if some one can help me out of this problem.